Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Boxing up Raspi?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 712 subscribers
  • Views 5031 views
  • Users 0 members are here
  • the
  • raspi
  • up
  • boxing
  • raspberry_pi
Related

Boxing up Raspi?

e14 Contributor
e14 Contributor over 14 years ago

I would like to think that I could make a box to contain the Raspi, but looking at the Safety Information,

it should be operated in a ventilated environment and not covered.

And of course, it would be electricily safe, wouldn't it?

I have seen a report somwhere that a container was made from Lego bricks!

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 14 years ago

    Some people have reported problems with RasPi overheating, so putting it in a closed box may not be a good idea.  The RasPi Foundation has been pretty quiet lately about plans for an official case.  Probably the best would be a metal box with a thermal pad on the bottom to take heat away from the 3.3V regulator RG2, the BCM2835 SoC and LAN9512 USB/Ethernet chips.  Or you can have a perforated metal cover like a power supply.  Highest voltage is 5V so you won't be harmed by electricity.  When I get mine, I'm planning to run it on conductive bubble wrap to start, and then if all works out make up a box I can run with the lid off or make a perforated metal lid.

     

    There are tons of case ideas and discussion at raspberrypi.org.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to johnbeetem

    I'd like to see someone water cool this kit. You'd probably have to use a waterblock designed for a North or South bridge, but it would be an interesting theory to see in action.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to johnbeetem

    I'd like to see someone water cool this kit. You'd probably have to use a waterblock designed for a North or South bridge, but it would be an interesting theory to see in action.