Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Ready for more testing: SPI enabled kernel.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 706 subscribers
  • Views 492 views
  • Users 0 members are here
  • lcd
  • hardware
  • spi
  • display
Related

Ready for more testing: SPI enabled kernel.

rew
rew over 14 years ago

I've done some work on the driver originally written by A Robinson<arobinson@cs.man.ac.uk>. I've implemented a few missing things and removed a bug or two.

 

Those that want this can test this, Both the patch and a binary kernel image are available for download linked from our WIKI.

 

http://www.bitwizard.nl/wiki/index.php/Raspberry_pi_spi_kernel

 

Things you might want to connect to your SPI bus on the raspberry pi can be bought at our shop: http://www.bitwizard.nl/catalog/ .

(The easiest way to start is with the rpi_serial board, which has the SPI bus in the same pinout as the expansion boards. )

 

Comments, bug reports etc etc. are welcome.

 

Requests for other boards are welcome as well. We'll look into making them.

 

I'll build a program for interfacing with the other boards tomorrow. (Mostly removing things from the program that displays things on the LCD).

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hi Roger,

     

    Thank you for your work! Your binary kernel's SPI functionality works (although there is a couple of issues), but with one I've built using your patch does not.

     

    When I insert the module I get an error that the chipselect is already in use and spidev0.x cannot be created. Am I missing something?

     

    I'm ready to perform extensive testing and possibly improvement of the driver (although I do not have much experience in kernel driver development).

     

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hi Roger,

     

    Thank you for your work! Your binary kernel's SPI functionality works (although there is a couple of issues), but with one I've built using your patch does not.

     

    When I insert the module I get an error that the chipselect is already in use and spidev0.x cannot be created. Am I missing something?

     

    I'm ready to perform extensive testing and possibly improvement of the driver (although I do not have much experience in kernel driver development).

     

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rew
    rew over 14 years ago in reply to e14 Contributor

    Sergey, there seem to be several independent people working on SPI stuff.

     

    Last I heard the debian wheezy distribution comes with the latest kernel, and that the latest kernel already has SPI support enabled. Someone else AGAIN wrote another SPI kernel driver. We'll have to check that one out to see if it works as good as this one and doesn't have these defects.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to rew

    Roger Wolff wrote:

    [...]

    Last I heard the debian wheezy distribution comes with the latest kernel, and that the latest kernel already has SPI support enabled.

    Well, I've downloaded the official public beta "wheezy" 2012-06-18 [1] - it comes with 3.1.9+ kernel and no SPI...

     

    [1] http://www.raspberrypi.org/archives/1435