Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Wireless network conectivity
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 75 replies
  • Subscribers 707 subscribers
  • Views 10232 views
  • Users 0 members are here
  • raspberry
  • pi
  • wireless
Related

Wireless network conectivity

wallarug
wallarug over 14 years ago

I bought one of these about 12 mths ago: http://www.jaycar.com.au/productView.asp?ID=YN8306&keywords=high+power+wireless+n&form=KEYWORD

I downloaded the drivers from the link above then installed them on a windows computer.  How do I use these linux drivers/installers on the raspberry pi to get the wireless adaptor to work?

 

Will this work with the Raspberry Pi?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    If your adaptor uses Broadcom chipset you may need to install a piece of firmware to make it work. I had a similar problem with my Linux netbook that had Ralink wifi. It booted up but said that there was no WiFi as no firmware was loaded! After much searching the solution is at http://linuxwireless.org/en/users/Drivers/b43.

     

    The B43 package installs the firmware needed to run the Broadcom chipset. As its not GPL it can't be released with any Linux package, but is able to be extracted from the Windows driver. This package is already to go, just install!

     

    I required the firmware-b43-installer package. Not sure if it's in the RasPi repositories as I haven't got mine to play with yet... :-( But the above site it fairly comprehensive!

     

    Hope it works.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    i have had issues with broadcom on various laptops using different distro's of linux, this is the best solution i have found so far. i also cant confirm at the moment if the b43 firmware is in the repositories. i will check tonight and see if it is.

     

    i cant actually try this on the R-Pi as i dont have a USB wifi adapter with the broadcom chipset.

     

    http://ubuntuforums.org/showpost.php?p=10527475&postcount=5

     

    hope this helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to GreenYamo

    I ahev the drivers, I just can't install them becasue I am a Linux n00b.image

     

    Could you help with this and this would solve my problem.

     

    Fergus

     

    See: http://www.raspberrypi.org/phpBB3/viewtopic.php?f=45&t=13482&p=143746#p143746 for files that I need help with.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to wallarug

    Fergus Byrne wrote:

     

    I ahev the drivers, I just can't install them becasue I am a Linux n00b.image

     

    Could you help with this and this would solve my problem.

     

    Fergus

     

    See: http://www.raspberrypi.org/phpBB3/viewtopic.php?f=45&t=13482&p=143746#p143746 for files that I need help with.

    Here is the instructions from the readme file that I don't understand/can't find the correct agruments to fill-in.  Could you PLEASE fill-in what I can't and then post back here.  please image.

     

              define the linux kernel source include file path LINUX_SRC

                         modify to meet your need.

     

    3> In os/linux/config.mk

              define the GCC and LD of the target machine

              define the compiler flags CFLAGS

              modify to meet your need.

              ** Build for being controlled by NetworkManager or wpa_supplicant wext functions

                 Please set 'HAS_WPA_SUPPLICANT=y' and 'HAS_NATIVE_WPA_SUPPLICANT_SUPPORT=y'.

                 => #>cd wpa_supplicant-x.x

                 => #>./wpa_supplicant -Dwext -ira0 -c wpa_supplicant.conf -d

              ** Build for being controlled by WpaSupplicant with Ralink Driver

                 Please set 'HAS_WPA_SUPPLICANT=y' and 'HAS_NATIVE_WPA_SUPPLICANT_SUPPORT=n'.

                 => #>cd wpa_supplicant-0.5.7

                 => #>./wpa_supplicant -Dralink -ira0 -c wpa_supplicant.conf -d

     

     

    4> $make

              # compile driver source code

              # To fix "error: too few arguments to function ¡¥iwe_stream_add_event"

                => $patch -i os/linux/sta_ioctl.c.patch os/linux/sta_ioctl.c

     

     

    5> $cp RT2870STA.dat  /etc/Wireless/RT2870STA/RT2870STA.dat

     

    6> load driver, go to "os/linux/" directory.

        #[kernel 2.4]

        #    $/sbin/insmod rt2870sta.o

        #    $/sbin/ifconfig ra0 inet YOUR_IP up

     

        #[kernel 2.6]

        #    $/sbin/insmod rt2870sta.ko

        #    $/sbin/ifconfig ra0 inet YOUR_IP up

     

     

    7> unload driver   

        $/sbin/ifconfig ra0 down

              $/sbin/rmmod rt2870sta

    Attachments:
    7674.Makefile.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GreenYamo
    GreenYamo over 14 years ago in reply to wallarug

    Hello Fergus, i'm afraid as I said above, i'm very much a Linux noob too, and other than looking like those instructions are for re-compiling the kernal with the drivers included (and even that is probably wrong) I can't help much image

    All I can say is that to get my USB stick working, I didn't have to do any this, just the instructions I posted a way back up this thread. I think there must be an easier way than doing the above.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to GreenYamo

    Thats ok.  but I found this site which looks interesting, I am posting it here so I can find it later image

    http://linux.die.net/man/8/iwconfig

     

    For fixing a file I messed up.

    http://elinux.org/RPi_Peripherals#Wireless:_TP-Link_TL-WN722N_USB_wireless_adapter_.28Debian_6.29

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to GreenYamo

    I bought the Edimax EW-7811Un but I need help setting it up, Steve, could you please help me with this one.  The RPi wiki says that it is verified but there is no guide to set-up this device for Raspbian.  I found this guide: http://www.ctrl-alt-del.cc/2012/05/raspberry-pi-meets-edimax-ew-7811un-wireless-ada.html but it has not worked for my RPi.  I think it has something to do with me not being able to get the rpi-update thing.  I tried to get this but failed.  Everytime I run rpi-update it returns:

     

    /usr/bin/rpi-update: line 1: syntax error near unexpected token `newline'

    /usr/bin/rpi-update: line 1: `<!DOCTYPE html PUBLIC "-//W3C//DTD XHTML 1.0 Trans                                                                             itional//EN" "http://www.w3.org/TR/xhtml1/DTD/xhtml1-transitional.dtd">'

     

     

    Can this be fixed so that I can update the firmware?

     

    Wireless card help would be nice as well image.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to wallarug

    I noticed from the link that Edimax uses the rtl8192cu driver.  I have another adapter (Asus USB-N13) which uses that driver and it did not work by default with the current Raspbian Wheezy image.  However, it did work ok with Adafruit's new image as it includes that driver, so you may want to give that a try: http://learn.adafruit.com/adafruit-raspberry-pi-educational-linux-distro/occidentalis-v0-dot-1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to GreenYamo

    With the EDIMAX, it gives me the errors:

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

     

    The "name of the parts" are all different.

     

    What can be done to fix this issue?  This might sovle my problem.

     

    How do you unpack a .ko file?

     

    I didn't unpack mine.  this could be leading to the above issues.








     

    Message was edited by: Fergus Byrne

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to fustini

    Drew Fustini wrote:

     

    I noticed from the link that Edimax uses the rtl8192cu driver.  I have another adapter (Asus USB-N13) which uses that driver and it did not work by default with the current Raspbian Wheezy image.  However, it did work ok with Adafruit's new image as it includes that driver, so you may want to give that a try: http://learn.adafruit.com/adafruit-raspberry-pi-educational-linux-distro/occidentalis-v0-dot-1

    I do not really want to change image (right now).  But I might give it a go in the future.

     

    Right now though, I just want to get this adapter working. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to wallarug

    My guess is that the 8192cu.ko module you have doesn't agree with the version of the kernel your running.  a .ko file is a kernel module file and shouldn't have to unpacked.  the utility "modinfo" will print out information about the module.  could you run that and paste the output?  also, could you paste what "uname -a" outputs?  it might be that the kernel versions don't agree.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to fustini

    will do image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • wallarug
    wallarug over 14 years ago in reply to fustini

    will do image