Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Wireless network conectivity
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 75 replies
  • Subscribers 707 subscribers
  • Views 10199 views
  • Users 0 members are here
  • raspberry
  • pi
  • wireless
Related

Wireless network conectivity

wallarug
wallarug over 14 years ago

I bought one of these about 12 mths ago: http://www.jaycar.com.au/productView.asp?ID=YN8306&keywords=high+power+wireless+n&form=KEYWORD

I downloaded the drivers from the link above then installed them on a windows computer.  How do I use these linux drivers/installers on the raspberry pi to get the wireless adaptor to work?

 

Will this work with the Raspberry Pi?

  • Sign in to reply
  • Cancel
Parents
  • wallarug
    wallarug over 14 years ago

    I should add that I am using the latest Debian image.

     

    If it does work, what are the commands to install this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GreenYamo
    GreenYamo over 14 years ago in reply to wallarug

    Fergus,

     

    I would try here first:

     

    http://elinux.org/RPi_VerifiedPeripherals#USB_WiFi_Adapters

     

    There is also a guide for installing if yours is on the working list.

     

    Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 14 years ago in reply to wallarug

    Hmmmm. It seems I missed one of your posts....

     

    WPA supplicant does something relating to WPA. So if your wifi is WPA protected, your 'pi will have to do something with WPA_SUPPLICANT. Whether or not this is hidden "behind  the scenes" I don't know.


    On my Ubuntu Laptop, I have this fancy network-icon in the toolbar. It shows the wifi networks, and when I select an encrypted one, it asks me for the password. From then on it connects automatically....


    That applet is called "nm-applet".

     

    I'm usually a commandline guy, but with wifi, I kind of like the fact that I haven't had to delve into it to have it work.

     

    Hmm. come to think of it, I have my home-pi on my (encrypted) home network. I just have

    auto wlan0

    iface wlan0 inet dhcp

    wpa-conf /etc/wpa.conf

    in /etc/network/interfaces and then

    network={

    ssid="XXXXXX"

    proto=RSN

    key_mgmt=WPA-PSK

    pairwise=CCMP TKIP

    group=CCMP TKIP

    psk="XXXXXXX"

    }

    in /etc/wpa.conf .


    Then a restart of the network should work. Again I'm lazy figuring out how to do that, so I either unplug/replug the wifi dongle, or I just reboot the whole thing. (I'm sure it can be done, but not doing it is faster).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to rew

    I will look into WPA supplicant.  For my RPi and network.  The link above seemed to look good and easy to do.,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to wallarug

    Have not had time to look into WPA supplicant stuff.  but now that I know the model of the wireless adapter (RT2870) I can put the supplied drivers up here.  I hope that someone can tell me what to do with what was given to me and whether or not I need to install/add anything to the Raspberry Pi for wireless adapter to work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    http://wiki.debian.org/rt2870sta#Installation

     

    i simply followed that for installing my RT2800 series wireless dongle, worked first time.

     

    so, simpllified these are the steps i took.

     

    sudo apt-get install firmware-ralink

    sudo apt-get install network-manager-gnome

    sudo reboot

     

    when rebooted, log in, startx and find the network manager in the bottom right corner, select your connection, put password in and it should all work.

    you can of course mess with the /etc/network/interfaces to enable network at boot.

     

    hope this helps somewhat...good luck

     

    EDITED TO REMOVE INCORRECT LINK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    Trying this now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    network manager seems to be slowing down the RPi quite alot.  I am having speed issues with this program.  Also, it installed a bluetooth process which I don't need, how do I kill that process?  (I tried "ps-l" but it does not come up but it does with "pstree")

    EDIT: so that it will not start ever-again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    you can remove the network manager if you want (sudo apt-get remove network-manager-gnome) and edit the /etc/network/interfaces file so it connects at boot (sudo nano /etc/network/interfaces)

     

    this is how mine looks:-

     

    auto lo

    iface lo inet loopback

     

    auto wlan0

    iface wlan0 inet static

    address 192.168.0.50 (for example)

    netmask 255.255.255.0 (for example)

    gateway 192.168.0.1 (for expample)

    wireless-essid wireless network name here

    wireless-key wireless password here

     

    iface eth0 inet dhep

     

     

    cant help with killing the bluetooth process (sorry).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    How come what you have in that file is different to what the wiki says to input? 

     

    Also, do you know if I have to change anything (from the above) if I use WPA2 security?

     

    I am also going to use a fresh image (Debian Wheezy) when I find time to set it up.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    i cant find where i got that info from, i will keep looking but in the mean time you can have a look at the following

     

    http://wiki.debian.org/WiFi/AdHoc

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    I see.

     

    You have an ADhoc network set-up.

     

    I want to use a different set-up involving existing network equipment.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    I see.

     

    You have an ADhoc network set-up.

     

    I want to use a different set-up involving existing network equipment.