Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Wireless network conectivity
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 75 replies
  • Subscribers 707 subscribers
  • Views 10173 views
  • Users 0 members are here
  • raspberry
  • pi
  • wireless
Related

Wireless network conectivity

wallarug
wallarug over 14 years ago

I bought one of these about 12 mths ago: http://www.jaycar.com.au/productView.asp?ID=YN8306&keywords=high+power+wireless+n&form=KEYWORD

I downloaded the drivers from the link above then installed them on a windows computer.  How do I use these linux drivers/installers on the raspberry pi to get the wireless adaptor to work?

 

Will this work with the Raspberry Pi?

  • Sign in to reply
  • Cancel
  • GreenYamo
    GreenYamo over 14 years ago in reply to wallarug

    Fergus,

     

    The wireless dongle you link to appears to use the realtek chipset, not the ralink firmware as mine does, so I would try

     

    apt-get install firmware-realtek

     

    then the rest as I linked to.

    It may also be worth having a play with the Beta of Debian Wheezy, as I think that has more support for wireless stuff : http://www.raspberrypi.org/archives/1435

     

    I would also try using the dongle in a powered hub, rather than directly into the pi as it may not be able to supply enough juice.

     

    Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to GreenYamo

    Steve,

     

    If i heve installed the wrong fireware (which you say) how do I uninstall the ralink fireware?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 14 years ago in reply to wallarug

    Installing an extra package isn't going to hurt your 'pi. It'll take a few bytes of SD-card-space, but that's all.

     

    If you installed it using apt-get, the command to uninstall is:

     

       apt-get remove <package name>

     

    (where you fill in the package name (without the brackets)).

     

    The realtek firmware lives in a file with "realtek" in it. When the system detects the insertion of a realtek wifi card, the driver will say: "Hey, I need the firmware for this realtek card". The system will look in a specific file and if that doesn't exist, that's the end of it. The driver will not be able to use your realtek wifi module.

     

    If you have an ra-link, the filename will be different, so it will load the proper firmware even if the realtek firmware is installed. Or the other way around.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to GreenYamo

    Anyone,

     

    After I added the lines to the /etc/network/interfaces I have lost all ethernet connections to the RPi.  Any fixes?   I can't change the fireware if I have no internet.

    EDIT: I have uninstalled the ralink fireware.and... still no ethernet! image

    EDIT (2): seems that the ethernet cable was not plug-in correctly.  Now onto the fixing that wireless card.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to rew

    Thanks for that, old fireware removed and new one installed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to wallarug

    This does not look good for the Raspberry Pi:

     

         DHCPDISCOVER on wlan0 to 255.255.255.255 port 67 interval 1

         send_packet: Network is down

         phy0 -> rt2x00lib_request_firmware: Error - Fail to request Fireware.

         No DHCPOFFERS recieved.

         No working lease in persistent database - sleeping.

     

    Make any sense to anyone?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to wallarug

    Can someone please tell me what drivers/firmware I need for my particular model of card, None of the above firmwares seem to be working.  Link to download: http://www.jaycar.com.au/productView.asp?ID=YN8306&keywords=high+power+wireless+n&form=KEYWORD

    All the Linux drivers are in the download.  Can someone please look though them and see what needs to be done.  I have no idea what is what and how to install this USB card.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 14 years ago in reply to wallarug

    Fergus Byrne wrote:

     

    This does not look good for the Raspberry Pi:

         phy0 -> rt2x00lib_request_firmware: Error - Fail to request Fireware.

     

    This is what I like about Linux, and dislike about Windows: When something goes wrong, you get an error message that makes sense. In this case you're missing the firmware files for your wireless card.


    If you've messed up your "interfaces" file so you no longer have any internet put:

     

      iface eth0 inet dhcp

     

    back in there. I have it there while my 'pi has wlan as well.

     

    Try "lsusb" to see the brand of your wlan chipset.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to rew

    [q] Try "lsusb" to see the brand of your wlan chipset. [/q]

     

    Will Do.  Away for weekend but will try to do some raspberry pi testing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to wallarug

    I can now confirm that it is a RALINK w/lan card (Ralink Technology Corp. RT2870 Wireless Adaptor).  I am going back to the Ralink Drivers now and then seeing what else I can do.  If this can help others to point me in the right direction after installing fireware, that would be much apreciated.

     

    I read a step in a previous post and on the wiki that you need to get "wifi-utils" but I can't seem to be able to install them.  Any help here?

     

    Fergus

     

    PS: Thanks in advanced.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>