I have the debian image which comes with "Midori" which is very slow.
I was wondering if there is a quicking browser for my image.
If so how do I get it?
I have the debian image which comes with "Midori" which is very slow.
I was wondering if there is a quicking browser for my image.
If so how do I get it?
@David: No, I haven't tried NetSurf, nor knew about it. It's not available in Gentoo's Portage, but I'll grab the sources and build it longhand on my main machines:
As indicated in coder27's linked item, obtaining NetSurf on Pi under Raspbian should be a simple matter of
This doesn't work on my plain Debian install though, as "apt-cache search netsurf" finds various GIF and BMP decoder libraries but no "netsurf-gtk" browser, even after an apt-get update. I expect that Debian just needs to be told about the Raspbian package repository (assuming the two repos are compatible), which I haven't looked into yet.
Thanks to coder27 and yourself for mentioning it. 
Morgaine.
I found a description of the Debian repo issues on the Raspbian site, specifically:
Short version: Raspbian uses armhf (Hard Float) architecture in contrast to the standard Debian ARM distro's armel which is soft float. In general, you can't install any old package from an armhf system into an armel one and expect it to work. There is a tool script "v7clean" that allows you to check whether a Raspbian package is armel compatible.
I haven't checked netsurf-gtk with v7clean yet.
Morgaine.
Morgaine,
I think you may be misunderstanding what v7clean does.
My understanding is that it predicts whether object code
will run on raspbian, that is, it doesn't use any v7-only instructions.
It doesn't predict whether raspbian code will run on armel.
That's not what the code says, coder27. I've got it here and the description is quite clear:
v7clean (from http://pastebin.com/BtSdvrXM ) says:
v7clean -- script to verify that a .deb and .udeb files are clean from armv7 code using the 'readelf' Linux utility.
Standard Debian on ARM is armv6l, so it must not have any ARMv7 instructions in it or it won't run. The script checks the number of files containing v6 and v7 instructions, and if the v7 count is greater than zero, it outputs "v7_dirty", which means that the package won't run on arv6l.
I still think you're confused. The raspbian guys are pulling code
from the debian v7 distro, and compiling for RPi (with different
compilation flags), and wrote the v7clean script to warn them when
that won't work due to v7-specific op codes. They aren't concerned
about whether code from their raspbian distro will work on a soft-float
armel v6 version of debian, since they don't expect that to work due to
abi differences.
Interestingly, I've extended my copy of the script a little to show the actual CPU architecture tags for each file processed by readelf, and it shows that every .deb I've installed so far has ARM architecture v4T.
That's positively antique, it's the architecture implemented on the ARM922T which predates even Pi's ARM11.
coder27 wrote:
I still think you're confused. The raspbian guys are pulling code
from the debian v7 distro, and compiling for RPi (with different
compilation flags), and wrote the v7clean script to warn them when
that won't work due to v7-specific op codes. They aren't concerned
about whether code from their raspbian distro will work on a soft-float
armel v6 version of debian, since they don't expect that to work due to
abi differences.
Heh, I think you need to read the code a bit, it's very helpful to explain what's going on. 
The '6' and '7' have nothing to do with Debian v6 or v7. It's the ARM architecture:
New architectures can often execute old instruction sets (it depends entirely on chosen core options), but old architectures can't execute newer instruction sets because ... well, because they're not clairvoyant. 
Anyway, the v7clean tool checks which instruction set a package's files were compiled for, nothing else. You can use that information in many ways, it's just a low-level information tool. Its name "v7clean" suggests that absence of ARMv7 arch tags was the desired property.
Presumably the Raspbian guys and gals are using it to check that their build is clean and hasn't accidentally pulled in libraries that were compiled for the wrong architecture --- for example (I'm guessing) they could be cross-compiling on a Pandaboard for ARMv6, but the Pandaboard is natively ARMv7 (Cortex-A8) so its native libraries are ARMv7 and they need to check that those haven't accidentally leaked in to their build. While I don't know exactly what Raspbian are doing, I do know what the script does so it's straightforward to see how it can be used.
In our case it can be used similarly to determine whether a compiled package out there somewhere in the world of .deb repos will run on Pi, since ARMv7 instructions won't run on our ARM1176.
Morgaine.
> The '6' and '7' have nothing to do with Debian v6 or v7. It's the ARM architecture:
agreed. didn't mean to imply otherwise.
>In our case it can be used similarly to determine whether a compiled package out there somewhere in the world of .deb repos will run on Pi, since ARMv7 instructions won't run on our ARM1176.
I think you also need to worry about the abi, and v7clean doesn't report that.
I don't think raspbian-built packages will generally run on RPi debian distros
even if v7clean shows no problems.
coder27 wrote:
I think you also need to worry about the abi, and v7clean doesn't report that.
I don't think raspbian-built packages will generally run on RPi debian distros
even if v7clean shows no problems.
Yep, you're probably right there.
This is all good stuff, Pi is helping to fill out our knowledge of ARM nicely. If the board wasn't using such an antiquated ARM core, we could be installing any Debian package that runs on the millions of Cortex-A8 smartphones and tablets and i.M53 QSBs and Beagleboards and Pandaboard development machines out there, and learn nothing at all about antique ARM instruction sets.
not to mention that a v7 ARM could run Ubuntu, Android, etc.
It seems the processor was selected a long time ago, when
it was supported by Ubuntu, but the world has moved on.
I think the RPi name was selected, the rpi.org domain acquired,
and Pete Lomas brought on board, all in Sept 2008; then the
foundation was founded in November 2008 and registered
in May 2009, but it took several years to bring to fruition.