Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum What other browsers work on RPi?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 711 subscribers
  • Views 4720 views
  • Users 0 members are here
Related

What other browsers work on RPi?

wallarug
wallarug over 14 years ago

I have the debian image which comes with "Midori" which is very slow.

 

I was wondering if there is a quicking browser for my image.

 

If so how do I get it?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    one other browser is NetSurf.

    The raspbian guys are saying good things about it.

     

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=66&t=8438&start=28

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to e14 Contributor

    A big thanks for the tip!  I tried out a couple images last weekend and used NetSurf.  It's a breath of fresh air indeed.  No JS means some sites don't function correctly (like this one, oy) but it is so much better than trying to interpret pages as pure text in lynx or pulling out my hair waiting for midori to load pages.

     

    Thanks!

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to fustini

    Midori is one of many (over half a dozen) lightweight browsers all based on webkit.  Most of them have a single-page paradigm, but a few support tabs as well --- Midori and Uzbl-tabbed are the best known for that.

     

    If Midori is giving you trouble, you might want to try some of the others.  I only care about open source ones, and of those, the ones I use occasionally other than Midori are:

     

    • Uzbl http://www.uzbl.org (come in three varieties, one of them tabbed)
    • LuaKit http://www.luakit.org
    • Jumanji http://pwmt.org/projects/jumanji
    • Surf http://surf.suckless.org/

     

    Of those, only LuaKit gets any significant use here.  Other similar lightweight browsers that I haven't tried personally but are also open source are:

     

    • Qupzilla http://www.qupzilla.com/
    • Arora http://code.google.com/p/arora/

     

    which don't appear to be available in Gentoo's Portage which may indicate that they have problems, or simply that they are new.  There's certainly no shortage of alternatives if Midori doesn't fit the bill.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Montala
    Montala over 14 years ago in reply to morgaine

    Have you tried NetSurf (which coder27 mentioned earlier) Morgaine, and if so what do you think of it?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to Montala

    @David: No, I haven't tried NetSurf, nor knew about it.  It's not available in Gentoo's Portage, but I'll grab the sources and build it longhand on my main machines:

     

    • NetSurf - http://www.netsurf-browser.org/

     

    As indicated in coder27's linked item, obtaining NetSurf on Pi under Raspbian should be a simple matter of

     

    • apt-get install netsurf-gtk

     

    This doesn't work on my plain Debian install though, as "apt-cache search netsurf" finds various GIF and BMP decoder libraries but no "netsurf-gtk" browser, even after an apt-get update.  I expect that Debian just needs to be told about the Raspbian package repository (assuming the two repos are compatible), which I haven't looked into yet.

     

    Thanks to coder27 and yourself for mentioning it. image

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to morgaine

    I found a description of the Debian repo issues on the Raspbian site, specifically:

     

    • http://www.raspbian.org/RaspbianFAQ#Can_I_mix_packages_from_the_Debian_repositories_with_Raspbian.3F
    • http://www.raspbian.org/RaspbianFAQ#What_do_I_need_in_my_sources.list_file_to_access_the_Raspbian_repository.3F

     

    Short version:  Raspbian uses armhf (Hard Float) architecture in contrast to the standard Debian ARM distro's armel which is soft float.  In general, you can't install any old package from an armhf system into an armel one and expect it to work.  There is a tool script "v7clean" that allows you to check whether a Raspbian package is armel compatible.

     

    I haven't checked netsurf-gtk with v7clean yet.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Morgaine,

      I think you may be misunderstanding what v7clean does.

    My understanding is that it predicts whether object code

    will run on raspbian, that is, it doesn't use any v7-only instructions.

    It doesn't predict whether raspbian code will run on armel.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    That's not what the code says, coder27.  I've got it here and the description is quite clear:

     

    v7clean (from http://pastebin.com/BtSdvrXM ) says:

     

    v7clean -- script to verify that a .deb and .udeb files are clean from armv7 code using the 'readelf' Linux utility.

     

    Standard Debian on ARM is armv6l, so it must not have any ARMv7 instructions in it or it won't run.  The script checks the number of files containing v6 and v7 instructions, and if the v7 count is greater than zero, it outputs "v7_dirty", which means that the package won't run on arv6l.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    I still think you're confused.  The raspbian guys are pulling code

    from the debian v7 distro, and compiling for RPi (with different

    compilation flags), and wrote the v7clean script to warn them when

    that won't work due to v7-specific op codes.  They aren't concerned

    about whether code from their raspbian distro will work on a soft-float

    armel v6 version of debian, since they don't expect that to work due to

    abi differences.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to morgaine

    Interestingly, I've extended my copy of the script a little to show the actual CPU architecture tags for each file processed by readelf, and it shows that every .deb I've installed so far has ARM architecture v4T.

     

    That's positively antique, it's the architecture implemented on the ARM922T which predates even Pi's ARM11.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    coder27 wrote:

     

    I still think you're confused.  The raspbian guys are pulling code

    from the debian v7 distro, and compiling for RPi (with different

    compilation flags), and wrote the v7clean script to warn them when

    that won't work due to v7-specific op codes.  They aren't concerned

    about whether code from their raspbian distro will work on a soft-float

    armel v6 version of debian, since they don't expect that to work due to

    abi differences.

     

    Heh, I think you need to read the code a bit, it's very helpful to explain what's going on.  image

     

    The '6' and '7' have nothing to do with Debian v6 or v7.  It's the ARM architecture:

     

    • ARMv4T as used in ARM922T and also accepted by Pi's ARM1176
    • ARMv6 which is native to ARM11 and is also used in Cortex-M0
    • ARMv7 as used in modern ARM CPUs like Cortex-M1/M3/M4/A8/9/15 (does not include Cortex-M0).

     

    New architectures can often execute old instruction sets (it depends entirely on chosen core options), but old architectures can't execute newer instruction sets because ... well, because they're not clairvoyant. image

     

    Anyway, the v7clean tool checks which instruction set a package's files were compiled for, nothing else. You can use that information in many ways, it's just a low-level information tool.  Its name "v7clean" suggests that absence of ARMv7 arch tags was the desired property.

     

    Presumably the Raspbian guys and gals are using it to check that their build is clean and hasn't accidentally pulled in libraries that were compiled for the wrong architecture --- for example (I'm guessing) they could be cross-compiling on a Pandaboard for ARMv6, but the Pandaboard is natively ARMv7 (Cortex-A8) so its native libraries are ARMv7 and they need to check that those haven't accidentally leaked in to their build.  While I don't know exactly what Raspbian are doing, I do know what the script does so it's straightforward to see how it can be used.

     

    In our case it can be used similarly to determine whether a compiled package out there somewhere in the world of .deb repos will run on Pi, since ARMv7 instructions won't run on our ARM1176.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    coder27 wrote:

     

    I still think you're confused.  The raspbian guys are pulling code

    from the debian v7 distro, and compiling for RPi (with different

    compilation flags), and wrote the v7clean script to warn them when

    that won't work due to v7-specific op codes.  They aren't concerned

    about whether code from their raspbian distro will work on a soft-float

    armel v6 version of debian, since they don't expect that to work due to

    abi differences.

     

    Heh, I think you need to read the code a bit, it's very helpful to explain what's going on.  image

     

    The '6' and '7' have nothing to do with Debian v6 or v7.  It's the ARM architecture:

     

    • ARMv4T as used in ARM922T and also accepted by Pi's ARM1176
    • ARMv6 which is native to ARM11 and is also used in Cortex-M0
    • ARMv7 as used in modern ARM CPUs like Cortex-M1/M3/M4/A8/9/15 (does not include Cortex-M0).

     

    New architectures can often execute old instruction sets (it depends entirely on chosen core options), but old architectures can't execute newer instruction sets because ... well, because they're not clairvoyant. image

     

    Anyway, the v7clean tool checks which instruction set a package's files were compiled for, nothing else. You can use that information in many ways, it's just a low-level information tool.  Its name "v7clean" suggests that absence of ARMv7 arch tags was the desired property.

     

    Presumably the Raspbian guys and gals are using it to check that their build is clean and hasn't accidentally pulled in libraries that were compiled for the wrong architecture --- for example (I'm guessing) they could be cross-compiling on a Pandaboard for ARMv6, but the Pandaboard is natively ARMv7 (Cortex-A8) so its native libraries are ARMv7 and they need to check that those haven't accidentally leaked in to their build.  While I don't know exactly what Raspbian are doing, I do know what the script does so it's straightforward to see how it can be used.

     

    In our case it can be used similarly to determine whether a compiled package out there somewhere in the world of .deb repos will run on Pi, since ARMv7 instructions won't run on our ARM1176.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    > The '6' and '7' have nothing to do with Debian v6 or v7.  It's the ARM architecture:

     

    agreed.  didn't mean to imply otherwise.

     

    >In our case it can be used similarly to determine whether a compiled package out there somewhere in the world of .deb repos will run on Pi, since ARMv7 instructions won't run on our ARM1176.

     

    I think you also need to worry about the abi, and v7clean doesn't report that.

    I don't think raspbian-built packages will generally run on RPi debian distros

    even if v7clean shows no problems.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    coder27 wrote:

     

    I think you also need to worry about the abi, and v7clean doesn't report that.

    I don't think raspbian-built packages will generally run on RPi debian distros

    even if v7clean shows no problems.

     

    Yep, you're probably right there.

     

    This is all good stuff, Pi is helping to fill out our knowledge of ARM nicely.  If the board wasn't using such an antiquated ARM core, we could be installing any Debian package that runs on the millions of Cortex-A8 smartphones and tablets and i.M53 QSBs and Beagleboards and Pandaboard development machines out there, and learn nothing at all about antique ARM instruction sets.

     

    A glass-half-full "benefit" if there ever was one .... image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    not to mention that a v7 ARM could run Ubuntu, Android, etc.

     

    It seems the processor was selected a long time ago, when

    it was supported by Ubuntu, but the world has moved on.

     

    I think the RPi name was selected, the rpi.org domain acquired,

    and Pete Lomas brought on board, all in Sept 2008; then the

    foundation was founded in November 2008 and registered

    in May 2009, but it took several years to bring to fruition.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    It's notable that Broadcom hasn't helped in that regard.  Modern versions of VideoCore 4 use Cortex-A9 dual-core CPUs, so Raspberry Pi could have been a modern computer board if Broadcom had had the will and flexibility.  Broadcom is Beancounters Consolidated though, so that was never going to happen.

     

    Maybe some day in the future if Pi goes into education everywhere and Broadcom can forecast sales of hundreds of millions ... it'll be too late by then though, because every ARM licensee under the sun will be there long before, and Pi is after all "just an ARM Linux box" as we are repeatedly told.  Broadcom is easily replaceable.