Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Lowest cost ARM + Arduino headers expansion for Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 709 subscribers
  • Views 4934 views
  • Users 0 members are here
  • raspberry_pi
Related

Lowest cost ARM + Arduino headers expansion for Pi

morgaine
morgaine over 14 years ago

As Eben Upton has often said, Arduino and Raspberry Pi don't really compete significantly because they're so different (maybe just 10% overlap).  They should instead be regarded as complementary.  When the rather meagre hardware interfacing of the Pi is not enough for your project, combining an Arduino with your Pi will often provide a very effective mix of extensive low-level interfacing and high-level programmability.

 

However,  traditional Arduino boards are based on 8-bit microcontrollers, and although these are perfect for a huge range of applications, there are times when it is desireable to use an ARM microcontroller when interfacing with the Pi's ARM1176, and not only for ARM symmetry.  Some things are simply easier to do with a 32-bit processor, and if processing speed matters in your application then an ARM microcontroller will almost always leave the 8-bit micro way behind.

 

Unfortunately your options become somewhat limited if you want to use an ARM microcontroller board yet still want to enjoy the ability to use Arduino "shields", the many hundreds of daughterboards that can plug into an Arduino board's headers and which make Arduino such a singularly impressive ecosystem.  Although the Arduino organization will soon be releasing their own ARM-based Arduino Due using an Atmel SAM3X8E device (a Cortex-M3), it's not officially out yet (despite having been sighted on flickr), and not many third parties have tackled this empty spot in the market.

 

The best known are probably the Maple from LeafLabs http://leaflabs.com/devices/maple/ , and the Olimexino-STM32 from Olimex http://www.olimex.com/dev/olimexino-stm32.html which offers quite a lot more and yet is cheaper (£16.96 from Farnell).  Both are based on an ARM Cortex-M3 from ST, and offer a degree of Arduino header compatibility.

 

Well, this area is about to be given an interesting shakeup, courtesy of yet another ARM licensee, Freescale.  Their Kinetis KL25Z Freedom Board is now on pre-order at Element 14:

 

  • http://www.element14.com/community/community/knode/dev_platforms_kits/element14_dev_kits/kinetis_kl2_freedom_board
  • http://uk.farnell.com/freescale-semiconductor/kl25z128vlk/board-kinetis-l-series-kl25z/dp/2115294?COM=freedompage_knode ,

 

and you really can't go wrong at its board price of £8.10 + Arduino header form factor . image

 

Admittedly the Kinetis KL25Z's KL2 microcontroller is a Cortex-M0 which is the little brother of the Cortex-M3, but for hardware interfacing that will often be more than ample and is still a huge step up from the 8-bit AVR.  What's more, it's highly likely to undercut the price of Arduino's about-to-be-released Arduino Due, so things may get quite interesting in this market niche.

 

[Added note:  the Kinetis KL25Z board uses  uses a Cortex-M0+, not M0  -- see post 16, http://www.element14.com/community/message/54650#54650 ]

 

For expanding the Pi (and the BeagleBone too) into the Arduino niche, the Kinetis KL25Z looks extremely good to me. Admittedly, it won't provide anything like the power of an STM32F4-Discovery board which uses a Cortex-M4  http://uk.farnell.com/stmicroelectronics/stm32f4discovery/board-eval-stm32f4-discovery/dp/2009276?Ntt=STM32F4-Discovery , and at £9.96 from Farnell this Discovery is the very clear price-performance leader.  However, the Kinetis KL25Z has the Arduino form factor, and that may make all the difference.  YMMV !!

 

Very interesting times ahead! image

 

And just in case that isn't tempting enough, ST's Discovery range has a Cortex-M0 version, the STM32F0-Discovery http://uk.farnell.com/stmicroelectronics/stm32f0discovery/eval-board-cortex-m0-stm32f0/dp/2096251?Ntt=STM32F0-Discovery which is even cheaper at £5.88.  If Arduino headers aren't essential but you want the cheapest possible Cortex-M0 board to expand your Pi, beating £5.88 on sheer price will be very hard.  It's fairly safe to predict that the Cortex-M0[+] range is going to have a colossal impact.

 

 

Morgaine.

  • Sign in to reply
  • Cancel
Parents
  • fustini
    fustini over 14 years ago

    Morgaine, I enjoyed your enlightening summary.  I've never used one of those Cortex M series boards before, and you've piqued my interest.  I'd seen news about the new Freescale board, but I didn't realize it was Arduino header compatible until I read your post - very interesting.

     

    The main requirement I would have for trying any of these boards would be Linux compatibility.  I would imagine there is gcc available, but I am interested to check on the IDEs.

     

    Thanks,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to fustini

    Drew Fustini wrote:

     

    The main requirement I would have for trying any of these boards would be Linux compatibility.  I would imagine there is gcc available, but I am interested to check on the IDEs.

     

    Software is definitely the problem in this area, particularly for those who run Linux but want an IDE, which is becoming more common but certainly isn't mainstream.  Although installing an ARM toolchain is very easy and is typically done by running a single command, that's only the start of the process.

     

    Setting up Eclipse, OpenOCD and finding an open debug adapter for cross-development requires a combination of bravery and masochism and a lot of spare time, which is less than ideal. The information is out there and just requires a degree in Googling to find, but it's certainly not "turnkey" to gather all the necessary information together and hook it all up.  It's also a barrier to entry, and has little to do with the end goal.

     

    Hopefully this will improve over the years, but there's little sign of it becoming a turnkey solution yet.  Turnkey solutions do exist for Linux of course (dozens of them!), but alas they employ closed-source IDEs (often derived from Eclipse, ironically) and require approved commercial debuggers.  Pity.  ARM is nowhere near to where Arduino/AVR is in this regard.

     

    Morgaine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to morgaine

    Thanks for the insight.  I'll have to try it to make my way through it one of these days.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fustini
    fustini over 14 years ago in reply to morgaine

    Thanks for the insight.  I'll have to try it to make my way through it one of these days.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • morgaine
    morgaine over 14 years ago in reply to fustini

    Drew Fustini wrote:

     

    I'll have to try it to make my way through it one of these days.

     

    Well let's talk to that other guy, Drew Fustini (Admin). image

     

    When the Kinetis KL25Z Freedom Board appears in stock, we might be able to get him to create an Element 14 group for it, and share the experience of setting up a development environment for that board, discuss interfacing, etc.

     

    There is a generic "Embedded Systems" group already but it mostly just deals with announcements.  I notice that Greg C (apparently from Freescale) has a couple of posts there about their Cortex-M0, but a more focused group would probably be helpful.  Given the extreme low price of that board and its Arduino-style headers, it could become very popular indeed.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to morgaine

    Hahaha, love this Freescale energy efficiency demo --- http://www.youtube.com/watch?v=FfsMCwUjNxw

     

    Last man left alive wins. imageimageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GregC
    GregC over 14 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Well let's talk to that other guy, Drew Fustini (Admin). image

     

    When the Kinetis KL25Z Freedom Board appears in stock, we might be able to get him to create an Element 14 group for it, and share the experience of setting up a development environment for that board, discuss interfacing, etc.

     

    There is a generic "Embedded Systems" group already but it mostly just deals with announcements.  I notice that Greg C (apparently from Freescale) has a couple of posts there about their Cortex-M0, but a more focused group would probably be helpful.  Given the extreme low price of that board and its Arduino-style headers, it could become very popular indeed.

    I fully agree with you concerning the creation of a more focus group to support freedom users would be more efficient.

    I will check with element14 support team if they have already this action in plan (as they did for XL-Star board with some engineer like roy_I to support the users) ... I will keep you in touch

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GregC
    GregC over 14 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Hahaha, love this Freescale energy efficiency demo --- http://www.youtube.com/watch?v=FfsMCwUjNxw

     

    Last man left alive wins. imageimageimage

    Eduardo (application engineer at Freescale) exposed this demo during FTF America June 18-21th

    This video is also available in Embedded Group, blog section HERE

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to morgaine

    good idea, i'll mention it to the content team, too.