Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Lowest cost ARM + Arduino headers expansion for Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 709 subscribers
  • Views 4953 views
  • Users 0 members are here
  • raspberry_pi
Related

Lowest cost ARM + Arduino headers expansion for Pi

morgaine
morgaine over 14 years ago

As Eben Upton has often said, Arduino and Raspberry Pi don't really compete significantly because they're so different (maybe just 10% overlap).  They should instead be regarded as complementary.  When the rather meagre hardware interfacing of the Pi is not enough for your project, combining an Arduino with your Pi will often provide a very effective mix of extensive low-level interfacing and high-level programmability.

 

However,  traditional Arduino boards are based on 8-bit microcontrollers, and although these are perfect for a huge range of applications, there are times when it is desireable to use an ARM microcontroller when interfacing with the Pi's ARM1176, and not only for ARM symmetry.  Some things are simply easier to do with a 32-bit processor, and if processing speed matters in your application then an ARM microcontroller will almost always leave the 8-bit micro way behind.

 

Unfortunately your options become somewhat limited if you want to use an ARM microcontroller board yet still want to enjoy the ability to use Arduino "shields", the many hundreds of daughterboards that can plug into an Arduino board's headers and which make Arduino such a singularly impressive ecosystem.  Although the Arduino organization will soon be releasing their own ARM-based Arduino Due using an Atmel SAM3X8E device (a Cortex-M3), it's not officially out yet (despite having been sighted on flickr), and not many third parties have tackled this empty spot in the market.

 

The best known are probably the Maple from LeafLabs http://leaflabs.com/devices/maple/ , and the Olimexino-STM32 from Olimex http://www.olimex.com/dev/olimexino-stm32.html which offers quite a lot more and yet is cheaper (£16.96 from Farnell).  Both are based on an ARM Cortex-M3 from ST, and offer a degree of Arduino header compatibility.

 

Well, this area is about to be given an interesting shakeup, courtesy of yet another ARM licensee, Freescale.  Their Kinetis KL25Z Freedom Board is now on pre-order at Element 14:

 

  • http://www.element14.com/community/community/knode/dev_platforms_kits/element14_dev_kits/kinetis_kl2_freedom_board
  • http://uk.farnell.com/freescale-semiconductor/kl25z128vlk/board-kinetis-l-series-kl25z/dp/2115294?COM=freedompage_knode ,

 

and you really can't go wrong at its board price of £8.10 + Arduino header form factor . image

 

Admittedly the Kinetis KL25Z's KL2 microcontroller is a Cortex-M0 which is the little brother of the Cortex-M3, but for hardware interfacing that will often be more than ample and is still a huge step up from the 8-bit AVR.  What's more, it's highly likely to undercut the price of Arduino's about-to-be-released Arduino Due, so things may get quite interesting in this market niche.

 

[Added note:  the Kinetis KL25Z board uses  uses a Cortex-M0+, not M0  -- see post 16, http://www.element14.com/community/message/54650#54650 ]

 

For expanding the Pi (and the BeagleBone too) into the Arduino niche, the Kinetis KL25Z looks extremely good to me. Admittedly, it won't provide anything like the power of an STM32F4-Discovery board which uses a Cortex-M4  http://uk.farnell.com/stmicroelectronics/stm32f4discovery/board-eval-stm32f4-discovery/dp/2009276?Ntt=STM32F4-Discovery , and at £9.96 from Farnell this Discovery is the very clear price-performance leader.  However, the Kinetis KL25Z has the Arduino form factor, and that may make all the difference.  YMMV !!

 

Very interesting times ahead! image

 

And just in case that isn't tempting enough, ST's Discovery range has a Cortex-M0 version, the STM32F0-Discovery http://uk.farnell.com/stmicroelectronics/stm32f0discovery/eval-board-cortex-m0-stm32f0/dp/2096251?Ntt=STM32F0-Discovery which is even cheaper at £5.88.  If Arduino headers aren't essential but you want the cheapest possible Cortex-M0 board to expand your Pi, beating £5.88 on sheer price will be very hard.  It's fairly safe to predict that the Cortex-M0[+] range is going to have a colossal impact.

 

 

Morgaine.

  • Sign in to reply
  • Cancel
  • morgaine
    morgaine over 14 years ago in reply to GregC

    Greg C wrote:

     

    In addition, Freescale offer for FREE its own IDE CodeWarrior (with code-size limitations up to 128KB)

     

    No sign of the CodeWarrior special edition for Kinetis KL25 in the downloads section yet.  I'm looking foreward to trying the Linux version when it appears.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GregC
    GregC over 14 years ago in reply to fustini

    Drew Fustini wrote:

     

    The main requirement I would have for trying any of these boards would be Linux compatibility.

    I need to investigate concerning the other IDE supplier, but I have first in mind that CodeWarrior is available for Windows and Linux platform and should be released in September to support Kinetis-L KL family (now just Kinetis-K with M4 is supported by v10.2).

    I have copied below an extract from this topic, I just posted concerning Kinetis-K (Cortex-M4) available tools.

    Just consider that code size limitations for IDE in evaluation versions are/will be lower with Cortex-M0 and M0+ than M3 and M4.

     

    FREESCALE CODEWARRIOR Development Studio for Microcontrollers (Eclipse IDE, Windows and Linux Hosted)

    http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10&nodeId=0152102726E4C7E4CB

    Freescale’s CodeWarrior for Microcontrollers v10.2 integrates the development tools for the ColdFireRegistered, ColdFire+, DSC, Kinetis, Qorivva, PX, RS08 and S08 into a single product based on the Eclipse open development platform.

    Eclipse offers an excellent framework for building software development environments and is becoming a standard framework used by many embedded software vendors.

    Compatible with : RS08, S08, S12Z, ColdFireRegistered, ColdFire+, DSC, Kinetis, Qorivva and PX

    Free  FREESCALE CodeWarrior Development Studio for Microcontrollers V10.2 editions
    available in 30-day evaluation (Windows or Linux hosted) or Special 128KB Kinetis (Windows or Linux hosted)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GregC
    GregC over 14 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Well let's talk to that other guy, Drew Fustini (Admin). image

     

    When the Kinetis KL25Z Freedom Board appears in stock, we might be able to get him to create an Element 14 group for it, and share the experience of setting up a development environment for that board, discuss interfacing, etc.

     

    There is a generic "Embedded Systems" group already but it mostly just deals with announcements.  I notice that Greg C (apparently from Freescale) has a couple of posts there about their Cortex-M0, but a more focused group would probably be helpful.  Given the extreme low price of that board and its Arduino-style headers, it could become very popular indeed.

    I fully agree with you concerning the creation of a more focus group to support freedom users would be more efficient.

    I will check with element14 support team if they have already this action in plan (as they did for XL-Star board with some engineer like roy_I to support the users) ... I will keep you in touch

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GregC
    GregC over 14 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Hahaha, love this Freescale energy efficiency demo --- http://www.youtube.com/watch?v=FfsMCwUjNxw

     

    Last man left alive wins. imageimageimage

    Eduardo (application engineer at Freescale) exposed this demo during FTF America June 18-21th

    This video is also available in Embedded Group, blog section HERE

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GregC
    GregC over 14 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Apparerently the illustration for the Kinetis KL25Z Freedom Board shown at the Farnell ordering link I gave is wrong,  Element 14's knode page shows it more accurately ---

     

    • http://www.element14.com/community/community/knode/dev_platforms_kits/element14_dev_kits/kinetis_kl2_freedom_board

     

    You can read "Freedom KL25Z" there on expanded images of the board, which inspires confidence that it's the right picture.

     

    Still no sign of a proper board document though, nor a real datasheet for the KL25Z128VLK4 processor on it, just general KL24/KL25 product briefs.

     

    I take the hard engineering line on this:  no datasheet == vapourware. image

     

    Documentation (Reference Manual or Datasheet) from Freedom board should be available in max 2 weeks as it is still in examination.

     

    I would like just highlight some interesting features from KL25 silicon illustrated with the bloc diagram found in its product brief

    - Analog to Digital Converter with a resolution up to 16-bit

    - Touch Sensor Interface

    - RTC

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to GregC

    Expanding on my first post, after being prompted by Greg -- thanks! image

     

    It's worth pointing out that the ARM on the Freescale KL25Z128VLK4 device is correctly termed a Cortex-M0+ and not a Cortex-M0 at all.  And no, this is not just Marketting inventing a new term for a brochure (as one might cynically expect), but an official redesigned ARM core.  This caught me out initially, as I hadn't realized that ARM had officially released a new M0+ core as an improvement over their M0, but they have.  The info from ARM is here --- http://www.arm.com/products/processors/cortex-m/cortex-m0plus.php

     

    This seems like a very nice little device, and I'm really looking forward to using it, both with Pi and standalone. image

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to morgaine

    good idea, i'll mention it to the content team, too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to GregC

    Thanks, that's encouraging to know.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago

    image

     

    I'm not sure what communication channels exist between Element 14 admins and Farnell product store admins, but if the means are available, it would probably be a good idea to put a thumbnail of this clear picture of the Freedom KL25Z in place of the image they're using "for illustrative purposes only" at http://uk.farnell.com/freescale-semiconductor/freedom-kl25z/board-kinetis-l-series-kl25z/dp/2115294?Ntt=2115294 (assuming that this is similar to the final one of course, which seems likely).

     

    It's probably confusing a lot of people that the store image is so dramatically different (a prototype?) from the end product. image

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to morgaine

    Yay, somebody did update the Farnell store product image, and with a nice angle shot of the board.

     

    Well done, unknown admin! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>