Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Can I connect Pi to a VGA monitor ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 24 replies
  • Subscribers 711 subscribers
  • Views 8877 views
  • Users 0 members are here
  • video
  • raspberry_pi
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Can I connect Pi to a VGA monitor ?

mgt6910
mgt6910 over 14 years ago

I don't have a HD monitor (the TV is out of bounds....), so can I connect the Pi's  RCA  or DVI output to

a VGA screen via an adaptor ?   I've found this RCA/VGA converter, but it is designed to work in the other direction ..

 

http://www.amazon.co.uk/S-VIDEO-ADAPTER-CONVERTER-CABLE-LAPTOP/dp/B000P3UB24/ref=pd_sim_ce_1

  • Cancel
Parents
  • johnbeetem
    johnbeetem over 14 years ago

    Some Razzers have reported success with HDMI to VGA adapters.  You need more than just a cable: the adapter must have ICs to convert digital HDMI to analog VGA.  They generally cost more than the RasPi, but probably less than a new monitor.  Some verified peripherals are listed here: http://elinux.org/RPi_VerifiedPeripherals#Display_adapters.  There are also some listed here which "should" work: http://elinux.org/Rpi_Screens.  You can find discussion about this at raspberrypi.org.  Search for "HDMI to VGA" in the Google Search box on the home page.  Searching for VGA in the Forum search is a problem because it requires keywords to be longer than 3 characters.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • mgt6910
    mgt6910 over 14 years ago in reply to johnbeetem

    Many thanks for the clarification, I have ordered a DVI/VGA converter, only half the cost of the Pi.  I plan (medium/long term) on giving a Pi to each of my 2 grandsons, and recycling my old VGA-monitors as part of the bundle.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to mgt6910

    I'm afraid you will find the cheap DVI/VGA converters useless for the task. They are merely socket adaptors, all they do is pass through the analogue signal that is available on the DVI-I connectors present on many graphics cards. It's still the graphics card that is generating the analog VGA signal. This is not present on HDMI output of the Pi, so going HDMI - DVI - VGA won't work.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • mgt6910
    mgt6910 over 14 years ago in reply to e14 Contributor

    My mistake, my converter does not have a DVI stage. I ordered the Neewer unit after taking advice from :

     

    http://elinux.org/RPi_VerifiedPeripherals#HDMI-.3EVGA_converter_boxes

     

    According to user "asb" -- http://www.amazon.co.uk/gp/product/B007KEIRNG -- the Neewer HDMI to VGA adapter works with the Pi.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to mgt6910

    That looks like a handy little device, not seen one so cheap before!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to mgt6910

    Malcolm Turner wrote:

     

    My mistake, my converter does not have a DVI stage. I ordered the Neewer unit after taking advice from :

     

    http://elinux.org/RPi_VerifiedPeripherals#HDMI-.3EVGA_converter_boxes

     

    According to user "asb" -- http://www.amazon.co.uk/gp/product/B007KEIRNG -- the Neewer HDMI to VGA adapter works with the Pi.

    There may be a problem with the Neewer unit.  One user at the RasPi forum reported that hooking up that unit to his RasPi burned out BAT54 diode D1.  (Awww... you let the magic smoke out.)  However, the RasPi didn't have any other damage.  See http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=9819

     

    It's not clear whether Tom1989's particular Neewer had an internal short or just drew more than 200 mA from RasPi and burned out D1, which is only rated for 200 mA.  gritz suggested that the successful Amazon user's D1 may have failed as a short circuit without release of magic smoke, which makes it work with the Neewer but the RasPi loses D1's protection when plugging directly into an HDMI monitor.

     

    mahjongg suggested that an HDMI -> VGA converter with its own power supply is safer.

     

    EDIT: mahjongg has suggested the NXP (or equivalent) PMEG2010AET,215PMEG2010AET,215 as a high-current replacement for Schottky diode BAT54.  The PMEG2010AET,215PMEG2010AET,215 has 1A max forward current.  Remember that the HDMI -> VGA converter current must come from your RasPi power supply and go through the Micro USB cable and polyfuse F3, so you may get extra voltage drops and/or cause F3 to trip.  As always with board modifications, YMMV.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 14 years ago in reply to mgt6910

    Malcolm Turner wrote:

     

    My mistake, my converter does not have a DVI stage. I ordered the Neewer unit after taking advice from :

     

    http://elinux.org/RPi_VerifiedPeripherals#HDMI-.3EVGA_converter_boxes

     

    According to user "asb" -- http://www.amazon.co.uk/gp/product/B007KEIRNG -- the Neewer HDMI to VGA adapter works with the Pi.

    There may be a problem with the Neewer unit.  One user at the RasPi forum reported that hooking up that unit to his RasPi burned out BAT54 diode D1.  (Awww... you let the magic smoke out.)  However, the RasPi didn't have any other damage.  See http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=9819

     

    It's not clear whether Tom1989's particular Neewer had an internal short or just drew more than 200 mA from RasPi and burned out D1, which is only rated for 200 mA.  gritz suggested that the successful Amazon user's D1 may have failed as a short circuit without release of magic smoke, which makes it work with the Neewer but the RasPi loses D1's protection when plugging directly into an HDMI monitor.

     

    mahjongg suggested that an HDMI -> VGA converter with its own power supply is safer.

     

    EDIT: mahjongg has suggested the NXP (or equivalent) PMEG2010AET,215PMEG2010AET,215 as a high-current replacement for Schottky diode BAT54.  The PMEG2010AET,215PMEG2010AET,215 has 1A max forward current.  Remember that the HDMI -> VGA converter current must come from your RasPi power supply and go through the Micro USB cable and polyfuse F3, so you may get extra voltage drops and/or cause F3 to trip.  As always with board modifications, YMMV.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • mgt6910
    mgt6910 over 14 years ago in reply to johnbeetem

    Yes I've seen the report. It looks like 1 failure and several successes with the neewer uinit.  I'll

    report my result soonest (Amazon purchase, via a UK address..........)