Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Does anyone know what USB plug power for RaspberryPi?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 707 subscribers
  • Views 1214 views
  • Users 0 members are here
  • raspberry_pi
Related

Does anyone know what USB plug power for RaspberryPi?

e14 Contributor
e14 Contributor over 14 years ago

There must be about a dozen USB Mini connector types out there and this does not seem to be a common connector to use...

 

I've got 3 types of Mini USB connectors and neither one fits!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    You'll need a micro USB connector. A lot of Androids have it, Samsungs and HTCs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Are they an exact match for the USB connector for the RaspberryPi??????

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    The power connector that you plug into the Pi has to be a micro-USB male connector (ie. plug).  An example is shown on the far left of this Wikipedia picture:

     

    http://upload.wikimedia.org/wikipedia/commons/thumb/d/d6/Usb_connectors.JPG/800px-Usb_connectors.JPG

     

    From http://upload.wikimedia.org/wikipedia/commons/thumb/d/d6/Usb_connectors.JPG/800px-Usb_connectors.JPG , see also http://en.wikipedia.org/wiki/File:Usb_connectors.JPG , http://en.wikipedia.org/wiki/Universal_Serial_Bus

     

    The majority of cellphone chargers have a flying lead that terminates in such a micro-USB connector, and are therefore physically compatible with the Pi.  However, that is not true of all cellphone chargers, and nor does it mean that all cellphone chargers terminating in a micro-USB male connector are compatible with the Pi.  One important consideration is that they need to be able to deliver roughly 700mA (0.7 A) within the rated +5V USB supply voltage limits, and it is not uncommon that they cannot do so.

     

    If you are inexperienced in electronics or computers, it's probably best to check the information at the eLinux.org Pi site -- http://elinux.org/RaspberryPiBoard -- and pick a charger from among those that other people have found to work.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    "Are they an exact match for the USB connector for the RaspberryPi??????"

    The Androids are, yes. But if you're worried, don't be. If they don't fit, you won't get them fitting either. Just be sure it powers around 700 mA (0.7A), or even better, around 1A (that way you'll be sure it can handle everything) at 5 volts.

    Also note that Amperes can't really break your Pi. See it as... cookies. 1A compared against 0.7A means you'll give your Pi more cookies, but it'll always eat just the right amount of cookies. But giving more than 5 volts (or less) will make the cookies... "poisoned".

     

    Good luck!

     

    - Wouter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    "Are they an exact match for the USB connector for the RaspberryPi??????"

    The Androids are, yes. But if you're worried, don't be. If they don't fit, you won't get them fitting either. Just be sure it powers around 700 mA (0.7A), or even better, around 1A (that way you'll be sure it can handle everything) at 5 volts.

    Also note that Amperes can't really break your Pi. See it as... cookies. 1A compared against 0.7A means you'll give your Pi more cookies, but it'll always eat just the right amount of cookies. But giving more than 5 volts (or less) will make the cookies... "poisoned".

     

    Good luck!

     

    - Wouter