Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum USB powered hub to power the Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 706 subscribers
  • Views 670 views
  • Users 0 members are here
  • raspberry
  • usb_hub
  • raspberry_pi
Related

USB powered hub to power the Pi

recantha
recantha over 14 years ago

Hi all.

I know there's a Wiki with a list of peripherals, both working and non-working, but I'm finding it difficult to tell which one has which capabilities.

 

Ideally, what I'd like is to have a powered 7-port USB hub into which I can plug a USB-to-micro-USB cable to power the Pi itself. I'm aiming to get my 'system' so that I do not need yet another mains cable for the Pi itself.

 

Has anyone had any experience or heard of anyone who has managed to get it working?

 

Here's hoping! :-)

 

--

Mike Horne

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 14 years ago

    I have that working pretty well with a 4-port Inland powered hub, which I got as a US$5 special from Fry's years ago.  My hub has a Schottky diode in the upstream USB cable which makes sure the hub doesn't try to power RasPi through its USB A ports.  Also, my hub just connects all the downstream +5V signals together so there's no current limiting (other than wires and PC board traces).  A smart hub might have slow-start current control and not provide adequate current to RasPi.  I don't know how to tell what a candidate hub is going to do looking at a web page for it.  I found out what my Inland does by taking it apart and playing with an Ohmmeter.

     

    The main problem I have with my set-up is that the Inland hub has a 3.5 mm barrel power jack, and it doesn't always make good contact.  I found out recently that barrel connectors are iffy: the outer conductor has good wiping contact, but the inner pin of the jack has only casual contact with the plug.  You can get a high-current version of a 5.5 mm barrel plug with wiping inner contacts, but I haven't found such a thing for 3.5 mm.

     

    Currently I'm running at 4.65V on my RasPi (if the 3.5 mm jack is conducting well), which happens to work OK with my peripherals but doesn't leave any margin.  My planned solution is to solder power wires directly to my RasPi with a real SMT fuse instead of polyfuse F3.  With that I expect to get 4.8V or more since I'm not getting drops across my 3.5 mm power jack, micro USB cable, and polyfuse F3.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 14 years ago

    I have that working pretty well with a 4-port Inland powered hub, which I got as a US$5 special from Fry's years ago.  My hub has a Schottky diode in the upstream USB cable which makes sure the hub doesn't try to power RasPi through its USB A ports.  Also, my hub just connects all the downstream +5V signals together so there's no current limiting (other than wires and PC board traces).  A smart hub might have slow-start current control and not provide adequate current to RasPi.  I don't know how to tell what a candidate hub is going to do looking at a web page for it.  I found out what my Inland does by taking it apart and playing with an Ohmmeter.

     

    The main problem I have with my set-up is that the Inland hub has a 3.5 mm barrel power jack, and it doesn't always make good contact.  I found out recently that barrel connectors are iffy: the outer conductor has good wiping contact, but the inner pin of the jack has only casual contact with the plug.  You can get a high-current version of a 5.5 mm barrel plug with wiping inner contacts, but I haven't found such a thing for 3.5 mm.

     

    Currently I'm running at 4.65V on my RasPi (if the 3.5 mm jack is conducting well), which happens to work OK with my peripherals but doesn't leave any margin.  My planned solution is to solder power wires directly to my RasPi with a real SMT fuse instead of polyfuse F3.  With that I expect to get 4.8V or more since I'm not getting drops across my 3.5 mm power jack, micro USB cable, and polyfuse F3.