Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi HDMI problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 704 subscribers
  • Views 1351 views
  • Users 0 members are here
  • raspberry
  • pi
  • hdmi
  • raspberry_pi
  • raspberrypi
Related

Raspberry Pi HDMI problem

e14 Contributor
e14 Contributor over 14 years ago

Hi , I cant run the Pi through the hdmi port, It worked a couple of times but since then I have bought new leads a re-flashed the sd card.

any advice anyone is able to give me would be greatly appreciated

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 14 years ago

    A good place to start for any problem is the RasPi Wiki Troubleshooting page.

     

    If you downloaded a different image from before, the new image may have different requiremens for config.txt, or something regressed between versions.

     

    Since you changed leads, I recommend checking for power supply problems.  If you replaced the Micro USB cable, it may be that the new cable has a higher voltage drop.  Check that TP1-TP2 is in the correct range (there's information on this at the Troubleshooting page, which also points to useful information on the RasPi Wiki Hardware page).  On my RasPi, my DVI-D monitor blanks out if TP1-TP2 goes too low.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 14 years ago

    A good place to start for any problem is the RasPi Wiki Troubleshooting page.

     

    If you downloaded a different image from before, the new image may have different requiremens for config.txt, or something regressed between versions.

     

    Since you changed leads, I recommend checking for power supply problems.  If you replaced the Micro USB cable, it may be that the new cable has a higher voltage drop.  Check that TP1-TP2 is in the correct range (there's information on this at the Troubleshooting page, which also points to useful information on the RasPi Wiki Hardware page).  On my RasPi, my DVI-D monitor blanks out if TP1-TP2 goes too low.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • wallarug
    wallarug over 14 years ago in reply to johnbeetem

    Read my posts on: http://www.element14.com/community/thread/18205?tstart=0 This fixed my problem and might fix yours.

     

    All fixed (audio + resolution)

    Instuctions for others who may be experiencing the same issue with a TV and the Raspberry Pi:

    1. Install a fresh image (optional)

    2. start-up the Raspberry Pi and let it set itself up (normal set-up) - only on first boot

    3. After you have gone through normal set-up:

    a. Log-in as a normal user (debian image: pi)

    b. Type the command: "sudo nano /boot/config.txt "

    c. Press enter

    d. Type in: "hdmi_drive=2 " [exactly as it is here]

    e. Then press crtl + o

    f. Press Enter

    g. then press crtl + x

    4. Restart using the command: " sudo shutdown -r now "

     

    That gets the Raspberry Pi to register the TV as a HDMI device. You now have sound! For different resolution:

    5. After you have gone through normal set-up:

    a. Log-in as a normal user (debian image: pi)

    b. Type the command: "sudo nano /boot/config.txt "

    c. Press enter

    d. Type in: "hdmi_group=1 " [exactly as it is here]

    Press Enter

    Type : "hdmi_mode=x " where x = corresponding number of resolution mode. See: http://www.raspberrypi.org/phpBB3/viewtopic.php?f=26&t=5851

    e. Then press crtl + o

    f. Press Enter

    g. then press crtl + x

    6. Restart using the command: " sudo shutdown -r now "

     

    Now you have desired resolution and Sound!!!

     

    Happy Raspberry Pi...ing

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to wallarug

    That fixed my issue - Thanks!  I'm surprised it's not marked as a correct answer.

     

    I was almost going to ship the PI back because I bought it for the HDMI!  I guess we'll have to keep an old composite video monitor around a bit longer...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 13 years ago in reply to e14 Contributor

    It should be marked as the correct answer.  maybe this is a new person who doesn't know who to make correct.