Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Possible Hardware fixes
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 44 replies
  • Subscribers 709 subscribers
  • Views 5066 views
  • Users 0 members are here
  • raspberry_pi
Related

Possible Hardware fixes

e14 Contributor
e14 Contributor over 14 years ago

So one of the things I plan to do when R-Pi are more available is to butcher a couple of them and incorporate some things I consider to be appropriate hardware fixes. This is my list so far, any feedback or additional suggestions welcome.

 

1. Remove the SD Card slot and replace it with a small adapter pcb containing a micro-sd connector. The full size SD card sticking out the end is ok for development or when you want to swap the card a lot, not so good when you want to build the whole Pi into something else and would like to use some of that dead space for other things. 1764377 micro-sd connector chosen, will be oriented at right angle to the current slot.

 

2. Replace usb polyfuse arrangement. Diodes Inc AP1212 seems to fit the bill. 1825303 33 pence each

 

3. Replace RG1 & RG2. Current plan is to use the TPS54231 1755637 as suggested by jamodio, however it's relatively expensive. Also looking at AP1533, 1825334 which appears similar from an external components point of view, but approx 1/10 the cost.

 

4. Cut the 1.8v from the Lan9512. Could do with the full gerbers to work out if this is possible. C29, C36 & C43 along with pins 15 & 38 just vanish into vias. Ideas welcome.  My other options are to remove the Lan9512 and make myself a model A, or to leave RG1 off and see if we still boot with 1.8v from the lan9512 regulator.

 

5. As I'll be replacing the SD card slot, I'm contemplating if it's possible to add some power switching to allow running the slot at 1.8v to get some of the faster access modes. I think this will probably need some driver work and stealing a gpio from somewhere. I'd be tempted to use GPIO5 or GPIO27 (CAM_CLK, CAM_GPIO), but maybe the GPU will mess with those and GPIO31/CONFIG3 could be a better choice.

 

6. RTC based on MCP79410, 1823155

 

7. Removal of micro-usb power connector as I don't consider it appropriate. 5v and 3.3v can be supplied via P1 instead.

 

If only 1.8v was available on P1, some things could have been easier. So...

 

8. Replace P1 with a 28 pin connector to allow 1.8v to be made available. The extra two pins to extend off the end on the pcb and be wired to RG1's previous position.

 

9. For ease of integration, put P1 on the underside of the board and likely also replace P4 & S7 with headers allowing their connectors to be moved onto the underlying board and aligned better wrt case.

 

Thoughts ?

  • Sign in to reply
  • Cancel
Parents
  • morgaine
    morgaine over 14 years ago

    This thread is totally awesome, almost to the extent of demanding some 4-letter words to hammer home the point.  Mankind will reach the stars only by improving on what went before.  Being attached to what exists is barely worthy of bacteria.

     

    +1000

     

    My area of head-scratching:  how to turn the SD card into a network boot.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    >My area of head-scratching:  how to turn the SD card into a network boot.

     

    There are some adapters that convert SD into USB, such as this one:

     

    http://www.teampctechnology.com/product_detail.php?id=603

     

    It appears to be discontinued, but there are probably others,

    athough most SD/USB adapters go the opposite direction.

     

    Once you've got USB, I think you're home free.

    You can connect it to a usb hub, with an ethernet port,

    along with usb keyboard/mouse and then disable the

    lan chip and save 20% of your cpu time.  Would make

    for the fastest RPi youtube demo to date if it works.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to e14 Contributor

    Why do you think it will save 20% CPU, you are still using USB and it needs to be polled. The LAN9512 acts as a USB hub so even if you go external is the same thing.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to jamodio

    you wouldn't be going through the lan chip at all, because you're

    not using the RPi's USB or ethernet ports, you're using the SD interface.

     

    I'm not sure that the keyboard/mouse would work, since the SD interface

    is expecting a file system.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to jamodio

    you wouldn't be going through the lan chip at all, because you're

    not using the RPi's USB or ethernet ports, you're using the SD interface.

     

    I'm not sure that the keyboard/mouse would work, since the SD interface

    is expecting a file system.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jamodio
    jamodio over 14 years ago in reply to e14 Contributor

    Ohh, I see you mean using that SD<->USB converter not going directly to the USB pins (sort of model A) of the SoC.

     

    But how efficient is that thing ? is it available ?, can't find any similar to that one

     

    Also it would have been nicer to have more of the GPIO pins available somewhere, even on a non populated 2mm header.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to jamodio

    >is it available ?, can't find any similar to that one

     

    I've looked, and strangely, I can't find anything like it,

    although quite a few people seem to want such a thing.

    The closest I've found is SD to WiFi adapters, such as

    eye-fi, but I'm not sure if special drivers would be needed.

     

    http://www.eye.fi/how-it-works/basics

     

    See also the Toshiba FlashAir wireless LAN SD card

    http://www.engadget.com/2012/01/11/toshiba-flashair-hands-on/

    said to be the first card implementing the SD association's

    Wireless LAN Standard.