Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Possible Hardware fixes
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 44 replies
  • Subscribers 709 subscribers
  • Views 5058 views
  • Users 0 members are here
  • raspberry_pi
Related

Possible Hardware fixes

e14 Contributor
e14 Contributor over 14 years ago

So one of the things I plan to do when R-Pi are more available is to butcher a couple of them and incorporate some things I consider to be appropriate hardware fixes. This is my list so far, any feedback or additional suggestions welcome.

 

1. Remove the SD Card slot and replace it with a small adapter pcb containing a micro-sd connector. The full size SD card sticking out the end is ok for development or when you want to swap the card a lot, not so good when you want to build the whole Pi into something else and would like to use some of that dead space for other things. 1764377 micro-sd connector chosen, will be oriented at right angle to the current slot.

 

2. Replace usb polyfuse arrangement. Diodes Inc AP1212 seems to fit the bill. 1825303 33 pence each

 

3. Replace RG1 & RG2. Current plan is to use the TPS54231 1755637 as suggested by jamodio, however it's relatively expensive. Also looking at AP1533, 1825334 which appears similar from an external components point of view, but approx 1/10 the cost.

 

4. Cut the 1.8v from the Lan9512. Could do with the full gerbers to work out if this is possible. C29, C36 & C43 along with pins 15 & 38 just vanish into vias. Ideas welcome.  My other options are to remove the Lan9512 and make myself a model A, or to leave RG1 off and see if we still boot with 1.8v from the lan9512 regulator.

 

5. As I'll be replacing the SD card slot, I'm contemplating if it's possible to add some power switching to allow running the slot at 1.8v to get some of the faster access modes. I think this will probably need some driver work and stealing a gpio from somewhere. I'd be tempted to use GPIO5 or GPIO27 (CAM_CLK, CAM_GPIO), but maybe the GPU will mess with those and GPIO31/CONFIG3 could be a better choice.

 

6. RTC based on MCP79410, 1823155

 

7. Removal of micro-usb power connector as I don't consider it appropriate. 5v and 3.3v can be supplied via P1 instead.

 

If only 1.8v was available on P1, some things could have been easier. So...

 

8. Replace P1 with a 28 pin connector to allow 1.8v to be made available. The extra two pins to extend off the end on the pcb and be wired to RG1's previous position.

 

9. For ease of integration, put P1 on the underside of the board and likely also replace P4 & S7 with headers allowing their connectors to be moved onto the underlying board and aligned better wrt case.

 

Thoughts ?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    looks like a good list.  Too bad the PoP ram is so hard to replace,

    as that would be another nice improvement.  I've been thinking of

    modifying one for high-altitude balooning, or similar uses, where

    size and/or weight matter.  So here's my list:

      1) remove csi connector,

      2) remove dsi connector,

      3) remove hdmi connector,

      4) remove RCA connector,

      5) remove audio connector,

      6) remove ethernet connector,

      7) remove micro usb connector (directly solder power wires),

      8) remove GPIO pins,

      9) remove LDO voltage regulators, replace with switch mode,

    10) remove LAN chip,

    11) remove dual-usb connector, directly solder one usb device,

    12) remove polyfuses, replace with 1 Ohm resistor,

    13) remove the capacitor that frequently falls off,

    14) as you suggest, replace SD with micro SD.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to e14 Contributor

    I'll be replacying the polyfuses with 0 ohm resistors, no need ot waste power.

     

    I'll probably keep ethernet and HDMI.

     

    Agreed with the two FPC connectors, good move by RPF to offer a camera that will be more expensive than the board.

     

    The RCA jack takes too much space, same as audio, perhaps something done on similar designs like Roku2, replace both by a single jack that can carry all signals, but resolution and image quality out of the composite video output is not very good, perhaps better use something that can support VGA instead.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to jamodio

    the 1 Ohm resistor is to avoid voltage drops from

    power surges on the USB device.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to e14 Contributor

    For that you should have a pair of good tantal bulk caps as recommended by the USB spec sort of 150µF, and I'd add USB power switches.

     

    I'd be nice if Broadcom started selling the "alpha" boards :-)

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to jamodio

    and I'd add USB power switches.

    I probably didn't make it clear enough in the list, the AP1212 I mentioned is a usb power switch.

     

    Making the obvious comparison, the cheapest 140mA polyfuse from farnell is 0.113 gbp in qty 5, and the AP1212 is 0.33 gbp in qty 1. So I'm not at all sure the case for using polyfuses is a good one. Don't know what costs @ 10K, 100K etc would be like though.

     

    Anyway, remove D10, D11 and both polyfuses and it should be simple to put the power switch in, the datasheet suggests a 33uF cap on the usb connector side and it has a soft-start feature to avoid the power dip when connecting a device.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to jamodio

    The RCA jack takes too much space, same as audio,

    I didn't add those to my list, almost goes without saying that I  won't use them and will likely remove them. For add-on boards that plug onto the gpio on top of the board that RCA connector is just too high.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to e14 Contributor

    Ohh you right I missed that one.

     

    Cost and the fixation on the credit card size form factor are very lame design guidelines, It is not bad to have an approximate target size, but they didn't have any mechanical restrictions or requirements, so component and connector layout could have been much better.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Dom said today:

     

          I agree that a small resistor is a better solution.  ...    

         The problem was that by the time the first report of the small resistor         

         fixing the reset problem was posted, the rev2 PCB had already been laid out.

     

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=5249&start=166

     

    I wonder exactly when the rev2 PCB was laid out, especially since PeteL

    was apparently getting up to speed on the 1.8V issue quite recently.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    coder27 wrote:

     

    Dom said today:

     

          I agree that a small resistor is a better solution.  ...   

    It's really not. The better solution is to use a proper USB Power Switch IC like a AP1212 or similar that has a slow-start feature and big enough reservoir capacitors.  As Burngate said in the post after the one you linked, v2 is a backward step in this regard as it removes the possibility to do something better yourself.

    I wonder exactly when the rev2 PCB was laid out, especially since PeteL

    was apparently getting up to speed on the 1.8V issue quite recently.

    It was my thought that v2 was probably done in conjunction with the move to UK manufacturing. The chinese factory has built enough without needing holes for the ATE fixture, but a new manufacturer might well demand some improvements to help their process.

    I could obviously be wrong in that assumption, but if I'm right it would likely put it's layout at around the time of Pete's last visit here.  That ties in reasonably well with the 1.8v fix, but I'm also fairly sure the low ohm resistor ideas were being talked about much earlier. 

    But was anyone listening ?  One of the big problems I see with the level of interest in the Pi is that discussions inevitably get drowned out by the noise, especially in the RPF forums, and solutions with solid engineering reasoning often get blown out of the water or simply ignored by the clueless masses flapping around in the dark. Just look at jamoido's post on the RPF forum on the 1.8v thing, as far as I can tell it was completely ignored at the time.

    Not sure there's an easy solution though, the RPF is somewhat a victim of it's success and the way it's forums are run doesn't engourage proper discussion on issues or the engineering reasons why they're an issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    I somtimes have the impression they really want to create confusion on the RPF forum.

    Like Jamesh agreeing there is a problem with the usb stack, and a bit later claiming that he fixed his stuck keys by replacing his supply...

    You don't need a 5000 euro usb analyser to test that theory. A simple lab adjustable power supply can do the trick.

    When I told them Element 14 was selling usb hubs for the Pi that apparently provided power on their upstream port, they said it wasn't their problem.

    Every technical question about the current progress on the issues is simply ignored....

    A lot of people have no problems. That sure helps if you go to a forum with a problem.

    But as Jamesh pointed out very accurate yesterday...It's just a waste of time...

    And even better I found ...how much more open can the foundation be?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    I somtimes have the impression they really want to create confusion on the RPF forum.

    Like Jamesh agreeing there is a problem with the usb stack, and a bit later claiming that he fixed his stuck keys by replacing his supply...

    You don't need a 5000 euro usb analyser to test that theory. A simple lab adjustable power supply can do the trick.

    When I told them Element 14 was selling usb hubs for the Pi that apparently provided power on their upstream port, they said it wasn't their problem.

    Every technical question about the current progress on the issues is simply ignored....

    A lot of people have no problems. That sure helps if you go to a forum with a problem.

    But as Jamesh pointed out very accurate yesterday...It's just a waste of time...

    And even better I found ...how much more open can the foundation be?