Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Possible Hardware fixes
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 44 replies
  • Subscribers 709 subscribers
  • Views 5081 views
  • Users 0 members are here
  • raspberry_pi
Related

Possible Hardware fixes

e14 Contributor
e14 Contributor over 14 years ago

So one of the things I plan to do when R-Pi are more available is to butcher a couple of them and incorporate some things I consider to be appropriate hardware fixes. This is my list so far, any feedback or additional suggestions welcome.

 

1. Remove the SD Card slot and replace it with a small adapter pcb containing a micro-sd connector. The full size SD card sticking out the end is ok for development or when you want to swap the card a lot, not so good when you want to build the whole Pi into something else and would like to use some of that dead space for other things. 1764377 micro-sd connector chosen, will be oriented at right angle to the current slot.

 

2. Replace usb polyfuse arrangement. Diodes Inc AP1212 seems to fit the bill. 1825303 33 pence each

 

3. Replace RG1 & RG2. Current plan is to use the TPS54231 1755637 as suggested by jamodio, however it's relatively expensive. Also looking at AP1533, 1825334 which appears similar from an external components point of view, but approx 1/10 the cost.

 

4. Cut the 1.8v from the Lan9512. Could do with the full gerbers to work out if this is possible. C29, C36 & C43 along with pins 15 & 38 just vanish into vias. Ideas welcome.  My other options are to remove the Lan9512 and make myself a model A, or to leave RG1 off and see if we still boot with 1.8v from the lan9512 regulator.

 

5. As I'll be replacing the SD card slot, I'm contemplating if it's possible to add some power switching to allow running the slot at 1.8v to get some of the faster access modes. I think this will probably need some driver work and stealing a gpio from somewhere. I'd be tempted to use GPIO5 or GPIO27 (CAM_CLK, CAM_GPIO), but maybe the GPU will mess with those and GPIO31/CONFIG3 could be a better choice.

 

6. RTC based on MCP79410, 1823155

 

7. Removal of micro-usb power connector as I don't consider it appropriate. 5v and 3.3v can be supplied via P1 instead.

 

If only 1.8v was available on P1, some things could have been easier. So...

 

8. Replace P1 with a 28 pin connector to allow 1.8v to be made available. The extra two pins to extend off the end on the pcb and be wired to RG1's previous position.

 

9. For ease of integration, put P1 on the underside of the board and likely also replace P4 & S7 with headers allowing their connectors to be moved onto the underlying board and aligned better wrt case.

 

Thoughts ?

  • Sign in to reply
  • Cancel
Parents
  • jamodio
    jamodio over 14 years ago

    There is another DC-DC converter I'm testing for another design from Intersil, ISL9104 500mA 4.3MHz high efficiency, very small package and cheap, few external components.

     

    The Alpha board had DC-DC converters and apparently a better power supply design. The micro USB and phone chargers is turning to be a really bad idea, so I agree about changing that, actually I'm powering the board from the P1 header.

     

    Yes without the Gerbers is not easy to envision what kind of "blue wire" fixes can be done.

     

    I'm thinking seriously if after all there is enough interest and momentum to start a true "open source hardware" development.for a Pi like board, with parts that are documented. Even if I understand the reasons I don't like at all that the Pi design was built around a part that has practically no documentation publicly available.

     

    I may be able to get some funding and people interested to support an open project, perhaps I should exchange some lines with Jim Manley that seems interested to the right thing.

     

    I'm really pissed with all the secrecy, conspiracy, mystery, bad vibes and misinformation emanating from RPF.

     

    -J

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to jamodio

    I'm thinking seriously if after all there is enough interest and momentum to start a true "open source hardware" development.for a Pi like board, with parts that are documented.

    I could certainly be interested, but I see two stumbling blocks. First is that anything with a GPU is unlikely to have good enough docs, second is that anything without a GPU seems unlikely to have the sort of mass market appeal to get the cost down to something reasonable.

     

    The rhombus-tech guys seem to be a reasonable way along this road already, with some interesting info like the cpus they've evaluated: http://rhombus-tech.net/evaluated_cpus/

    However they seem to be a long way from an actual released product and I'm not at all convinced of the EOMA-68 form factor. Although I do like the idea of a set of standard interfaces.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to e14 Contributor

    selsinork wrote:

     

    I'm thinking seriously if after all there is enough interest and momentum to start a true "open source hardware" development.for a Pi like board, with parts that are documented.

    I could certainly be interested, but I see two stumbling blocks. First is that anything with a GPU is unlikely to have good enough docs, second is that anything without a GPU seems unlikely to have the sort of mass market appeal to get the cost down to something reasonable.

     

    The rhombus-tech guys seem to be a reasonable way along this road already, with some interesting info like the cpus they've evaluated: http://rhombus-tech.net/evaluated_cpus/

    However they seem to be a long way from an actual released product and I'm not at all convinced of the EOMA-68 form factor. Although I do like the idea of a set of standard interfaces.

    This is extremely hard to do without corporate sponsorship.  You have to build a lot of boards before they become cost-effective.  Sure, at $89 BeagleBone sounds like a lot of money, but I expect it's quite reasonable given the quantities sold.  If more people get behind BeagleBone, the costs would come down to something closer to RasPi.

     

    Then you have the BeagleBone "capes".  They're pricey, but again it's because of the quanties manufactured.  You really cannot make anything with high-density SMT without specialized equipment and know-how, so it's almost always cheaper to contract it out.  However, the fixed costs of doing so are quite high so you need to pretty large quantity to get something reasonable.  Custom bare PC boards are pretty cheap now, but populating them with BGAs and QFNs isn't.

     

    So my recommendations would be:

     

    1.  Support the most open existing boards, e.g., BeagleBone.

     

    2.  Take existing tablets and make the software open, like Make Play Live's Vivaldi and ZaReason's ZaTab.

     

    3.  Take a look at Xilinx Zynq.  I don't know if that has a complete technical reference yet, but there's no reason it shouldn't completely document the ARM A9s and its hard peripherals.  And it's technically possible to design a completely-open GPU using the FPGA fabric.  Yes, a big job but so is reverse-engineering closed GPUs.  And yes, the FPGA image is (I assume) closed as well, but you can design at the Verilog or EDIF level.

     

    It's really too bad that the Zed Board is so expensive.  I could afford one, but it's unlikely to get a mass following at the current price so my work wouldn't find wide distribution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to johnbeetem

    Sure, at $89 BeagleBone sounds like a lot of money, but I expect it's quite reasonable given the quantities sold.  If more people get behind BeagleBone, the costs would come down to something closer to RasPi.

    Looking at BeagleBone on uk.farnell.com the other day, out of stock. Approx 300 available for delivery sometime between now and 2nd week in August.

    Compare to the 12000+ available for delivery on 23rd July that the Pi was showing a few days ago and the difference in scale is clear.

     

    You have to give the RPF credit for managing to get the interest and backing to be able to ramp up to where they are in such a short time. They seem to be the only ones to have managed it so far. As everyone keeps pointing out there's plenty of other boards out there, but none seem to be gaining the necessary momentum.

     

    How much of the success of the R-Pi is down to aiming low to begin with and praying that the interest will be there ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to e14 Contributor

    selsinork wrote:

     

    ... As everyone keeps pointing out there's plenty of other boards out there, but none seem to be gaining the necessary momentum.

     

    How much of the success of the R-Pi is down to aiming low to begin with and praying that the interest will be there ?

    I think the success of RasPi is the US$25 price.  "A computer for $25?  You've got to be kidding!"  And yes, they are kidding because you can't get the $25 unit, only the warmer $35 version.  Oh, and that doesn't include a case or compatible power supply or mass storage or monitor or cables or keyboard or mouse or any of the other gewgaws you expect to have with a computer -- but you already had those, right?  So there's a big red asterisk beside that "An ARM GNU/Linux box for $25" slogan.  Must be a new meaning of the word "box" I'm not familiar with.

     

    [I'm not complaining.  I knew exactly what I was getting when I ordered a RasPi and it's a great board for the price.  But having grown up reading MAD Magazine I dislike misleading marketing.  "An ad that's bad gets spoofed in MAD."]

     

    Anyway, the US$25 price point gets you interested.  When BeagleBoard came out in 2008, the US$150 price point was terrific for a tiny GNU/Linux capable development board, especially compared to the US$800 (IIRC) full-size board you could get from TI.  But as Morgaine has pointed out, US$35 buys you a good dinner with shipping paying for the tip.  The risk in buying a RasPi and discovering that it's useless for your needs is pretty low.  And US$35 is usually below the level requiring spousal approval.

     

    I imagine that the RPF is flabbergasted by the level of interest -- in a world where desktops are dominated by Windows and most consumer computers are closed consumption devices, who could imagine that you could sell 1 million uncased boards for which you have to download the operating system yourself and transfer it to an SD card.  I'm flabbergasted by the level of interest as well -- the idea that millions are becoming GNU/Lunix users is terrific and helps the future of computing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to johnbeetem

    at least you find out that the advertized $25 price isn't real before you

    commit to the purchase.   Only later do you find out that your keyboard

    doesn't work, or your SD card, or your power supply, or your usb hub,

    or your wifi dongle, or your mpeg-2 TV tuner, etc.   And only after getting

    everything to work do you find out the performance issues, that the hyped

    GPU isn't used for X acceleration, that the SD cards run slow, that the

    cpu overhead for USB interrupts is 20% at idle, the L2 cache isn't attached

    to the cpu, etc.  And then you find out about the intermittent problems,

    such as usb packet loss, SD card corruption, audio pops, failure to boot

    after working fine for a week, etc.

     

    All the front-page blog stories are happy stories, the sad stories are

    in the discussion forums, and the media hasn't picked up on them yet.

     

    I think it's interesting that half (10 of 19 by my count) of next month's

    magpi interview questions have to do with hardware fixes.  So that's

    clearly on people's minds.  We'll see if they actually answer those,

    or just dodge them like they've been doing so far.

     

    http://issuu.com/themagpi/docs/the_magpi_issue4_draft

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to johnbeetem

    at least you find out that the advertized $25 price isn't real before you

    commit to the purchase.   Only later do you find out that your keyboard

    doesn't work, or your SD card, or your power supply, or your usb hub,

    or your wifi dongle, or your mpeg-2 TV tuner, etc.   And only after getting

    everything to work do you find out the performance issues, that the hyped

    GPU isn't used for X acceleration, that the SD cards run slow, that the

    cpu overhead for USB interrupts is 20% at idle, the L2 cache isn't attached

    to the cpu, etc.  And then you find out about the intermittent problems,

    such as usb packet loss, SD card corruption, audio pops, failure to boot

    after working fine for a week, etc.

     

    All the front-page blog stories are happy stories, the sad stories are

    in the discussion forums, and the media hasn't picked up on them yet.

     

    I think it's interesting that half (10 of 19 by my count) of next month's

    magpi interview questions have to do with hardware fixes.  So that's

    clearly on people's minds.  We'll see if they actually answer those,

    or just dodge them like they've been doing so far.

     

    http://issuu.com/themagpi/docs/the_magpi_issue4_draft

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jamodio
    jamodio over 14 years ago in reply to e14 Contributor

    At least they removed that silly picture on the front cover.

     

    I'll not deny that the R-pi was a good market test that if there is demand for this type of boards, but the success (not sure how to define that) in the rapid volume of units ordered was essentially driven by a misleading amount of hype and confusing messages, most of them emanating from RPF and its minions. Eben still today keeps saying that you can do whatever other computers do with the R-pi, which as we know is not quite true.

     

    When you get the beaglebone you know exactly what you are getting and all the parts used are documented and it is a true open source project, you get full Gebers, etc.

     

    Everything around the R-pi is a mystery cloud, and if you can't ask or comment freely.

     

    I'm almost sure that we'll see a lot of R-pis on eBay in the near future from people that got it because it was cool or some friends told them, etc, etc.

     

    -J