Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Possible Hardware fixes
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 44 replies
  • Subscribers 709 subscribers
  • Views 5066 views
  • Users 0 members are here
  • raspberry_pi
Related

Possible Hardware fixes

e14 Contributor
e14 Contributor over 14 years ago

So one of the things I plan to do when R-Pi are more available is to butcher a couple of them and incorporate some things I consider to be appropriate hardware fixes. This is my list so far, any feedback or additional suggestions welcome.

 

1. Remove the SD Card slot and replace it with a small adapter pcb containing a micro-sd connector. The full size SD card sticking out the end is ok for development or when you want to swap the card a lot, not so good when you want to build the whole Pi into something else and would like to use some of that dead space for other things. 1764377 micro-sd connector chosen, will be oriented at right angle to the current slot.

 

2. Replace usb polyfuse arrangement. Diodes Inc AP1212 seems to fit the bill. 1825303 33 pence each

 

3. Replace RG1 & RG2. Current plan is to use the TPS54231 1755637 as suggested by jamodio, however it's relatively expensive. Also looking at AP1533, 1825334 which appears similar from an external components point of view, but approx 1/10 the cost.

 

4. Cut the 1.8v from the Lan9512. Could do with the full gerbers to work out if this is possible. C29, C36 & C43 along with pins 15 & 38 just vanish into vias. Ideas welcome.  My other options are to remove the Lan9512 and make myself a model A, or to leave RG1 off and see if we still boot with 1.8v from the lan9512 regulator.

 

5. As I'll be replacing the SD card slot, I'm contemplating if it's possible to add some power switching to allow running the slot at 1.8v to get some of the faster access modes. I think this will probably need some driver work and stealing a gpio from somewhere. I'd be tempted to use GPIO5 or GPIO27 (CAM_CLK, CAM_GPIO), but maybe the GPU will mess with those and GPIO31/CONFIG3 could be a better choice.

 

6. RTC based on MCP79410, 1823155

 

7. Removal of micro-usb power connector as I don't consider it appropriate. 5v and 3.3v can be supplied via P1 instead.

 

If only 1.8v was available on P1, some things could have been easier. So...

 

8. Replace P1 with a 28 pin connector to allow 1.8v to be made available. The extra two pins to extend off the end on the pcb and be wired to RG1's previous position.

 

9. For ease of integration, put P1 on the underside of the board and likely also replace P4 & S7 with headers allowing their connectors to be moved onto the underlying board and aligned better wrt case.

 

Thoughts ?

  • Sign in to reply
  • Cancel
Parents
  • morgaine
    morgaine over 14 years ago

    This thread is totally awesome, almost to the extent of demanding some 4-letter words to hammer home the point.  Mankind will reach the stars only by improving on what went before.  Being attached to what exists is barely worthy of bacteria.

     

    +1000

     

    My area of head-scratching:  how to turn the SD card into a network boot.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    My area of head-scratching:  how to turn the SD card into a network boot.

    Are you prepared to keep an sd card installed with some minimal code on it ?  If so then perhaps u-boot. There's been some efforts to port it to the Pi and as there appears to be somewhat functional usb and network drivers it's possible to have u-boot load from the sd card then pull kernel etc from something on the network.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    selsinork wrote:

     

    My area of head-scratching:  how to turn the SD card into a network boot.

    Are you prepared to keep an sd card installed with some minimal code on it ?  If so then perhaps u-boot. There's been some efforts to port it to the Pi and as there appears to be somewhat functional usb and network drivers it's possible to have u-boot load from the sd card then pull kernel etc from something on the network.

     

    Aye, some people are already doing that, and it's definitely the easiest approach.  But in the "no limits" spirit of this thread, what I had in mind was bypassing the Pi's built-in requirement for the VideoCore to boot from SD card by making a networked subsystem emulate the SD card at the hardware level.

     

    It's certainly doable in principle.  What's less certain is whether it makes sense to invest so much time though in a device with restricted documentation and many closed-source blobs.  Probably not.  There are better targets out there.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    selsinork wrote:

     

    My area of head-scratching:  how to turn the SD card into a network boot.

    Are you prepared to keep an sd card installed with some minimal code on it ?  If so then perhaps u-boot. There's been some efforts to port it to the Pi and as there appears to be somewhat functional usb and network drivers it's possible to have u-boot load from the sd card then pull kernel etc from something on the network.

     

    Aye, some people are already doing that, and it's definitely the easiest approach.  But in the "no limits" spirit of this thread, what I had in mind was bypassing the Pi's built-in requirement for the VideoCore to boot from SD card by making a networked subsystem emulate the SD card at the hardware level.

     

    It's certainly doable in principle.  What's less certain is whether it makes sense to invest so much time though in a device with restricted documentation and many closed-source blobs.  Probably not.  There are better targets out there.

     

    Morgaine.