Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum ASUS USB-N10 Wifi Adapter Installation Problems
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 704 subscribers
  • Views 1474 views
  • Users 0 members are here
  • raspberry_pi
  • usb-n10
  • asus
  • adapter
  • wireless
  • installation
Related

ASUS USB-N10 Wifi Adapter Installation Problems

e14 Contributor
e14 Contributor over 14 years ago

Hi All

 

I've got my RPi up and running with wireless keyboard & mouse. Connected to the internet via a cable at the mo.

I'm trying to install the Asus USB-N10 wireless adapter to get rid of the cable.

I've downloaded and extracted the r8712u staging driver & it appears to be installed in the right place (lib/modules/3.1.9+/kernel/drivers/staging/rtl8712/r8712u.ko) - or is it ?

I've also downloaded the "firmware-realtek_0.35~bpo60+1_all.deb" file to the /home/pi directory and tried to (blindly !) follow debian's instructions on how to install the firmware - with no luck.

I should point out here that I am just starting out with Linux and a lot of the commands are a complete mystery to me so I'm a long way from being confident that I'm doing the right things.

Just wondered if anyone out there could explain in simple terms what I need to do to get the adapter installed & functional.

 

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • fustini
    fustini over 14 years ago

    Hi Horus,

     

    I tried this adapter with the latest Raspbian "Wheezy" image last week and worked without any changes.  This is the recommended image from the Raspberry Pi Foundation:

     

    http://www.raspberrypi.org/downloads

     

    It looks like we are finally at the point where most wi-fi drivers and firmware are included by default.  I would suggest moving to Raspbian "Wheezy" if possible.  If that is a problem for you, then could you please let me know which image you are running and also the output of these commands:

     

    Linux distribution info:

    cat /etc/issue

    Kernel info:

    uname -a

     

    Cheers,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fustini
    fustini over 14 years ago

    Hi Horus,

     

    I tried this adapter with the latest Raspbian "Wheezy" image last week and worked without any changes.  This is the recommended image from the Raspberry Pi Foundation:

     

    http://www.raspberrypi.org/downloads

     

    It looks like we are finally at the point where most wi-fi drivers and firmware are included by default.  I would suggest moving to Raspbian "Wheezy" if possible.  If that is a problem for you, then could you please let me know which image you are running and also the output of these commands:

     

    Linux distribution info:

    cat /etc/issue

    Kernel info:

    uname -a

     

    Cheers,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • morgaine
    morgaine over 14 years ago in reply to fustini

    @Horus: While you're at it, the output from a few other commands will also shed some light:

     

    modprobe r8712u

     

    which loads the r8712u.ko kernel module, and

     

    lsmod  |  grep r8712u

     

    which would show that the module is loaded if it returns anything at all.  The last few lines of the kernel ring buffer after running the modprobe would also help, which can be displayed with

     

    dmesg  |  tail -n20

     

    If any command (say "XX") is a mystery, then

     

    man XX

     

     

    will often shed some light on it, as will

     

    XX --help

     

    Beyond that, don't be afraid to ask.  Everything was a mystery to all of us, at one point in time. image

     

    Morgaine.

     

    Reply was to Horus, but incorrectly created as a reply to Drew, sorry.