Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RG1 1.8v regulator
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 231 replies
  • Subscribers 711 subscribers
  • Views 36366 views
  • Users 0 members are here
Related

RG1 1.8v regulator

e14 Contributor
e14 Contributor over 14 years ago

Ok, so in a different thread I threatened to remove RG1 and do some current measurements on it's output after seeing those thermal images that show it's not generating any heat...

 

Well, I did it tonight. Some photos here: https://picasaweb.google.com/selsinork/RPi18v

 

The jumper pins in the output let me either just put a jumper on and verify the Pi boots ok, or wire a multimeter in series to get some current readings.

 

The results were interesting to say the least. I had to go back and check I was reading the multimeter correctly, that it wasn't broken etc.

 

On initial power up I see a negative current for a second or so which then reverses to about 0.5mA (yes half a milliamp, that's not a typo) for a few seconds while we get the first sd-card accesses. Once we're booted and sitting at the login prompt the current reading fluctuates from around 0.001mA to maybe 0.04mA. 

 

I'm using the 40mA range on a decent Fluke multimeter, so I've no reason to doubt the results. There's obviously going to be some inaccuracy down at that level due to length of meter leads etc, but the result is fairly clear.  You'll understand why I was checking the meter was working and I was reading it correctly though image

 

 

So from there onto the next test, lets try completely disconnecting RG1 and see if the Pi boots while using the LAN9512 1.8v 'output'.  Yes it does! 

 

I think that's reasonably good indication that jamodio got it spot on, the lan9512 shouldn't be connected to the 1.8v plane and it's heat problems are going to be largely due to supplying current on it's 1.8v filter pin that it was never designed to do.

 

So anyone willing to pull RG1 off a Pi and verify my results ?

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 14 years ago

    I just did some digging in the NCP1117 data sheet (ONsemi version).

     

    RG1 is an NCP1117-1v8 fixed linear LDO regulator.  We have suggested that if RG1's regulation voltage Vreg is greater than IC3's (LAN9512) internal Vreg, then RG1 will supply 1.8V current instead of IC3, reducing IC3's power consumption.

     

    The NCP1117 has a "adjustable output" version which sets Vreg using external resistors instead of internal resistors like the NCP1117-1v8.  In addition, you can adjust Vreg of the "fixed" version with an external resistor plus a stabilization capacitor.  Take a look at Figures 31 and 32.  In Figure 31, a 50 Ohm resistor between the NCP1117's GND pin and circuit GND shifts its output by 300 mV.  Figure 32 uses a variable resistor.  Shifting RG1's Vreg up by 90 mV (+5%) might do a nice job of cooling down IC3 -- probably a 15 Ohm resistor.

     

    Figure 31 also confirms that if two NCP1117's are connected in parallel, the LDO with higher Vreg does switch off the LDO with lower Vreg.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to johnbeetem

    Figure 31 also confirms that if two NCP1117's are connected in parallel, the LDO with higher Vreg does switch off the LDO with lower Vreg.

    The engineer in me asks which electrical characteristic on the datasheet defines the voltage differential required to turn the regulator off? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    selsinork wrote:

     

    If there's a pcb respin needed then it makes sense to take some time and fix as many problems as can be identified in one go - alignment of the RJ45 would be quite high on my personal list.

     

    You would have hoped that Pete had a bunch of fixes pretty much

    ready to go by now, and that this one would just get added to the list

    without much further delay.

     

    But I don't get the impression that Pete has been very active on RPi

    issues lately, based on him being absent from this forum (not even

    monitoring the hardware flaws and fixups thread that he started)

    and based on his recent comment that this issue was just one on

    his list of board issues to look at.  It sounds to me like the returned

    boards have just been piling up unopened in his office.

     

    Since we aren't getting much help from Pete in understanding how

    the regulators work, is anyone able to attach a scope and measure

    any oscillations?

     

    In post #74, Pete wrote:

    "Of the returns I have for analysis, I have still have not found a real ‘steamer’. These could be in part due to poor underfill or even a short/defect elsewhere on top of what we are asking the chip to do."

     

    I find this interesting in regard to element14's limited warranty, which says:

    "Newark element14 warrants that the Raspberry pi will be free from defects in material or workmanship for a period of 12 months from the date of Newark element14's shipment of the Raspberry pi to you, the Customer."

    http://www.farnell.com/datasheets/1627216.pdf

     

    Notice that "design defects" are not explicitly mentioned.  So I wonder if

    "poor underfill" would be a covered defect in workmanship, but an error in

    the schematics would be an uncovered design defect?  I presume if the

    temperatures are hot enough to be considered a safety issue, that it would

    be covered by law in most jurisdictions regardless of whether it was a

    considered to be a design issue or not.

     

    Hopefully someone from element14 will speak up soon as to how the

    warranty applies to this design error.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    coder27 wrote:

     

    But I don't get the impression that Pete has been very active on RPi

    issues lately, based on him being absent from this forum (not even

    monitoring the hardware flaws and fixups thread that he started)

    and based on his recent comment that this issue was just one on

    his list of board issues to look at.  It sounds to me like the returned

    boards have just been piling up unopened in his office.

     

    Since we aren't getting much help from Pete in understanding how

    the regulators work, is anyone able to attach a scope and measure

    any oscillations?

     

    It's rather likely that we've been guilty of wishful thinking regarding Pete's visits to this forum, sometimes seeing it as vindicating our view that (Foundation minus Pete) is on drugs whereas Pete as their engineer retains his professional standards and distances himself from the shenanigans of the rest of the Foundation.  Unfortunately, that's almost certainly naive in the extreme.  He knows that his toast is buttered on the RPF side, and that being seen as a small hero here does not pay the rent.  His absence and silence probably reflects reality rather than our wishful thinking:  we misjudged his desire to do the right thing for the community.

     

    We still don't have the old gerbers despite countless requests and no rational reason for them to be withheld, we still have no information on whether the first revision is intended to be minimal or extensive, and we still don't  have any engineering feedback about Model A operation despite the continued false advertising of "$25 computer" (it would be valuable to quantify USB faults in the absence of the LAN9512).  If Pete wanted, he could be pushing the Foundation towards being more open about these things, but this has not happened.

     

    While wishful thinking makes all us feel better, the facts are not encouraging:  Pete spent at most a few hours on a number of occasions gathering input from the Element 14 forum, but the information flow has been completely one-way.  I think it's time to put the rose-tinted spectacles aside.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to e14 Contributor

    Since we aren't getting much help from Pete in understanding how

    the regulators work, is anyone able to attach a scope and measure

    any oscillations?

     

    On the scope I can see just a little bit of noise less than 20mV but no oscillations, I'm hitting the ethernet port with flood packets.

     

    I'll put the ScopeMeter on a long term plot of 1V8.

     

    About my comments on analysis, etc, the issue is that we have many variables moving at the same time that induce a large deviaton on any measurements, we are not following a common test procedure or similar instruments while testing different boards to be able to produce a reasonable bell curve.

     

    So "it works for me" is valid report too, actually so far it has been working for me too in some aspects.

     

    I'm still wating to see what else Pete has on his "list" ...

     

    BTW I'm playing with the MK802 and the thing works out of the box with Android 4.0, no issues with the RF keyboard/touchpad, video and audio are great, yes I paid $72 for it but includes a power supply, HDMI cable, USB cable, USB adaptor, comes with a nice box and btw has a case !!, ohh and 1GB RAM, 4GB FLASH, the Cortex-A8 runs at 1GHz and the GPU at 500MHz. With all that now the R-pi feels more expensive ...

    I've the little Gizmo attached to one of the corners of my monitor.

    image

     

    I'll try some time later to get Ubuntu running on it

     

    -J

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to jamodio

    Cute, thanks for the pic. image

     

    Cortex-A8 seems a good foundation on which to base a multi-machine home ARM capability.  My BeagleBone and original-version 7" Samsung Galaxy Tab both use Cortex-A8, and so does the forthcoming Olimex A13-based board (all those A10 gadgets too).  Moreover, Cortex-M3 and M4 microcontrollers use the same ARMv7 instruction architecture, so in principle one could do development on a Cortex-A8 Linux machine to target a Cortex-M3/4 series microcontroller without needing cross-compilation.

     

    More advanced application processors like Cortex-A9 MPcore and Cortex-A15 still retain the same basic ARMv7 instruction architecture as Cortex-A8, so there's a solid growth path into the future there too.  ARMv7 is effectively ARM's equivalent of the ubiquitous x86.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    He knows that his toast is buttered on the RPF side, and that being seen as a small hero here does not pay the rent.

     

    I'm not sure the RPF is paying Pete much rent money either,

    given that they have long claimed not to have any paid employees.

    I think it's much more likely that he hasn't been doing much if any

    RPi work lately because they aren't paying him much if anything. 

     

    When Pete first responded to this issue, he didn't say the RPF

    asked him to respond, or that he was responding on behalf of the

    RPF, he said Mike Powell of element14 asked him to respond.

    Of course, the RPF may have later asked him _not_ to respond further.

     

    I suspect there is some checking going on regarding Pete's work

    in designing the board, to see who is liable for fixing the problem.

    If Pete did the work as an employee of RPF, then RPF would probably

    be liable.  If Norcott was involved, then Norcott might be liable.

    I notice that Pete appears to be deflecting some of the blame toward

    Broadcom, in saying that the error was in the earlier prototype boards

    and his work was extensively checked by the SoC experts.  I don't see

    anybody stepping up and taking responsibility.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Cortex-A8 seems a good foundation on which to base a multi-machine home ARM capability.  My BeagleBone and original-version 7" Samsung Galaxy Tab both use Cortex-A8, and so does the forthcoming Olimex A13-based board (all those A10 gadgets too).  Moreover, Cortex-M3 and M4 microcontrollers use the same ARMv7 instruction architecture, so in principle one could do development on a Cortex-A8 Linux machine to target a Cortex-M3/4 series microcontroller without needing cross-compilation.

     

    More advanced application processors like Cortex-A9 MPcore and Cortex-A15 still retain the same basic ARMv7 instruction architecture as Cortex-A8, so there's a solid growth path into the future there too.  ARMv7 is effectively ARM's equivalent of the ubiquitous x86.

     

    Morgaine.

    Cortex-A8 uses the ARMv7-A instruction set which includes both 32-bit ARM instructions plus 16/32bit Thumb/Thumb2  instructions.  Cortex-M3/4 use the ARMv7-M instruction set which only has Thumb/2 instructions.  So if you compile your programs and libraries using Thumb/2, you'll be able to run on both (unless you use integer divide -- Gotcha!)   But if you use ARM instructions, the binaries won't run on Cortex-M3/4.  Yes, it really is this complicated.  Take a look at the latest ARM ARMs (Architecture Reference Manuals).  Or better yet, download the quick reference cards.  They read like railroad time-tables with myriad footnotes.  OTOH, I am truly impressed that they're able to squeeze the intricacies of the ARM/Thumb/2 instruction sets into a few pages.

     

    I guess ARMv7 is equivalent to the x86 in that both evolved from a simpler architecture into a dog's breakfast.  Both are a far cry from my personal favorite, PowerPC, which was a clean, well-designed architecture long before it was implmented as an IC.  OTOH, you can't get a PowerPC board that can run GNU/Linux for under US$120.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to jamodio

    jamodio wrote:

     

    BTW I'm playing with the MK802 and the thing works out of the box with Android 4.0, no issues with the RF keyboard/touchpad, video and audio are great, yes I paid $72 for it but includes a power supply, HDMI cable, USB cable, USB adaptor, comes with a nice box and btw has a case !!, ohh and 1GB RAM, 4GB FLASH, the Cortex-A8 runs at 1GHz and the GPU at 500MHz. With all that now the R-pi feels more expensive ...

     

    I'll try some time later to get Ubuntu running on it

    Thank you for the MK802 photo.  Cute little board, though it obviously has limited I/O.  Please let us know how Ubuntu (or any other GNU/Linux distro) goes.

     

    I'm also going to watch the US$49 cubieboard (http://en.wikipedia.org/wiki/Cubieboard, http://cubieboard.org/).  If cubieboard becomes real and a good community develops, it (and other A10-based boards) could be effective competitors to RasPi.  Love those 2 mm headers!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to jamodio

    jamodio wrote:

     

    Since we aren't getting much help from Pete in understanding how

    the regulators work, is anyone able to attach a scope and measure

    any oscillations?

     

    On the scope I can see just a little bit of noise less than 20mV but no oscillations, I'm hitting the ethernet port with flood packets.

    I think it's really unlikely that you'd see oscillations.  My guess would be that only a handful of boards -- well fewer than 1% -- have RG1 Vref and IC3 Vref so close together that oscillation could occur.  I would guess that usually one or the other simply dominates.  OTOH, as the board heats up, dominance could shift from one regulator to the other, and you might see 1V8 oscillation at the crossover point.  But the dominance could just as easily diverge, and it could depend on NCP1117 manufacturer or lot.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to johnbeetem

    I don't mind much about the limited I/O. On my projects list to try I've connecting it to a USB hub and to one of the IOIO boards from SparkFun that are already supported by Android and other Linux distros.

     

    This is the IOIO board from SparkFun -> https://www.sparkfun.com/products/10748

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to jamodio

    John Beetem wrote:

     

    I think it's really unlikely that you'd see oscillations

     

    Be sure to check all the way up in frequency.  The USB and ETH sections of LAN9512 are isolated with inductors specified at 100MHz, and I'm sure there's a reason for that.  HF parasitics could be very damaging even at very low amplitude.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 14 years ago in reply to jamodio

    John Beetem wrote:

     

    I think it's really unlikely that you'd see oscillations

     

    Be sure to check all the way up in frequency.  The USB and ETH sections of LAN9512 are isolated with inductors specified at 100MHz, and I'm sure there's a reason for that.  HF parasitics could be very damaging even at very low amplitude.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Be sure to check all the way up in frequency.  The USB and ETH sections of LAN9512 are isolated with inductors specified at 100MHz, and I'm sure there's a reason for that.  HF parasitics could be very damaging even at very low amplitude.

    Do you think it would be worth tacking on a couple of 100nF caps across C29 in light of this? I didn't think it was worth the effort at the time but it might be important for HF dampening.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    Troy Mackay wrote:

     

    Do you think it would be worth tacking on a couple of 100nF caps across C29 in light of this? I didn't think it was worth the effort at the time but it might be important for HF dampening.

     

    Probably, although I can't claim to have a really solid justification.  We're pretty much in the dark when tampering with black boxes, and we don't really know whether the manufacturer is just designing defensively or has a very specific thing that he wants to suppress.

     

    But when in doubt, it's probably a good idea to replicate the manufacturer's recommended circuitry religiously, and those 100nF's are very likely to have less parasitic inductance than C29 so they'll do a better job of decoupling at higher frequencies.

     

    If it's a pain, maybe compromise and fit just one. image