Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RG1 1.8v regulator
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 231 replies
  • Subscribers 711 subscribers
  • Views 36451 views
  • Users 0 members are here
Related

RG1 1.8v regulator

e14 Contributor
e14 Contributor over 14 years ago

Ok, so in a different thread I threatened to remove RG1 and do some current measurements on it's output after seeing those thermal images that show it's not generating any heat...

 

Well, I did it tonight. Some photos here: https://picasaweb.google.com/selsinork/RPi18v

 

The jumper pins in the output let me either just put a jumper on and verify the Pi boots ok, or wire a multimeter in series to get some current readings.

 

The results were interesting to say the least. I had to go back and check I was reading the multimeter correctly, that it wasn't broken etc.

 

On initial power up I see a negative current for a second or so which then reverses to about 0.5mA (yes half a milliamp, that's not a typo) for a few seconds while we get the first sd-card accesses. Once we're booted and sitting at the login prompt the current reading fluctuates from around 0.001mA to maybe 0.04mA. 

 

I'm using the 40mA range on a decent Fluke multimeter, so I've no reason to doubt the results. There's obviously going to be some inaccuracy down at that level due to length of meter leads etc, but the result is fairly clear.  You'll understand why I was checking the meter was working and I was reading it correctly though image

 

 

So from there onto the next test, lets try completely disconnecting RG1 and see if the Pi boots while using the LAN9512 1.8v 'output'.  Yes it does! 

 

I think that's reasonably good indication that jamodio got it spot on, the lan9512 shouldn't be connected to the 1.8v plane and it's heat problems are going to be largely due to supplying current on it's 1.8v filter pin that it was never designed to do.

 

So anyone willing to pull RG1 off a Pi and verify my results ?

  • Sign in to reply
  • Cancel
Parents
  • electron2
    electron2 over 14 years ago

    As shown in Troy Mackay's post on Jul 28 it seems to me that we could mod our PI's to work more as the chips were designed.

     

    I think that this could make the PI more stable, from the looks of it.

     

    I am not a designer Just an old tech, but I think we need to find a way to FIX what we now know is an error in the board.

     

    So could someone do some practical testing to see if there is something that can be done to easly fix the current board, rather than wait for RPI foundation to fix it by waiting for a board redesign?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to electron2

    i will love to try out the hack Troy mackay has done also and then test again with that fix on the board, but i have looked into this and i most say it is very well done by Troy as i think it is to small for me todo and i done have an microscope as need for this.

     

    so yes if some one can findout where to make an cut to split the LAN9512 1v8 from the lod 1v8 then i will try this also.

     

     

    Tooms

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to e14 Contributor

    It would help to have a nice set of Gerber files with the current pcb layout to take a look a the traces and vias to chose what is the best course of action

    before cutting stuff.

     

    One option could be to just lift the two VDD18CORE pins, put togeher a small board that can be placed on top where the logo is with the 3.3 and 1.8

    swtiched regulators, there are some very efficient and small ones like the LMZ10501 that can handle up to 1A and includes the FET and inductor

    on the chip, add the decoupling caps for VDD18CORE on this board and run a wire to those pins. With some work you could manage to have

    through hole pads to match the pads for the existing regulators.

     

    I think there are two or three tiny ceramic caps that will get hidden under the add-on board. It may work ...

     

    My .02

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Tooms wrote:

     

    i will love to try out the hack Troy mackay has done also and then test again with that fix on the board, but i have looked into this and i most say it is very well done by Troy as i think it is to small for me todo and i done have an microscope as need for this.

     

    so yes if some one can findout where to make an cut to split the LAN9512 1v8 from the lod 1v8 then i will try this also.

     

     

    Tooms

    The microsope is really handy (and didn't cost me a cent), you'd be surprised what you can do when you can see what it is you are doing. I haven't even done a lot of SMD work. I'd love one of those IR cameras though... They'd be a bit harder to find in someones junk bin.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to e14 Contributor

    I really don't know how much effort to put on modifying the existing boards, what should happen is the RPF people acknowledge the problem, come up with a workaround, fix it for future boards and analyze the long term effects of THEIR ERROR.

     

    Don't think anybody will be open to a massive recall, but the right thing to do is TO FIX THE ERROR.

     

    My .02

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to jamodio

    For $38 I don't expect a great deal of support, but I do expect that for a first revision board shipped naked without accessories or a case in limited numbers that it was never intended for the classroom in this form. More likely their target was developers and hackers to help mature the product, find bugs and develop software. I would hope that there will be future revisions, debugged, upgraded, shipped with a case and basic accessories, but I'm happy to tinker about with what I have; that is, after all, what I bought it for.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to jamodio

    For $38 I don't expect a great deal of support, but I do expect that for a first revision board shipped naked without accessories or a case in limited numbers that it was never intended for the classroom in this form. More likely their target was developers and hackers to help mature the product, find bugs and develop software. I would hope that there will be future revisions, debugged, upgraded, shipped with a case and basic accessories, but I'm happy to tinker about with what I have; that is, after all, what I bought it for.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jamodio
    jamodio over 14 years ago in reply to e14 Contributor

    Well they missed the target for about couple of million miles. At the development phase price is irrelevant, and on the production phase what matters is cost, and not just components and assembly, you have to factor in that you will also need people and systems if you pretend to do a professional and serious job.

     

    Being a charity or non-profit doesn't mean you have to cry all the time about it, I'm associated with non-profits that deal with huge piles of money and have a full time staff to do the organization's job to deliver on their mission and goals.

     

    I think the argument "you get what you paid for" is very lame, I really don't care much about how much I paid for it or even if I had to pay much more to be part of what was promised to be an initiative to improve education on computer science.

     

    There are no clear indications that there will be future versions or revisions and trying to obtain any information on that front is almost impossible. The only thing they keep talking about is the model "A" which is the same thing less few components and the camera module.

     

    Still is a nice gadget to play with eLinux.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to jamodio

    jamodio wrote:

     

    There are no clear indications that there will be future versions or revisions and trying to obtain any information on that front is almost impossible. The only thing they keep talking about is the model "A" which is the same thing less few components and the camera module.

    Ironically, the Model A fixes the 1.8V regulator problem by not populating the LAN9512 image, which also allows RasPi to run in a closed plastic case w/o heat problems.  Moderators at the RasPi Forum like to point out that the BCM2835 is used in cell phones without heat problems.  I don't recommend asking them how many cell phones have LAN9512 chips.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to johnbeetem

    John Beetem wrote:

     

    Moderators at the RasPi Forum like to point out that the BCM2835 is used in cell phones without heat problems.

     

    The moderators live in a fanboi partition of reality where facts are an inconvenient irrelevance.  The BCM2835 is not known to have been used in anything other than Roku 2 until the Pi, and no BCM28xx series VideoCore has ever been used in a cellphone.

     

    It's the same odd partition of reality in which the Pi is called a "low power consumption" computer, the same "low power" that caused plastic components in that balloon payload to melt, and the same "low power" that doesn't allow me to keep my finger on the LAN9512 for longer than reflex time.

     

    Pity that XKCD isn't too interested in us.  There's enough material here for volumes.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Troy,

    You wrote:

    "More likely their target was developers and hackers to help mature the product, find bugs and develop software."

     

    I think that is a widely held misconception.  Liz has explicitly said the

    product is not in beta test.  Eben has explicitly said it is for sale to

    anyone, not just developers and hackers.  If they were wanting to

    find bugs and mature the product, they would have a highly visible

    bug tracking system, and they would be eager to hear complaints. 

    Instead they ban people who complain, labelling them "concern trolls". 

    Jamodio ought to be a hero on the RPi forum for finding what is probably

    the most serious design error.  Instead, he is banned as a concern troll.

     

    JamesH has made clear that they have no intention of disclosing

    defects to potential buyers, and Abishur banned the guy yesterday

    who advocated disclosing the known USB problems, and who said

    he wouldn't have bought his RPi had he known.  Certainly they don't

    show even the slightest bit of sympathy for those who end up

    feeling duped.

     

    So my impression is that their target market is the unsuspecting

    buyer who is blinded by the low price.  I think they are afraid that

    their sales would dry up if they disclosed that the product isn't finished,

    and they seem to think that they can't afford to lose the sales to those

    who end up feeling duped.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to jamodio

    I think the argument "you get what you paid for" is very lame,

    Possibly true.  My take on it is that something that's agressively designed down to a very low cost inevitably leads to compromises, doesn't matter if it's the RPF or IBM.  You have to account for that somehow and expecting the same results as something designed to a 10x greater cost with a huge R&D budget behind it just isn't realistic.

     

    We may not like all the compromises, but it's done now. Hopefully a potential version 2 can improve things.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    If they were wanting to

    find bugs and mature the product, they would have a highly visible

    bug tracking system,

    Yeah, it's long past the point where the blog and forum format outlived it's usefulness - I'd argue mid April when the first boards were delivered was when it should have changed. The Raspbian site makes them look so much better and they probably have less people and resources, so it's not hard.

     

    Jamodio ought to be a hero on the RPi forum for finding what is probably

    the most serious design error. 

    Agreed. I haven't looked recently, but I noticed that they basically just blanked him when he posted it which, to me, says a lot.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to e14 Contributor

    coder27 wrote:

     

    Jamodio ought to be a hero on the RPi forum for finding what is probably

    the most serious design error.  Instead, he is banned as a concern troll.

     

    I don't think I have to be considered a hero, somebody else would have noticed and reported the error(s) if RPF had released the schematics and Gerbers before sending the boards to production.

     

    There is another major issue with the quality of some of the components as I reported before. In particular the LDO voltage regulators that on the beta board were from NXP and now are from some Chinese knock off.

     

    In my company we are moving away from buying some cheap components produced in China, it is well known in the electronics community that counterfeiting of components have been increasing substantially, like one of the more known cases being the Nichicon aluminium electrolytic blowing up on monitors and computer switching power supplies since the counterfeit part used a very low quality dialectic and the part does not meet the specs.

     

    To tell the truth this is not a complex board in number of parts, signals, nets, and we engineers often make errors, that's why when we work professionally we have a review process before we commit to large scale production. In this case the process didn't exist or some people were not paying attention.

     

    What really concerns me (after all I'AM a "concern troll") is that this type of situation serves as a learning experience so we don't repeat the same errors or wrong processes, but I doubt that if there is ever a new revision or version of this board, we'll have the opportunity to review it before the hype-pi 2.0 starts.

     

    My .02

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to jamodio
    In my company we are moving away from buying some cheap components produced in China, it is well known in the electronics community that counterfeiting of components have been increasing substantially, like one of the more known cases being the Nichicon aluminium electrolytic blowing up on monitors and computer switching power supplies since the counterfeit part used a very low quality dialectic and the part does not meet the specs.

    I must have replaced thousands of those in PC's, but that particular problem seems to be solved - at least from what I see.

     

    From the people I know who work for chinese manufacturers it certainly appears that a large part of going to china is to do with getting counterfeit parts - if not the whole device!

    Part of the problem is quickly going to become - if it hasn't already - that your 'original' NXP LDO will have been made in the same factory, on the same equipment, and to the same design as the chinese one. Maybe both will use the NXP design, maybe the chinese one. As long as they're not totally flaky and outlast the warranty there's a part of me that thinks nobody will care - stuff dying sooner means you replace it sooner and someone makes another sale. The beancounters like that idea image

     

    Have we all seen this before ?

    image

    I have no idea if it's real or someone just did a mockup to illustrate a point, but certainly made me smile image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to jamodio

    jamodio wrote:

     

    What really concerns me (after all I'AM a "concern troll") is that this type of situation serves as a learning experience so we don't repeat the same errors or wrong processes, but I doubt that if there is ever a new revision or version of this board, we'll have the opportunity to review it before the hype-pi 2.0 starts.

     

    +1.

     

    Feedback on issues is part of the engineering process.  That's alien to Liz's hype & fandom process.

     

    PeteL wrote:

     

    As always - comments welcome.

     

    +1

     

    I've been trying to quantify one particular area of faulty operation, RF mice on self-powered USB hubs .  With dozens of tested (device X hub) combinations, and all 8 of the data points for RF mice showing complete failure on Pi, it's a very black-and-white test bench for USB functionality.  I happen to have a hot-running LAN9512, so I may be able to provide relevant testing if the 1.8v issues are thought to couple to USB operation.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to jamodio

    J

     

     

    Connecting the two 1V8’s is a sub optimal piece of design (you can look that up in the engineering translation dictionary - starts with a 'c' ends in ‘up’), and I didn't think that was of debate.

     

     

    The design did go through extensive review within the 'inner circle' of supporters who 'know' and have worked with the chips before especially the BCM. Both prototypes and pre-prototypes had this same connection and that of course made it more difficult. I also suspect, had there not been some reason to go and look, it would have never been identified. Just for the record, your technical input is appreciated, but rather than just implying - you could have just asked? Maybe you did earlier and I missed it.

     

     

    We tried to do the best job possible with the limited support and resources that the early phase project had. (We were going to make 5000-10,000 beta boards max). None of the early stress testing revealed the issue and only a small population (sub 0.01%) are reported to run unbearably hot (although more may, just not flagged up because it does not concern their owner - they are just having fun with it). Of the returns I have for analysis, I have still have not found a real ‘steamer’. These could be in part due to poor underfill or even a short/defect elsewhere on top of what we are asking the chip to do.

     

    There is an implication in posts that this is responsible for something else to do with USB but to date no info is forthcoming? (Stop press - just seen that other thread - will go and look later).

     

    It doesn't matter if you spend £1 or $10M things slip through, and there have been some very high profile events in that $10M category in all walks of engineering!

     

     

    I remember saying at the outset that Pi would never be perfect - just doesn't happen in engineering there is always something to be optimised, improved. What we do need to do is measure, evaluate, garner input and decide what, if anything, needs to be done. And I do appreciate the work done by people on this thread already.

     

     

    Pete