Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RG1 1.8v regulator
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 231 replies
  • Subscribers 711 subscribers
  • Views 36411 views
  • Users 0 members are here
Related

RG1 1.8v regulator

e14 Contributor
e14 Contributor over 14 years ago

Ok, so in a different thread I threatened to remove RG1 and do some current measurements on it's output after seeing those thermal images that show it's not generating any heat...

 

Well, I did it tonight. Some photos here: https://picasaweb.google.com/selsinork/RPi18v

 

The jumper pins in the output let me either just put a jumper on and verify the Pi boots ok, or wire a multimeter in series to get some current readings.

 

The results were interesting to say the least. I had to go back and check I was reading the multimeter correctly, that it wasn't broken etc.

 

On initial power up I see a negative current for a second or so which then reverses to about 0.5mA (yes half a milliamp, that's not a typo) for a few seconds while we get the first sd-card accesses. Once we're booted and sitting at the login prompt the current reading fluctuates from around 0.001mA to maybe 0.04mA. 

 

I'm using the 40mA range on a decent Fluke multimeter, so I've no reason to doubt the results. There's obviously going to be some inaccuracy down at that level due to length of meter leads etc, but the result is fairly clear.  You'll understand why I was checking the meter was working and I was reading it correctly though image

 

 

So from there onto the next test, lets try completely disconnecting RG1 and see if the Pi boots while using the LAN9512 1.8v 'output'.  Yes it does! 

 

I think that's reasonably good indication that jamodio got it spot on, the lan9512 shouldn't be connected to the 1.8v plane and it's heat problems are going to be largely due to supplying current on it's 1.8v filter pin that it was never designed to do.

 

So anyone willing to pull RG1 off a Pi and verify my results ?

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 14 years ago

    I just did some digging in the NCP1117 data sheet (ONsemi version).

     

    RG1 is an NCP1117-1v8 fixed linear LDO regulator.  We have suggested that if RG1's regulation voltage Vreg is greater than IC3's (LAN9512) internal Vreg, then RG1 will supply 1.8V current instead of IC3, reducing IC3's power consumption.

     

    The NCP1117 has a "adjustable output" version which sets Vreg using external resistors instead of internal resistors like the NCP1117-1v8.  In addition, you can adjust Vreg of the "fixed" version with an external resistor plus a stabilization capacitor.  Take a look at Figures 31 and 32.  In Figure 31, a 50 Ohm resistor between the NCP1117's GND pin and circuit GND shifts its output by 300 mV.  Figure 32 uses a variable resistor.  Shifting RG1's Vreg up by 90 mV (+5%) might do a nice job of cooling down IC3 -- probably a 15 Ohm resistor.

     

    Figure 31 also confirms that if two NCP1117's are connected in parallel, the LDO with higher Vreg does switch off the LDO with lower Vreg.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to johnbeetem

    I spotted that too but initially dismissed the idea since I thought they must be assuming constant current drain for those figures based on my misunderstanding of how these regulators worked.

     

    From the description of the adjustable variety, and assuming the fixed version is basically the same with internal resistance, the GND pin is a constant current source (with unknown current due to unknown internal resistors) with a negligible contribution from the internal reference "pin".

     

    "For the fixed output devices R1 and R2 are included within the device and the ground current Ignd, ranges from 3.0 mA to 5.0 mA depending upon the output voltage." - from the datasheet in question.

     

    I can't see anywhere on the datasheet what these internal resistances are or if it is even consistent since the output voltage depends largely on the ratio of these two resistors.

     

    From the two examples for the fixed XT50 we can work out the internal resistance, but I don't get consistent results:

     

    5V=1.25V(1+R2/R1) -> R2/R1 constant

    5.3V=1.25V(1+(R2+50Ohm)/R1) -> R1=50Ohm x 1.25/0.3=208Ohm

    12V=1.25V(1+(R2+2kOhm)/R1) -> R1=2kOhm x 1.25/7=357Ohm - perhaps that's approximately 12V?

     

    At at any rate, I don't think this is well described by the datasheet. The fact that they included that use case seems to suggest it is supported but don't give the required information to work out the details. I guess it's one of those try it and see kind of designs. I've also got some adjustable regulators here I was planning to try but haven't had time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to johnbeetem

    I spotted that too but initially dismissed the idea since I thought they must be assuming constant current drain for those figures based on my misunderstanding of how these regulators worked.

     

    From the description of the adjustable variety, and assuming the fixed version is basically the same with internal resistance, the GND pin is a constant current source (with unknown current due to unknown internal resistors) with a negligible contribution from the internal reference "pin".

     

    "For the fixed output devices R1 and R2 are included within the device and the ground current Ignd, ranges from 3.0 mA to 5.0 mA depending upon the output voltage." - from the datasheet in question.

     

    I can't see anywhere on the datasheet what these internal resistances are or if it is even consistent since the output voltage depends largely on the ratio of these two resistors.

     

    From the two examples for the fixed XT50 we can work out the internal resistance, but I don't get consistent results:

     

    5V=1.25V(1+R2/R1) -> R2/R1 constant

    5.3V=1.25V(1+(R2+50Ohm)/R1) -> R1=50Ohm x 1.25/0.3=208Ohm

    12V=1.25V(1+(R2+2kOhm)/R1) -> R1=2kOhm x 1.25/7=357Ohm - perhaps that's approximately 12V?

     

    At at any rate, I don't think this is well described by the datasheet. The fact that they included that use case seems to suggest it is supported but don't give the required information to work out the details. I guess it's one of those try it and see kind of designs. I've also got some adjustable regulators here I was planning to try but haven't had time.