Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RG1 1.8v regulator
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 231 replies
  • Subscribers 711 subscribers
  • Views 36411 views
  • Users 0 members are here
Related

RG1 1.8v regulator

e14 Contributor
e14 Contributor over 14 years ago

Ok, so in a different thread I threatened to remove RG1 and do some current measurements on it's output after seeing those thermal images that show it's not generating any heat...

 

Well, I did it tonight. Some photos here: https://picasaweb.google.com/selsinork/RPi18v

 

The jumper pins in the output let me either just put a jumper on and verify the Pi boots ok, or wire a multimeter in series to get some current readings.

 

The results were interesting to say the least. I had to go back and check I was reading the multimeter correctly, that it wasn't broken etc.

 

On initial power up I see a negative current for a second or so which then reverses to about 0.5mA (yes half a milliamp, that's not a typo) for a few seconds while we get the first sd-card accesses. Once we're booted and sitting at the login prompt the current reading fluctuates from around 0.001mA to maybe 0.04mA. 

 

I'm using the 40mA range on a decent Fluke multimeter, so I've no reason to doubt the results. There's obviously going to be some inaccuracy down at that level due to length of meter leads etc, but the result is fairly clear.  You'll understand why I was checking the meter was working and I was reading it correctly though image

 

 

So from there onto the next test, lets try completely disconnecting RG1 and see if the Pi boots while using the LAN9512 1.8v 'output'.  Yes it does! 

 

I think that's reasonably good indication that jamodio got it spot on, the lan9512 shouldn't be connected to the 1.8v plane and it's heat problems are going to be largely due to supplying current on it's 1.8v filter pin that it was never designed to do.

 

So anyone willing to pull RG1 off a Pi and verify my results ?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Just to expand on my original observations, the negative current I see on the output of RG1 seems to be due to it outputting 1.79v for a few seconds on initial powerup before stabilising at 1.804v. While the LAN9512 appears to power up at 1.805v and stay there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    My second order of Raspberry Pis arrived earlier in the week. A quick check shows one of them is running slightly warmer than the rest, not too much, I can still hold my finger on the LAN chip. I measure 1837mV at RG1 compared to 1793mV on one of the cooler ones (at idle, unmodified boards). Perhaps the LAN9512 core is running over voltage due to the external source and hence a bit hotter in this case. There may be multiple scenarios depending on components.

    I don't expect it will reduce the life of the chip unless it gets really hot, so I'll leave the rest alone unless LAN chips start dying all over the place.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    PeteL wrote:

     

    (I wonder if this post will dissolve into the Ether as soon as I post? image)

     

    You're in luck Pete!  The SHA-512 of the characters in the subject line multiplied by the current distance to Jupiter in furlongs added to the day of the week is not prime!

     

    Or maybe Loki was so stunned at selsinork's awesome chart that he forgot his usual duties. image

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    Pete, if your examination of Pi design around the LAN9512 leads to board changes in that area, you might wish to consider the problem of self-powered USB hubs attempting to power the Pi upstream through their A-B lead, which typically fails and sends the Pi into a rapid continuous reboot cycle and a consequent rapid power cycling of attached HDMI equipment.

     

    I reported it in a thread here -- http://www.element14.com/community/thread/19316?tstart=0

     

    Unfortunately this affects an official Farnell "Pi Accessory" hub, and I'm sure it's not the only one.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    My IR thermometer arrived yesterday and I was able to take some more measurments. The laser sight is mounted off to the side, so it is necessary to scan around to find the hot spot. Measurements taken after 20min of video playback over network.

     

    FN120508290 The first board the mod was applied to, still in a configuration where I can switch between the 1.8V power sources with a jumper.

      Powered from RG1 exclusively

        RG1 ____mV/IC3 ____mV idle (I forgot to measure this, will edit later as it might give an indication of each regulators ouput as a function of load)

        RG1 ____mV/IC3 ____mV playback

        45.7C

     

      Powered from IC3 exclusively

        RG1 ____mV/IC3 ____mV idle

        RG1 ____mV/IC3 ____mV playback

        49.1C - hot spot seems to be larger

     

    FN120744907 The second board which seemed to be running a bit warmer from the beginning

      Unmodified (RG1 removed and replaced in previous test. Heat stress may have influenced result)

        1837mV idle

        49.9C playback

     

      RG1 removed

        1837mV idle

        50.7C playback

     

      Mod applied

        RG1 1795mV/IC3 1845mV idle

        RG1 ____mV/IC3 ____mV playback

        46.0C - 49.5C (initially 46.0C after 20mins video playback, but it continued to rise for another 5 minutes or so)

     

    I thought I was getting consistent results until that last measurement. Not sure what happenned, maybe it needs more time to equilibriate or there was an action scene. I measured again after leaving it overnight and still read 47.2C and climbing after at least 20 mins _at idle_ (lan plugged in, but no traffic, no video playback), then after another 10 minutes back down to 46.0C. Maybe this is normal, at least we seem to have elliminated the dependance on video playback.

     

    The results seem to suggest that powering the 1.8V rail from IC3 might account for up to 4 degrees higher temperature on IC3. Looks like there might be quite a bit of variation in the LAN9512 chips based on the observed variation of VDD18CORE voltage so some may be affected more so than others.

     

    This doesn't really confirm if this bug is the source of the _really_ hot LAN chips, but my chips don't seem to be in that category anyway (50C seems to be the norm from what I see). Perhaps some chips handle this extra current drain more gracefully than others though.

     

    Here is the second attempt at the mod

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    My IR thermometer arrived yesterday

    I was looking at picking one up, but noticed that even rather expensive ones seem to have a minimum measurement 'spot' of something around 20mm which is rather larger than the lan9512. I was wondering just how that affects the readings..  Presumably they average the total emissions over whatever is in the sensors view somehow.

     

    Like you I don't have a Pi that runs as hot as some reports, and without one it's difficult to form a theory on what the cause is.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    selsinork wrote:

     

    My IR thermometer arrived yesterday

    I was looking at picking one up, but noticed that even rather expensive ones seem to have a minimum measurement 'spot' of something around 20mm which is rather larger than the lan9512. I was wondering just how that affects the readings..  Presumably they average the total emissions over whatever is in the sensors view somehow.

     

    Like you I don't have a Pi that runs as hot as some reports, and without one it's difficult to form a theory on what the cause is.

     

    yes the IR meter have there issues and you have to know it to get good readings and i have even an very good Fluke 568 there is on the high side of them and i dont use muchs because they crude in eletronics work and it is better to use an IR cam

     

    The Fluke 568 IR meter i am having is having and IR spot of (the number is is IR spot size and the distance from the surface)

    Spot 19mm @ 300mm distance

    Spot 18mm @ 900mm distance

    Spot 42mm @ 1500mm distance

     

    you also has to hold it at an right angle

     

     

    next time i will do some testing i will take both some IR images and use the IR meter and let you know what it is showing, but in the mean time try look at the images i have posted there is an graf showing the temparatura across the surface of the chip and you can clearly see the edges of the chip and that there is an very tinny hotsport at the center of the chip.

     

     

    Tooms

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    it is better to use an IR cam

    I'd love one.. I looked at prices. No way can I afford one image

     

    The Fluke 568 IR meter i am having

    Yeah, that's the one I was looking at, it was the only one I could find that gave a good explanation of the D:S relationship and that was what decided me not to bother getting one - my dodgy sensor stuck to the top center of the IC is likely more accurate image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Has anyone found the emissivity coefficients that we should use for the encapsulant on the chip (0.92 has been suggested)?

     

    I've asked a few chip suppliers FAEs and been met with a blank stare!  I guess that's why I still use thermocouples, but they are messy as I always gunk them up with heatsink compound.

     

    Cheers

     

    Pete

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi

     

    I am using the 0.95e on my Fluke 568 as this is the default one and it is for black plastic

     

    the 568 build in tabel has:

    0.93 paint

    0.95 plastic

    0.93 water

     

    an book i have about IR is having

    0.85 Brick, common

    0.94 Brick, refractory rough

    0.95 electrical tape black plastic

    0.92 Glass

    0.93 lacquer, bakelite

    0.94 paint average oil based

    0.94 paper black

    0.93 rubber

    0.92 tar paper

     

    (I have only listed the values there seems usagbol to this as the list is alot longer..)

     

    So based on this i will say around 0.93-0.95 so a good point will be 0.94e but as other users here is having IR meters and they are very likly fixed at 0.95e so i think it is best to use 0.95 so it is easyer to compire the results there is posted.

     

     

    Thomas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Seems like a good suggestion - as you say at least we can compare results with some confidence, I think the issue on resolution, spot size is also a complicating factor.  From what I understand you will get the average of the spot size so any real hot spots will be averaged away.

     

    I've been trying to find a IR lens that will give 10mm x 15mm as the total field of view.  Interestingly it gets even more complicated when you look at effective touch temperature and we need a gizmo called a "thermesthesiometer probe" but these are not commercially available as far as I have found - if you find one let me know.

     

    NASA (slightly old but the most recent I could find) have suggested that 45C is tolerable (indefinitely) for polished metal with an effective infinite heat capacity, and obviously a very high thermal conductivity, but this does not play well to our circumstances unless we measure less than that.

     

    So I think there are three issue in this thread:

     

    1) Touch temperature concern.

    2) Die temperature and effect on performance.

    3) Effect on functionality of USB? (Circumstances yet to be determined)**.

     

    I have not seen any reports that making the suggested mod fixes anything, I'm sure you will let me know if I've missed it.

     

    As always - comments welcome.

     

    Cheers

     

    Pete

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Hey Morgaine,

    As a somewhat related question. . . posible for you to suggest an affordable soldering iron with a small tip-to-grip ratio? Price range around $125 or so? Everything I come across is beaucoup bucks! I have a "hobbiest" iron from Adafruit but don't think it's going to work for me. Since I'm quite interested in this stuff I should invest in something I can use for eons..

    Thanks as always

    Peg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Hey Morgaine,

    As a somewhat related question. . . posible for you to suggest an affordable soldering iron with a small tip-to-grip ratio? Price range around $125 or so? Everything I come across is beaucoup bucks! I have a "hobbiest" iron from Adafruit but don't think it's going to work for me. Since I'm quite interested in this stuff I should invest in something I can use for eons..

    Thanks as always

    Peg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jamodio
    jamodio over 14 years ago in reply to e14 Contributor

    You are in the US right ?

     

    This is one option -> https://www.sparkfun.com/products/10553

     

    This is a better option -> http://www.newark.com/weller/wes51/analog-soldering-station-50w-120v/dp/92C1414?in_merch=Popular%20Soldering%20Stations&in_merch=Popular%20Products&MER=PPSO_N_C_SolderingStations_None

     

    And if you want digital (more expensive) -> http://www.newark.com/weller/wesd51/digital-soldering-station-50w-120v/dp/94C3885?in_merch=Popular%20Soldering%20Stations&in_merch=Popular%20Products&MER=PPSO_N_C_SolderingStations_None

     

    - J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 14 years ago in reply to e14 Contributor

    Peg,

    Check out Aoyue. http://www.aoyue.com/en/ArticleShow.asp?ArticleID=372

    For a little over $125 you might be able to get a combination station that also does hot-air. I have the just-hot-air station from them. (and the weller)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    I don't know of one yet, but I'm definitely in the market for one because under 14X binocular magnification it's really hard to control an iron with a long tip.  Currently looking through jamodio's links.

     

    Addendum:

     

    • The iron that comes with Adafruit's Hakko FX888 Soldering Station seems to be 190mm long without cord, and the tip looks kinda long.
    • Newark's Tech Data Sheet link for the Weller WES51 is currently down for me, I'll check again later.  On Farnell UK, no such model, might be US-only.
    • Weller have a "micro" range WHS-M,  http://uk.farnell.com/weller/whs-m-uk-eu/soldering-staion-40w-230v/dp/1729967 , which looks very small, but I can't see the actual tip length specified.

     

    General comment about Weller pricing ... ouch. image  It's clearly industrial pricing, hard to justify for very occasional use.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    I found other discussions regarding this question. Sorry to have jumped in to the wrong discission. . . I'm going to check into the chinese market. Thanks for the suggestions. I'll let you know what I come across for soldering irons. The "re-work" stations have me confused. . .like what would I ever need a hot air gun for??

    Best,

    Peg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to e14 Contributor

    Peg Wagner wrote:

     

    The "re-work" stations have me confused. . .like what would I ever need a hot air gun for??

    A soldering iron is great for soldering or desoldering a single terminal.  It doesn't work well if you want to heat up multiple terminals simultaneously, such as the two terminals of an SMT resistor.  And if you want to desolder the LAN9512 chip, forget it.  You have to heat up 64 tiny terminals plus a large ground pad under the chip which you can't even touch with the iron.

     

    The right hot air tool makes it possible to desolder these kinds the packages, and resolder all pins at the same time.  But you do need to know what you're doing (which I don't).