Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RG1 1.8v regulator
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 231 replies
  • Subscribers 711 subscribers
  • Views 36541 views
  • Users 0 members are here
Related

RG1 1.8v regulator

e14 Contributor
e14 Contributor over 14 years ago

Ok, so in a different thread I threatened to remove RG1 and do some current measurements on it's output after seeing those thermal images that show it's not generating any heat...

 

Well, I did it tonight. Some photos here: https://picasaweb.google.com/selsinork/RPi18v

 

The jumper pins in the output let me either just put a jumper on and verify the Pi boots ok, or wire a multimeter in series to get some current readings.

 

The results were interesting to say the least. I had to go back and check I was reading the multimeter correctly, that it wasn't broken etc.

 

On initial power up I see a negative current for a second or so which then reverses to about 0.5mA (yes half a milliamp, that's not a typo) for a few seconds while we get the first sd-card accesses. Once we're booted and sitting at the login prompt the current reading fluctuates from around 0.001mA to maybe 0.04mA. 

 

I'm using the 40mA range on a decent Fluke multimeter, so I've no reason to doubt the results. There's obviously going to be some inaccuracy down at that level due to length of meter leads etc, but the result is fairly clear.  You'll understand why I was checking the meter was working and I was reading it correctly though image

 

 

So from there onto the next test, lets try completely disconnecting RG1 and see if the Pi boots while using the LAN9512 1.8v 'output'.  Yes it does! 

 

I think that's reasonably good indication that jamodio got it spot on, the lan9512 shouldn't be connected to the 1.8v plane and it's heat problems are going to be largely due to supplying current on it's 1.8v filter pin that it was never designed to do.

 

So anyone willing to pull RG1 off a Pi and verify my results ?

  • Sign in to reply
  • Cancel
  • jamodio
    jamodio over 14 years ago in reply to johnbeetem

    Just a quick FYI, the NCP1117 you have on your board is most probably not from ON Semi but from a cheap chinese knock off.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to e14 Contributor

    Would you be satisfied knowing that you've been proven technically correct whilst successfully preventing the device from reaching those people whom the device may work within their requirements or that the device now costs $70.00 before adding the power supply, etc?

     

    There is no war and these are not issues related to "people's requirements," there are design errors and basic stuff that does not work as expected, and unless the requirements include blowing up TV's, collecting power supplies, USB hubs, keyboard, mouses and SD cards, like it or not the R-Pi has design and functional problems that need to be corrected so the people that are the main target for this device can receive what they expect.

     

    About the cost, RPF continues to provide a bogus and misleading statement on their home page ...

     

    -J

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to rew

    Roger Wolff wrote:

     

    Please provide an URL to the datasheet you found. I searched for NCP1117 and

    found: http://unihedron.com/projects/sqm-le/PDFspecs/NCP1117-D.PDF as the first hit. That one doesn't have figures 31 and 32. (but you're referring to figures 28 and 29 in that datasheet).

    http://www.onsemi.com/pub/Collateral/NCP1117-D.PDF

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to jamodio

    jamodio wrote:

     

    Just a quick FYI, the NCP1117 you have on your board is most probably not from ON Semi but from a cheap chinese knock off.

    Quite true, so we can pretty much expect that it won't regulate as precisely as a real ON Semi part -- where "real" has to be taken with a grain of element14 dioxide in these days of counterfeit chips.  OTOH, they probably did faithfully copy the NCP1117 circuit (and probably reverse-engineered the masks too) so I expect some  resistor value to work :-)

     

    Now if anyone tries the resistor trick, be sure that 1V8 doesn't get too high -- I wouldn't go above 1.9V as this would cause excess power consumption inside IC3 and the SDRAM.  Power consumption increases linearly with frequency and quadratically with voltage, so you don't want the extra switching power consumption of IC3's 1.8V logic to exceed what was saved by switching off IC3's internal LDO.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    Steve Lockett wrote:

     

    Convincing people relies on an aspect of humanity which most technical types I've dealt with seem to lack and that aspect is empathy

     

    Empathy is helpful in education because it assists the educator to understand why understanding is not being communicated, and in many cases this allows a different tack to be taken which can be successful.

     

    But empathy by the educator cannot override deliberate denial of facts and dismissal of rational arguments by the person they are trying to educate.  Nor can it overcome malicious responses like shutting down rational discussion, and that is what we are seeing in the RPF forums.  Perhaps it's not too surprising that denial has become so common among RPF forum posters, since they're following the appalling example set by RPF leaders.

     

    As I tried to explain earlier on, our topic here has nothing to do with "technical vs non-technical", nor "informed vs uninformed", which is how you tried to portray it.  It is targetted purely at those who willfully reject information and deny the whole process of critical inquiry because it conflicts with irrationally held beliefs or some agenda.

     

    Not knowing is the normal state of affairs, and we are all deeply immersed in it.  Not wanting to know and actively preventing others from learning through open discussion is a completely different condition, and it's deeply pathological for a thinking species.  I have no empathy with it whatsoever, because it is harmful to the educational goals of this project and a direct attack on the engineering process and the scientific method which are key to future generations of engineers.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to johnbeetem

    Figure 31 also confirms that if two NCP1117's are connected in parallel, the LDO with higher Vreg does switch off the LDO with lower Vreg.

    The engineer in me asks which electrical characteristic on the datasheet defines the voltage differential required to turn the regulator off? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to johnbeetem

    I spotted that too but initially dismissed the idea since I thought they must be assuming constant current drain for those figures based on my misunderstanding of how these regulators worked.

     

    From the description of the adjustable variety, and assuming the fixed version is basically the same with internal resistance, the GND pin is a constant current source (with unknown current due to unknown internal resistors) with a negligible contribution from the internal reference "pin".

     

    "For the fixed output devices R1 and R2 are included within the device and the ground current Ignd, ranges from 3.0 mA to 5.0 mA depending upon the output voltage." - from the datasheet in question.

     

    I can't see anywhere on the datasheet what these internal resistances are or if it is even consistent since the output voltage depends largely on the ratio of these two resistors.

     

    From the two examples for the fixed XT50 we can work out the internal resistance, but I don't get consistent results:

     

    5V=1.25V(1+R2/R1) -> R2/R1 constant

    5.3V=1.25V(1+(R2+50Ohm)/R1) -> R1=50Ohm x 1.25/0.3=208Ohm

    12V=1.25V(1+(R2+2kOhm)/R1) -> R1=2kOhm x 1.25/7=357Ohm - perhaps that's approximately 12V?

     

    At at any rate, I don't think this is well described by the datasheet. The fact that they included that use case seems to suggest it is supported but don't give the required information to work out the details. I guess it's one of those try it and see kind of designs. I've also got some adjustable regulators here I was planning to try but haven't had time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi all, first post from another refugee...

     

    selsinork wrote:

     

    Figure 31 also confirms that if two NCP1117's are connected in parallel, the LDO with higher Vreg does switch off the LDO with lower Vreg.

    The engineer in me asks which electrical characteristic on the datasheet defines the voltage differential required to turn the regulator off? 

     

    It's simply the way that the average linear regulator works (caveat alert: there's no schematic in my 1117 datasheet, so I'm assuming a standardish circuit). A linear reg (very basically) dumps current into a load while monitoring the voltage on it's output pin with reference to it's ground pin. A feedback loop varies the current from input to output to keep the output pin at setpoint. If you apply a voltage higher than setpoint to the output pin via a low impedance source the regulator has no way of dumping current from output to to ground internally, so the output voltage is pulled high. The internal error correction then takes a dump (technical term!). So then in this case, the regulator with even a marginally higher output voltage supplies all the current to the surrounding circuitry, while the other is shut down. As has already been mentioned there may be parasitic oscillation, thermal effects... allsorts going on too. There's no easy way to make fixed regulators work in parallel either - best to let the right one do all the work! What's the upper voltage limit of the 1V8 line anyway?

     

    Hope this all makes sense.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    There's a report today that adding a heatsink cures networking problems:

     

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=24&t=14478&start=4

    by lajos » Thu Aug 16, 2012 3:01 pm

     

    So I did an experiment. I installed heatsinks on both the SOC and memory chip. It's a small heatsink, the SOC still gets pretty hot (I don't have a surface thermometer, but it's not comfy to the touch.) But now the ethernet works without dropping out.

     

    Before heatsink, I would get at tops 40-50KB/s transfer rate, with frequent stalling, with heatsink I can move large files at ~2.0MB/s.

     

     

    Although there is a contrary report as well:

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=12097&start=247

     

    I added a radiator to the chip but there was no difference. Perhaps it was too small.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to e14 Contributor

    That is sort of a synonym for "unreliable."

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>