Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum First time login over ethernet?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 705 subscribers
  • Views 316 views
  • Users 0 members are here
  • raspberry_pi
Related

First time login over ethernet?

e14 Contributor
e14 Contributor over 14 years ago

I've loaded Wheezy on an SD card and from the flickering green LED I think it is booting fine.

 

I can't get a display when I connect the yellow RCA connector to my analog TV, and I don't have HDMI.

 

When I connect a crossover ethernet between my computer and the Raspberry Pi,  one yellow and two green LED's light up  -  I presume this indicates the ethernet is working OK.

 

Is there a way with an unmodified Wheezy distribution to connect to the Raspberry Pi over ethernet (using a crossover ethernet cable)?

 

If so, what is the IP address to use?

 

And does one use telnet, ssh, or what?

 

 

Thanks

 

Giacomo

  • Sign in to reply
  • Cancel
Parents
  • wallarug
    wallarug over 14 years ago

    You can not connect to the RPi on first boot-up with a cross-over cable. 

     

    Using a cross over cable means that you would have to configure the IP addresses on both devices (RPi and PC) manually. 

     

    You cannot do this without using a screen / router (to give your little Pi an IP address that it needs).

     

    If you do connect your RPi to a router/DHCP server, then you can ssh into it using a program such as PuTTy.  But even then, you would have to find-out your RPi's IP address some how.  If on a home network, you could use your router's User Interface or a program that tells you what is on your network. (for example FastResolver).

     

    Hope this helps

     

    Fergus

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • wallarug
    wallarug over 14 years ago

    You can not connect to the RPi on first boot-up with a cross-over cable. 

     

    Using a cross over cable means that you would have to configure the IP addresses on both devices (RPi and PC) manually. 

     

    You cannot do this without using a screen / router (to give your little Pi an IP address that it needs).

     

    If you do connect your RPi to a router/DHCP server, then you can ssh into it using a program such as PuTTy.  But even then, you would have to find-out your RPi's IP address some how.  If on a home network, you could use your router's User Interface or a program that tells you what is on your network. (for example FastResolver).

     

    Hope this helps

     

    Fergus