Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum New RPi seems not to work
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 32 replies
  • Subscribers 710 subscribers
  • Views 3963 views
  • Users 0 members are here
  • raspberry_pi
Related

New RPi seems not to work

e14 Contributor
e14 Contributor over 14 years ago

I have recently got an RPi, downloaded the Raspian OS, put the image on an SD card with WinImager and plugged in.

I use an USB power supply ( 5V 1A) and connected to a TV. I just wanted to see it all boot up before I got a suitable keyboard,

network connection, etc. Much to my disappointment, I saw nothing. I checked the voltage at TP1, and that appears OK ( 4.8V),

the power light is on and some chips appear to get warm.

Can anyone please suggest what to check to determine if I have a dud RPi or if I have done something incorrectly?

 

John

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 14 years ago

    There are some suggestions at the RasPi Troubleshooting Wiki: http://elinux.org/R-Pi_Troubleshooting#Power_.2F_Start-up.  Are you getting any flickering of the green OK LED?  That would suggest that the BCM2835 is reading the SD card and trying to boot.

     

    I've heard of people having trouble with Win32DiskImager.  Search for "Win32DiskImager" in the above search box and at the raspberrypi.org front page search box.

     

    Is it possible to use "dd" to write the SD card image on Ubuntu VM?  This way you avoid any issues with Win32DiskImager.

     

    You might also try a different SD card -- I think the OSes are doing better with SD card compatibility, but there may still be some RasPi doesn't like.  There's a list of known good and known bad SD cards at: http://elinux.org/RPi_VerifiedPeripherals#SD_cards.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to johnbeetem

    Thank you for these suggestions.

    I went through the list in the troubleshooting guide, and wrote to the card using dd rather than WinImager. But, was not able to get anything out of the RPi.

    I did try a different card ( all were 4GB), but whether either of them was on the list, I am not sure.

    I found it a little difficult to get sufficient ID to be sure. Certainly the file structure seems to be OK, and all the files mentioned in the discussions seem present. Oh and I also tried archlinux.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    I have now had some time to look at this.

    I was able to locate a power supply with a current indicator. This made it clear that the board was not functioning.

    On the board, the red power light was on, all other lights off.

    The measured values were as follows -

    Voltage@TP1( +5V) = 4.92V; ( implies that the fuse is not damaged)

    Voltage( +2.5V @C15) = 2.48V;

    Voltage( +1.8V@C9) = 1.8V;

    Current( total in ) = 0.17A. ( This should be at least 0.7A from what I can gather from the discussions.)

    ( Component designators from the schematic, 17Apr2012)

    Clearly, this is most likely the current for the peripheral circuit, and the CPU is not drawing current. No amount of fiddling with the rest is going to help.

    I think this is unambiguous evidence for a faulty board.

    Thank you to everyone who offered help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    This begs the Question....Is there other faulty boards out there?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    This begs the Question....Is there other faulty boards out there?