Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum How to get Micronext mnwd152b working?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 703 subscribers
  • Views 1467 views
  • Users 0 members are here
  • wifi
  • ethernet
  • raspberry_pi
Related

How to get Micronext mnwd152b working?

e14 Contributor
e14 Contributor over 14 years ago

Hello,

 

When I purchased my Raspberry Pi from Element14, I bought a MicroNext mnwd152b because Element 14 recommended it.

 

Now that I have set it all up, when I have the dongle connected to the USB connected on the RPi, as you boot up, it just says it is timing out when Modprobe runs and never seems to work. How do I get this working? I am running a current Raspbian Wheezy.

 

To get it running, I connected it via a cat5 cable which works nicely if you start doing networking operations as soon as it boots up. Unfortunately, if you leave it alone for a minute or two, you seem to lose connectivity - if you check ifconfig, eth0 no longer has an IP address assigned and you can no longer ping it from the rest of the network.

 

Any suggestions as to how I may diagnose this problem? Other computers on the network continue working fine through the FritzBox 7390 it is connected to.

 

Thanks in advance,

 

MarkL

  • Sign in to reply
  • Cancel
Parents
  • fustini
    fustini over 14 years ago

    Hi Mark,

     

    I believe this adapter would use the RTL8192cu driver.  I had tested a similar adapter the Asus N13.  In my Wi-Fi document, there is a link to the 8192cu driver which was compiled by a colleague in the UK (ajtag).  However, this kernel module needs to be recompiled to work with the kernel in the current Raspbian Wheezy image.  I'll ping him as I don't think he has done this yet.

     

    In the meantime, Adafruit has released there own version of Raspbian Wheezy to support the products they sell including RTL8192cu-based WiFi:

     

    http://learn.adafruit.com/adafruit-raspberry-pi-educational-linux-distro/occidentalis-v0-dot-1

     

    Their image might work for your adapter.

     

    Cheers,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fustini
    fustini over 14 years ago

    Hi Mark,

     

    I believe this adapter would use the RTL8192cu driver.  I had tested a similar adapter the Asus N13.  In my Wi-Fi document, there is a link to the 8192cu driver which was compiled by a colleague in the UK (ajtag).  However, this kernel module needs to be recompiled to work with the kernel in the current Raspbian Wheezy image.  I'll ping him as I don't think he has done this yet.

     

    In the meantime, Adafruit has released there own version of Raspbian Wheezy to support the products they sell including RTL8192cu-based WiFi:

     

    http://learn.adafruit.com/adafruit-raspberry-pi-educational-linux-distro/occidentalis-v0-dot-1

     

    Their image might work for your adapter.

     

    Cheers,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • fustini
    fustini over 14 years ago in reply to fustini

    I was able to use the Asus USB-N13 without any problems with Adafruit's image (http://learn.adafruit.com/adafruit-raspberry-pi-educational-linux-distro/occidentalis-v0-dot-1).  It has the 8192cu driver module compiled into the kernel.  I believe the Micronext uses the same driver.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to fustini

    pi@raspberrypi:~$ cat /proc/config.gz  |gunzip - |grep 8192

    # CONFIG_RTL8192SE is not set

    # CONFIG_RTL8192DE is not set

    CONFIG_RTL8192CU=y

    CONFIG_RTL8192C_COMMON=m

    pi@raspberrypi:~$ grep 8192cu /lib/modules/3.1.9adafruit+/modules.*

    /lib/modules/3.1.9adafruit+/modules.builtin:kernel/drivers/net/wireless/rtl8192cu/8192cu.ko

    pi@raspberrypi:~$ lsusb

    Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub

    Bus 001 Device 002: ID 0424:9512 Standard Microsystems Corp.

    Bus 001 Device 003: ID 0424:ec00 Standard Microsystems Corp.

    Bus 001 Device 004: ID 0b05:17ab ASUSTek Computer, Inc. USB-N13 802.11n Network Adapter (rev. B1) [Realtek RTL8192CU]

    pi@raspberrypi:~$ iwconfig

    lo        no wireless extensions.

     

     

    eth0      no wireless extensions.

     

     

    wlan1     unassociated  Nickname:"<WIFI@REALTEK>"

              Mode:Auto  Frequency=2.412 GHz  Access Point: Not-Associated  

              Sensitivity:0/0 

              Retry:off   RTS thr:off   Fragment thr:off

              Power Management:off

              Link Quality:0  Signal level:0  Noise level:0

              Rx invalid nwid:0  Rx invalid crypt:0  Rx invalid frag:0

              Tx excessive retries:0  Invalid misc:0   Missed beacon:0

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to fustini

    Hi Drew,

     

    I have just created an Adafruit sdcard, so when the kids are off to school in the morning I will give it a try. From what you say it should work fine.

     

    Cheers,

     

    MarkL

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to e14 Contributor

    Great, Mark.  I'll be interested to know how it works out for that adapter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to fustini

    Hi Drew,

     

    I got it up and running with the Adafruit image, but the results - while better than Wheezy - are still not perfect.

     

    It  still seems that if left for some period of time, it loses connectivity (both ethernet and wifi) from which it cannot recover other than via reboot. I do notice however that if you do an ifconfig / iwconfig the IP address still shows, but you get timeouts / host resolution failures. I tried with both eth/wlan, and singly but same problem. When one goes, all go down :-(

     

    I did an apt-get upgrade but that doesn't seem to make any difference.

     

    All of the peripherals connect via a powered hub.

     

    I tried monitoring /var/log/messages and it seems to spend an inordinate amount of time trying to put the wifi dongle into power save mode just to then say that the dongle is currently busy. Is there some way of telling the RPi it is on AC and not to powersave anything?

     

    Also, every time it receives a wifi AES packet, it logs the fact. I suspect that once RPi gets bedded down, someone is going to have to make some hard decisions as to what gets put in the log - as we do not have an infinite harddisk in this case :-(

     

    So I guess the Adafruit is a step forward, but the connectivity over time problems still exist which appears to be common given troubleshooting forum messages.

     

    Cheers,

     

    MArkL