Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Help needed on Monitor settings problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 708 subscribers
  • Views 1262 views
  • Users 0 members are here
  • raspberry_pi
Related

Help needed on Monitor settings problem

cityswift
cityswift over 14 years ago

Hi I have just set up my new Pi B with Wheezy Linux and find that the HDMI output gives the correct picture on my 32" tv,  but when I use the RCA composite video output to feed the 15" LCDtv with 1024X768 resolution which I want to use on a permanent basis the picture is incorrectly sized and does not show the top and bottom of the raspberry logo and the text is faint. Is there a file somewhere that needs changing to give the correct size?    image

  • Sign in to reply
  • Cancel
Parents
  • GreenYamo
    GreenYamo over 14 years ago

    Hello,

     

    you need to play about with the config file, details are available here:

     

    http://elinux.org/R-Pi_Troubleshooting#Display

     

    Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cityswift
    cityswift over 14 years ago in reply to GreenYamo

    Hi Steve thanks for your reply. I have made the changes to the config.txt file as detailed in your link and saved it and then rebooted but there is no change to the display. There is a line in the file which states "overscan=0" and I assume this means overscan is off as opposed to "overscan=1" which would mean overscan is on. Can you confirm if that is the case? Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to cityswift

    overscan=1 / overscan=0 is NOT a command in the config.txt file.

     

    disable_overscan=               (either 1 or 0, where 0=off and 1=on)

     

    ...is a command in the config.txt file.

     

    the other commands allowed in the file are:

    overscan_left=

    overscan_right=

    overscan_top=

    overscan_bottom=

     

    any value can go after "=" but note that the value is the number of pixels you want to increase (positive value) or decrease (negative value --> eg. = -30).

    disable_overscan must = "0" when using the above 4 commands.

     

    Fergus

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • wallarug
    wallarug over 14 years ago in reply to cityswift

    overscan=1 / overscan=0 is NOT a command in the config.txt file.

     

    disable_overscan=               (either 1 or 0, where 0=off and 1=on)

     

    ...is a command in the config.txt file.

     

    the other commands allowed in the file are:

    overscan_left=

    overscan_right=

    overscan_top=

    overscan_bottom=

     

    any value can go after "=" but note that the value is the number of pixels you want to increase (positive value) or decrease (negative value --> eg. = -30).

    disable_overscan must = "0" when using the above 4 commands.

     

    Fergus