Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Wiring a motor to the RPi?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 63 replies
  • Subscribers 707 subscribers
  • Views 10481 views
  • Users 0 members are here
  • help
  • rc
  • pi
  • control
  • raspberry_pi
  • please
  • motor
  • raspberr
Related

Wiring a motor to the RPi?

wallarug
wallarug over 14 years ago

What do I need?

 

I am told that I need some transitors.  I have a 12v powerpack and 2 x12v motors.  How do I set this up so that I don't blow-up the RPi and that I can control the motors through the GPIO?

 

I have a gertboard on the way but I would like to see if I can do it without it first.

 

I have little knowlegde about transitors and electronics but I do know how to build circuits.

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 14 years ago

    If all you want to do is turn a small DC motor on and off, all you need is Gert van Loo's circuit in this thread's 7th post: http://www.raspberrypi.org/phpBB3/viewtopic.php?f=44&t=13473.  The motor is driven by an NPN Darlington Pair (http://en.wikipedia.org/wiki/Darlington_pair), which is a great way to convert a small current into a really big current.  The three diodes in series are for people are afraid the Darlington pair might accidentally conduct from collector to base.  Gert says they're not necessary, but with 12V present I'd worry about framboise flambée and put them in. 

     

    The diode next to the motor coil is critically important.  It's called a flyback diode (http://en.wikipedia.org/wiki/Flyback_diode).  When you turn on the transistor, the flyback diode is reverse-biased and has no effect.  However, when you turn off the transistor, the magnetic field in the motor will cause current to continue to flow for a while.  If that current can't go anywhere (because the transistor is off), it will charge the node to a very high voltage and turn the transistor into a fuse and possibly destroy anything connected to the transistor.  It's how spark plugs work.  The flyback diode gives the current somewhere safe to go to prevent Spitzensparken.  The diode should have a current rating higher than the current through the motor.

     

    Gert doesn't give a value for the resistor between the GPIO and the base of the Darlington pair.  I'd start with 1 KOhm which gives you 3.3 mA.  But then, I usually start with 1K image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to johnbeetem

    Could someone confirm if the GPIOs are a ground or send out signals.  I think they are grounds but I can't be certain.

     

    If they are grounds, then how would the transitor work if it is a NPN?  wouldn't you need some positive current comming from somewhere?

     

    Sorry if these are silly questions but I am only learning.

     

    could someone also point me towards a sample code please.  I have heard that the code is the tricky bit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    Fergus Byrne wrote:

     

    How do I install the RPi-GPIO-0.3.1a library onto my Raspberry Pi? This is very important right now so that I can code some LEDs.

    i have installed the above python library.  But I still don't know how to wire the motor to the raspberry pi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    Look up an H Bridge circuit.  I have had good luck with this kit with an Arduino.  I made a roller robot.  I tried and failed with TIP102 and TIP107 but I am clumsier than most.  If you go this route,

    buy extra transistors in case you fry them.

     

    Look at http://www.mcmanis.com/chuck/robotics/tutorial/h-bridge/.  Follow the links to basic transistor etc.

     

    The H bridge would have one output for forward and one for backwards.  The kit controls 2 motors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    Ken Seymour wrote:

     

    Look up an H Bridge circuit.  I have had good luck with this kit with an Arduino.  I made a roller robot.  I tried and failed with TIP102 and TIP107 but I am clumsier than most.  If you go this route,

    buy extra transistors in case you fry them.

     

    Look at http://www.mcmanis.com/chuck/robotics/tutorial/h-bridge/.  Follow the links to basic transistor etc.

     

    The H bridge would have one output for forward and one for backwards.  The kit controls 2 motors.

    Could you draw up a schematic diagram for me if I use this: https://www.adafruit.com/products/807.  My friend has informed me that a H-Bridge is required and I found this IC and I think that it could work nicely.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    I have not created schematics except with pencil and paper.  I noticed that his is a 5 Volt chip and the Pi outputs are 3.3 Volt.

     

    I am working on a schematic with 2N3906 transistors to level-shift the outputs.  If you power the motors off 5V as well, it avoids two power supplies.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    Motors are powered off 12volts.  Did you look at the Double H-Bridge IC I posted earlier?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    Here is the schematic.  JP1 is meant to be the motor.  I should mention that the transistor logically invert their signals.

    When the GPIO is high, the chip input is low. So from the Pi's perspective, they are active when they are zero.

     

    You need two power supplies.  The solarbotics board has an on board regulator to provide the +5 volts.

     

    The Pi only has one PWM output, so you could do PWM in software but get the motor going fast first.

     

    Make sure the motor fits within the chip's power output max or just buy extra chips.

     

    The 2N2222A2N2222A is cheap.  Buy extra.  I live in the US so I would get them here. http://www.jameco.com/webapp/wcs/stores/servlet/Product_10001_10001_38236_-1.

     

    Or use Newark/element 14, or Digikey, or Mauser.

    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    Thanks Ken.  Great work.  I will test later

     

    What about the double H-Bridge chip in the earlier post?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    The schematic is for TI's L293D chip, which was posted above in a link from Adafruit.

    It is a dual H-Bridge motor driver.

     

    The E on the end of the part number is from the Eagle part library, but the pinout is the same.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    Thanks for informing this of that fact.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    Ken Seymour wrote:

     

    The schematic is for TI's L293D chip, which was posted above in a link from Adafruit.

    It is a dual H-Bridge motor driver.

     

    The E on the end of the part number is from the Eagle part library, but the pinout is the same.

    How can I get PWM working on the motors? Can you please give me instructions on software and/or extra hardware required (input device)  for PWM to work.

     

    Thanks for all your help so far.

     

    Hardware such as what gert used in his video (the slider at 3:40):

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    Ken Seymour wrote:

     

    The schematic is for TI's L293D chip, which was posted above in a link from Adafruit.

    It is a dual H-Bridge motor driver.

     

    The E on the end of the part number is from the Eagle part library, but the pinout is the same.

    How can I get PWM working on the motors? Can you please give me instructions on software and/or extra hardware required (input device)  for PWM to work.

     

    Thanks for all your help so far.

     

    Hardware such as what gert used in his video (the slider at 3:40):