Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Wiring a motor to the RPi?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 63 replies
  • Subscribers 710 subscribers
  • Views 10355 views
  • Users 0 members are here
  • help
  • rc
  • pi
  • control
  • raspberry_pi
  • please
  • motor
  • raspberr
Related

Wiring a motor to the RPi?

wallarug
wallarug over 14 years ago

What do I need?

 

I am told that I need some transitors.  I have a 12v powerpack and 2 x12v motors.  How do I set this up so that I don't blow-up the RPi and that I can control the motors through the GPIO?

 

I have a gertboard on the way but I would like to see if I can do it without it first.

 

I have little knowlegde about transitors and electronics but I do know how to build circuits.

  • Sign in to reply
  • Cancel
Parents
  • yvanttt
    yvanttt over 13 years ago

    as an example use pins 5 and 6 (pins 20 and 22 on J25) on the atmega328 and connect them to the motor_a and motor_b input (J5) on the gertboard.

    Then the uart TXD (gpio pin22) of the raspberry to the RXD (pin 2 of the atmega, pin 1 of J64)

     

    Then it is a simple mater to program the atmega328 to intercept the bytes sent from the raspbery and copy them to the 2 PWM ports.

     

    http://arduino.cc/en/Reference/AnalogWrite

    http://arduino.cc/en/Reference/Serial

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • yvanttt
    yvanttt over 13 years ago

    as an example use pins 5 and 6 (pins 20 and 22 on J25) on the atmega328 and connect them to the motor_a and motor_b input (J5) on the gertboard.

    Then the uart TXD (gpio pin22) of the raspberry to the RXD (pin 2 of the atmega, pin 1 of J64)

     

    Then it is a simple mater to program the atmega328 to intercept the bytes sent from the raspbery and copy them to the 2 PWM ports.

     

    http://arduino.cc/en/Reference/AnalogWrite

    http://arduino.cc/en/Reference/Serial

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • wallarug
    wallarug over 13 years ago in reply to yvanttt

    Don't have a gertboard and won't get it for a while (Farnel issue).  But I am going to get an adruino eleven with ATMEGA328p which will help me do what I want.  I will look at your links though. 

     

    The only problem I have with coding such a chip.  I have no experience and will require massive amount of help with the coding in python (I know some already) or C (which sounds easy to learn).