Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Wiring a motor to the RPi?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 63 replies
  • Subscribers 710 subscribers
  • Views 10355 views
  • Users 0 members are here
  • help
  • rc
  • pi
  • control
  • raspberry_pi
  • please
  • motor
  • raspberr
Related

Wiring a motor to the RPi?

wallarug
wallarug over 14 years ago

What do I need?

 

I am told that I need some transitors.  I have a 12v powerpack and 2 x12v motors.  How do I set this up so that I don't blow-up the RPi and that I can control the motors through the GPIO?

 

I have a gertboard on the way but I would like to see if I can do it without it first.

 

I have little knowlegde about transitors and electronics but I do know how to build circuits.

  • Sign in to reply
  • Cancel
Parents
  • yvanttt
    yvanttt over 13 years ago

    These Arduino are the easiest to program.

    They made an IDE package that works on Windows, OS max and Linux 32 or 64 bits. These devices uses C

     

    They have all the major function already available on their site "www.arduino.cc".

    Plus they have "sheild" that can get you started then use the sheild schematics to build your permanent setup.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • yvanttt
    yvanttt over 13 years ago

    These Arduino are the easiest to program.

    They made an IDE package that works on Windows, OS max and Linux 32 or 64 bits. These devices uses C

     

    They have all the major function already available on their site "www.arduino.cc".

    Plus they have "sheild" that can get you started then use the sheild schematics to build your permanent setup.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • wallarug
    wallarug over 13 years ago in reply to yvanttt

    Ok, here is my idea:

    Using some of the set-up features that @aonsquared used with his Robot/Rover thing.

     

    image

    Using a 5 volt supply to power the Raspberry Pi and the Powered hub.

     

    The Raspberry Pi will send commands to the Ardunio Eleven (which I still have to get), which will control the Two Motors through a H-bridge and PWM.

     

    That camera will be powered through the 10 port hub, along with the Ardunio and the W/LAN dongle.

     

    The Motors will be powered though a 12 volt supply (8 AA batteries).

     

    All the commands will be sent through an Ad-Hoc Network to a Laptop running Windows 7 Pro 64 bit.  I think that I will use by Joystick to move the Motors but I don't know how that is going to work as @aonsquared used a PS3 controller instead. (Saitek ST90 is the Joystick).

     

    The LCD display will have the IP address so that I know exactly what it is whenever.

     

    The Raspberry Pi will host a live webcam feed though an old Logitec Camera I have lying around.

     

     

    One question is: Will PWM work on the motors through the Ardunio if I have the 12 volts going directly into the H-bridge Chip?   

     

     

    What do you think?