Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi can't remove micro USB power cable
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 705 subscribers
  • Views 5026 views
  • Users 0 members are here
  • raspberry_pi
Related

Raspberry Pi can't remove micro USB power cable

e14 Contributor
e14 Contributor over 14 years ago

When I got my RasPi I was so excited that I used the first micro USB cable I could find to power it up. 

 

The cable works but I cannot unplug it!  I've already put more pressure on the micro USB port than I feel comfortable doing. 

 

Has anyone else had this problem or know of a solution?

 

Thanks!

 

Dan

 

  • Sign in to reply
  • Cancel
  • johnbeetem
    johnbeetem over 14 years ago

    A Micro USB plug has two tiny clips on the wide surface which mate with two holes in RasPi's USB jack S1.  Here's a fairly high resolution photo of a Micro USB plug at Wikipedia: http://en.wikipedia.org/wiki/File:MicroB_USB_Plug.jpg.  Normally those two clips are triangular so you can pull the plug out with some side-to-side wiggling.  I think in your case one or both clips are bent in such a way that you cannot pull the cable out.  See if you can push the clip down with a precision screwdriver or other small object while you gently wiggle the plug sideways as you pull it out.  You may need a helper with small hands.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    This helped, thank you so much! 

     

    The problem seems to be in the micro USB port on the RasPi.  The cable doesn't get stuck in any of my other devices that use a micro USB cable.  I plugged it into the RasPi again and had the same problem.  However, now only one side of the plug is stuck, the other side will wiggle a little bit.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jakwai
    jakwai over 5 years ago in reply to johnbeetem

    Thank you! I was trying to remove the cable with many different small "objects" and it didn't work. In the end the side-to-side wiggle solved the problem!

     

    Greetings,

    Jakob