Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi can't remove micro USB power cable
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 705 subscribers
  • Views 5028 views
  • Users 0 members are here
  • raspberry_pi
Related

Raspberry Pi can't remove micro USB power cable

e14 Contributor
e14 Contributor over 14 years ago

When I got my RasPi I was so excited that I used the first micro USB cable I could find to power it up. 

 

The cable works but I cannot unplug it!  I've already put more pressure on the micro USB port than I feel comfortable doing. 

 

Has anyone else had this problem or know of a solution?

 

Thanks!

 

Dan

 

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 14 years ago

    A Micro USB plug has two tiny clips on the wide surface which mate with two holes in RasPi's USB jack S1.  Here's a fairly high resolution photo of a Micro USB plug at Wikipedia: http://en.wikipedia.org/wiki/File:MicroB_USB_Plug.jpg.  Normally those two clips are triangular so you can pull the plug out with some side-to-side wiggling.  I think in your case one or both clips are bent in such a way that you cannot pull the cable out.  See if you can push the clip down with a precision screwdriver or other small object while you gently wiggle the plug sideways as you pull it out.  You may need a helper with small hands.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 14 years ago

    A Micro USB plug has two tiny clips on the wide surface which mate with two holes in RasPi's USB jack S1.  Here's a fairly high resolution photo of a Micro USB plug at Wikipedia: http://en.wikipedia.org/wiki/File:MicroB_USB_Plug.jpg.  Normally those two clips are triangular so you can pull the plug out with some side-to-side wiggling.  I think in your case one or both clips are bent in such a way that you cannot pull the cable out.  See if you can push the clip down with a precision screwdriver or other small object while you gently wiggle the plug sideways as you pull it out.  You may need a helper with small hands.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jakwai
    jakwai over 5 years ago in reply to johnbeetem

    Thank you! I was trying to remove the cable with many different small "objects" and it didn't work. In the end the side-to-side wiggle solved the problem!

     

    Greetings,

    Jakob