Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum GPIO output from keyboard
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 705 subscribers
  • Views 1073 views
  • Users 0 members are here
  • gpio;
  • help
  • robot;
  • raspberry_pi;
  • rpi;
  • raspberry_pi
Related

GPIO output from keyboard

wallarug
wallarug over 14 years ago

Does anyone know how to code a python script that will be able to achieve this WITHOUT pressing enter each time?

 

I am building a car powered by the RPi and I was wondering if this was achieveable.  Here is what I have so far:

 

print "The controls are as follows: "

print "w = forward; a = left; s = backwards; d = right "

a = raw_input("Press a key to move the Robot: ")
while a:
    a = raw_input("Press a key to move the Robot: ")
    if a.lower() == 'w':
        print "working forward"
    if a.lower() == 'a':
        print "working left"
    if a.lower() == 's':
        print "working backwards"
    if a.lower() == 'd':
        print "working right"

 

Any Idea how I would Modify this to do what I want?

 

BTW: I know how to get the GPIOs working but I can't test then in a shell, so I just used print functions/output.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Console I/O in Python is OS dependent.

    On Posix compliant systems, such as Linux and Unix,

    you would put the terminal in "cbreak" mode,

    http://en.wikipedia.org/wiki/Cbreak_mode

    which doesn't wait for a whole line to be entered.

     

    Python docs are here:

    http://docs.python.org/library/tty.html

     

    For fancy uses, see the "curses" library, in cbreak mode.

    http://docs.python.org/howto/curses.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    Console I/O in Python is OS dependent.

    On Posix compliant systems, such as Linux and Unix,

    you would put the terminal in "cbreak" mode,

    http://en.wikipedia.org/wiki/Cbreak_mode

    which doesn't wait for a whole line to be entered.

     

    Python docs are here:

    http://docs.python.org/library/tty.html

     

    For fancy uses, see the "curses" library, in cbreak mode.

    http://docs.python.org/howto/curses.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    Can I just clarify,

     

    I am going to be using the Raspberry Pi (Linux).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    Should I use getch()?  I have done some research and this seems to be the way to go.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    Is getch() available on linux?  I think it's only available

    in the Windows msvcrt library, or in the curses library.

     

    On linux you will want to set the terminal in "cbreak" mode,

    and then read the character using

       ch = sys.stdin.read(1)

     

    when you are done, you will probably want to restore the

    terminal to normal mode.

     

    You can set "cbreak" mode on linux using

       tty.setcbreak(fd[, when])

    as shown here:

       http://docs.python.org/library/tty.html

     

    There is an example here:

       http://www.dzone.com/snippets/cross-platform-getch-python

    although it uses "raw" mode instead of "cbreak" mode,

    and doesn't restore the old settings.

     

    The difference between "raw" mode and "cbreak" mode is that

    control-C works normally in "cbreak" mode, but not in "raw" mode.

     

    There is an example of restoring the normal tty mode here:

       http://docs.python.org/library/termios.html#module-termios

     

    Alternately, you can use the curses library:

     

    import curses

    stdscr = curses.initscr()

    curses.cbreak()

    c = stdscr.getch()

    curses.nocbreak()

    curses.endwin()

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    Thanks for the responce.  I will look into cbreak mode and see if I can get it working on linux. image