I just found this: http://au.element14.com/raspberry-pi/raspbrry-modb-512m/sbc-raspberry-pi-model-b-512mb/dp/2191863
Is this a raspberry pi with 512Mb RAM or is this a joke.
I just found this: http://au.element14.com/raspberry-pi/raspbrry-modb-512m/sbc-raspberry-pi-model-b-512mb/dp/2191863
Is this a raspberry pi with 512Mb RAM or is this a joke.
Now it's official. A 512MB Pi, and we certainly as more often than not heard it here first.
Thank you all deep miners of the Pi caverns to keep us all on the forefront of knowledge.
Ray
P.S. Dear Distro maintainers please do not suddenly make all your Pi OS distros twice as big and only suitable for the larger memory machines.
Ray Hughes wrote:
Now it's official. A 512MB Pi, and we certainly as more often than not heard it here first.
Thank you all deep miners of the Pi caverns to keep us all on the forefront of knowledge.
Ray
P.S. Dear Distro maintainers please do not suddenly make all your Pi OS distros twice as big and only suitable for the larger memory machines.
Pretty sure that the people here had no more idea that a 512 was imminently on the way than anywhere else. Lots of people predicting it eventually (well, obvious it was going to happen at some point), but not sure anyone predicted it so soon. Anyone can make Pi in the the sky predictions, its getting the timing right that's the important bit, and I don't reckon anyone saw this one coming so soon.
Making a distro twice as 'big' doesn't mean you need twice the memory - the kernel stays the same size (within reason) on any platform. Linux uses swap, so lower memory system will still work, but slower.
Bill.
@Jamodio. I was told a few days ago that this was not a place for name calling. You just called me a moron (I assume you were talking to me). Don't call me a moron, that not very nice - or are you not a very nice person? I'm pretty sure that classes as name calling anyway. Even where I'm from.
RE: 1GB RAM chip - are you sure that would work on Raspberry PI, because a quick read of the specs would indicate that it wouldn't. And I'm not convinced that device is available.
@Morgaine. A few hours ago the device was indeed mythical. It has now, with the announcement, become factual. I'm not backpedalling and I also I don't delete my old posts when I'm wrong. Mythical does not imply it doesn't exist, merely that there is not enough evidence to say that it does exist - yet. Please don't read stuff in to my posts that isn't there.
I'm not going to work with you btw. Certainly not the last two posters anyway, you're mean to people. Happy to help out with others who don't feel to need to call people Morons.
As to the Raspberry Pi Foundation not being forthcoming? Like what? Should they have told people in advance there was a move to 512MB? That would be commercial suicide. What are they not forthcoming about that would be of use for their target market? Today we learnt that there is a 512device, we also learnt that the accelerated X driver is under serious development. Thats damn straight stuff! Do you want them to tell you all their commercial stuff? Or what?
Bill (not a moron despite what Jamodio says)
jamodio wrote:
Instead being a moron contesting anything that anybody says (starting with your useless comment about version numbers,) you should do more due diligence about what is going on, and who is working on what. It was not difficult to envision that sooner or later the Rpi was going to have 512MB RAM since RPF was already working and testing preliminary images of Android 4.0.
BTW, your citation and assumed authoritative answer from one of the moderators on the RPi forum is not valid ...
http://omapworld.com/4430_8Gb__DDR_PoP_111_1003122.pdf
I don't know what is your mission here but so far the only thing you are contributing is noise and additional fuel for flame wars.
Actually, forgot to ask something here - despite your inability to be polite, what's Android got to do with 512MB, and I don't remember talking about version numbers- what's up there dude?
My mission? To provide an antidote to the bitter vitriol and bile spouting from some of the posters on this site, who have an over exagerated sense of thier own importance, just 'cos they got banned from the other one. or something like that. Don't actually have a official mission statement, so I make it up as I go along. And it's the middle of the night, I'm tired aftyer working 14 hours straight, so it might change at short notice.
jamodio wrote:
Well you are failing in your mission and even if you were in front of my face I'll still call you a moron, I don't feel the need to be polite with people like you that seems to have every intent to create flame wars.
Good luck with that. Next time you are in the Far East give me a shout.
ps. See my previous comment.
Since my original reply stating that the 1GB ram package quoted by Jamodio has been deleted, presumably because he didnt like to be shown to be wrong, I'll reiterate. That package will not work on a Raspberry Pi. It's the right physical size, and the right sort of DDR2, but it's interface is different and it has a different number of balls in its BGA array to find on the Raspberry Pi SoC. I leave it as an exercise for the reader to compare the datasheet with those of the current 256 RAM chips used on the Rasberry Pi for the exact reason.
Billy Thornton wrote:
My prediction now; there will never be a 1GB version. You heard it here first! (Citation : no one makes 1GB ddr2 PoP ram, and its an old technology, so no-one ever will).
Billy, you forgot to include a smiley 
On Sept 2 earlier in this thread, John Beetem wrote:
The RasPi forum has just twigged to the 512MB version: see this thread. On 31 August jamesh said that 512MB is the limit for the current board. He didn't give away any RasPi Foundation plans.
Now, here's my prediction: there won't be a 1GB version with the BCM2835. But there will most likely be future RasPis with different SoCs, perhaps even ones with a more powerful general-purpose CPU or multiple CPUs so you can dedicate one to USB and other housekeeping.
I didn't delete anything and BTW my reply to you was also deleted. I never said that that particular part would work with the RPi, just a proof that somebody out there is actually working on 1GB DDR2 PoP memory.
jamodio wrote:
I didn't delete anything and BTW my reply to you was also deleted. I never said that that particular part would work with the RPi, just a proof that somebody out there is actually working on 1GB DDR2 PoP memory.
You certainly implied it. Although I have realised that in my posts I omitted to say there I was refereing to the Raspberry Pi SoC, not 1Gb Pop in general. I just assuemd that's what we were talking about. Sorry for not being clear - there are quite a few 1GB PoP already out there in devices being sold - but none that fit on the 2835, and none, as far as I know, in the pipeline. It's old tech, and modern SoC have more channels and more chip selects, so that pipline ain't gonna be filled up.
John Beetem wrote:
Billy Thornton wrote:
My prediction now; there will never be a 1GB version. You heard it here first! (Citation : no one makes 1GB ddr2 PoP ram, and its an old technology, so no-one ever will).
Billy, you forgot to include a smiley
On Sept 2 earlier in this thread, John Beetem wrote:
The RasPi forum has just twigged to the 512MB version: see this thread. On 31 August jamesh said that 512MB is the limit for the current board. He didn't give away any RasPi Foundation plans.
Now, here's my prediction: there won't be a 1GB version with the BCM2835. But there will most likely be future RasPis with different SoCs, perhaps even ones with a more powerful general-purpose CPU or multiple CPUs so you can dedicate one to USB and other housekeeping.
But that's cheating! I'd put money on their being a new Raspberry Pi with better SoC and 1GB but only when the p[rice point meets what they sell for now. And that will be a year at least.
The process of design, manufacture and release takes months end to end. During that period, the 512MB version was never mythical, because mythical denotes products of the imagination which do not exist and will never exist. In this case the 512MB version was completely tangible to RPF over that period, and to the rest of us it was a product with steadily increasing probability of existence as facts about it emerged piecemeal here and there.
This is how the community has to obtain its information by combining hints from various sources, because the Foundation's planning is not open about this. Calling fellow members' estimates "myths" is not helpful here.
The process of design, manufacture and release takes months end to end. During that period, the 512MB version was never mythical, because mythical denotes products of the imagination which do not exist and will never exist. In this case the 512MB version was completely tangible to RPF over that period, and to the rest of us it was a product with steadily increasing probability of existence as facts about it emerged piecemeal here and there.
This is how the community has to obtain its information by combining hints from various sources, because the Foundation's planning is not open about this. Calling fellow members' estimates "myths" is not helpful here.