Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RPi rev 2.0 explained
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 55 replies
  • Subscribers 709 subscribers
  • Views 8514 views
  • Users 0 members are here
Related

RPi rev 2.0 explained

e14 Contributor
e14 Contributor over 14 years ago

Eben has a front-page story up explaining rev 2.0.

It does fix the 1.8V problem, although no credit where

credit is due to Jamodio or any of the others here for

finding, characterizing, and reporting the problem.

 

No mention that I can see of FCC/CE residential

certification.  I assume the needed minor pcb changes

were made, but perhaps certification has not been

done yet.

 

http://www.raspberrypi.org/archives/1929

 

p.s.

   hopefully element14 will explain to their customers

how to be sure to get rev 2.0 when ordering.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    I wrote:

    >No mention that I can see of FCC/CE residential certification

     

    Much to my surprise, Eben says that Class B FCC/CE certification

    will have to wait for the educational release board.

     

    http://www.raspberrypi.org/archives/1929#comment-31756

     

    Back on May 31, Eben said: "there's pcb level work going on

    at the moment to accomplish that".

     

    http://www.youtube.com/watch?v=WIf4Fk2252A

    starting at about 17:35

     

    Liz has said on April 10, 2012 at 7:04 pm, in page 3 of the

    comments to this article: http://www.raspberrypi.org/archives/978

    "Happily, we’ve found it doesn’t need a shielded enclosure to

    reach Class B, although it will require a (very minimal) redesign."

     

    If the redesign really is "very minimal" and was underway as of

    May 31, I'd expect it would have been included in rev 2.0.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    With the new revision, will P2 and P5 be populated?  Or will we have to solder our own pins on?  This seems like a warrenty issue as well - solder and warrenty is void.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    There was mention that P5 would not be populated, at least for now.

     

    I've not found a use for P2 yet, what are you doing with it that would require you to solder one on ?   Unless I misunderstood, thet were allowing all of the arm jtag to appear on P5 ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    P2 has a 3v3 pin and 2 GND pins that could be useful.

    P5 is the main expansion of the GPIO and will include GPIO 7 -10 (4 extra ones onto of the current 8 GPIOs) and will include an extra 5v, 3v3 and 2 GNDs.

     

    That is why I though It was interesting that they were not populated when they can be used as GPIO or extra power.


    Also, the P2 header is currently populated on the current board - why would you need to change this when it is aready on?

     

    Strange.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    P2 has a 3v3 pin and 2 GND pins that could be useful.

    P5 is the main expansion of the GPIO and will include GPIO 7 -10 (4 extra ones onto of the current 8 GPIOs) and will include an extra 5v, 3v3 and 2 GNDs.

     

    That is why I though It was interesting that they were not populated when they can be used as GPIO or extra power.


    Also, the P2 header is currently populated on the current board - why would you need to change this when it is aready on?

     

    Strange.