Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum fake iphone charger can damage your monitor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 708 subscribers
  • Views 563 views
  • Users 0 members are here
  • raspberry_pi
Related

fake iphone charger can damage your monitor

e14 Contributor
e14 Contributor over 13 years ago

http://www.raspberrypi.org/archives/2151

  • Sign in to reply
  • Cancel
  • robotonics
    robotonics over 13 years ago

    Very useful information. I hope the message gets out to as many people as possible! These fake Iphone chargers need rooting out...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 13 years ago

    Saw it earlier and was thinking again about how good was the idea to use cellphone chargers as power source.

     

    Hope that sooner or later, fake or not fake, people realize and understand that it was and it continues to be actually a BAD idea.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago

    In the linked RPF thread, Norman Dunbar links to his write-up about a 7-port hub that appears to be identical in every respect to the product which I bought from Farnell UK, which I described in a dedicated thread right here -- Incompatible Self-Powered Hub .

     

    I strongly suspect that Farnell was caught out by a counterfeit supplier as well (either that or Dynamode themselves are the culprits).  There was no response from Element 14 in my thread, probably because this is not an appropriate channel and I didn't make an official customer complaint nor return the device since I am using it successfully attached to an Intel PC, not to the Pi.

     

    I'm actually rather surprised that no action was taken about this Farnell product, despite the lack of official channels.  Farnell is still selling the device as a Pi accessory (despite being incompatible and non-USB-compliant because of backfeed), and as the RPF blog points out, that is a bad idea.  The unit supplied is on at least two counts out of step with the claims made on the packaging, so it's a trades description issue as well as presenting an element of danger.

     

    Morgaine.

     

    PS. The larger part of my thread concerned incompatibility with Raspberry Pi.  To save wading through 3 pages of posts, the product misrepresentation issues (the USB certification question and the fact that the supplied charger was not 2A as claimed) were described in this post .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    In the linked RPF thread, Norman Dunbar links to his write-up about a 7-port hub that appears to be identical in every respect to the product which I bought from Farnell UK, which I described in a dedicated thread right here -- Incompatible Self-Powered Hub .

     

    I strongly suspect that Farnell was caught out by a counterfeit supplier as well (either that or Dynamode themselves are the culprits).  There was no response from Element 14 in my thread, probably because this is not an appropriate channel and I didn't make an official customer complaint nor return the device since I am using it successfully attached to an Intel PC, not to the Pi.

     

    I'm actually rather surprised that no action was taken about this Farnell product, despite the lack of official channels.  Farnell is still selling the device as a Pi accessory (despite being incompatible and non-USB-compliant because of backfeed), and as the RPF blog points out, that is a bad idea.  The unit supplied is on at least two counts out of step with the claims made on the packaging, so it's a trades description issue as well as presenting an element of danger.

    Actually, the backfeed has changed from a Bug to a Feature.  With RasPi rev 2 and Ohmless rev 1, you can now power your RasPi from a non-compliant hub and discard the Micro USB cable.  You lose the protection of F3.  I'm using my RasPi rev 1 with a Motorola Atrix Lapdock, which deliberately back-feeds on its Micro USB connector.  I replaced polyfuses F1 and F2 with 1.0A single-blow fuses.