Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum WiPi & VGA adapter draw too much power on older R Pi board
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 707 subscribers
  • Views 694 views
  • Users 0 members are here
  • raspberry
  • wifi
  • f2
  • pi
  • f3
  • hdmi
  • f1
  • r
  • raspberry_pi
  • adapter
  • wipi
  • vga
Related

WiPi & VGA adapter draw too much power on older R Pi board

klricks
klricks over 13 years ago

I just got the element14 WIFI adapter and the HDMI to VGA adapter.

Together they draw too much power when used on the older rev 256K board.

The display blanks off every few seconds or so and the WIFI can't connect. Gets worse the longer it's powered on.

I 'pennied' the fuses F1 and F2 by soldering a wire across them but not much help.

I then shorted across the main fuse F3 and all works fine now.

The original board has a 700mA 'poly' fuse at F3. According the posted schematics the newer Rev 2.0 boards have a 1000mA fuse at F3, and F1, F2 have been eliminated.

I will most likely put in a 1 or 2A poly fuse when I get a chance so the board will not melt down if there is a short.

Hopefully the 1A fuse is good enough on the rev 2.0 boards? Anyone tried my combination on a new board?

Note I am using a 5V 10A regulated switching power supply.

  • Sign in to reply
  • Cancel
Parents
  • klricks
    klricks over 13 years ago

    I went and did some measurements.

    The R Pi with WiPi (WIFI) and HDMI to VGA adapter are drawing about 850 mA  That is with WIFI activity going on.

    RPi and VGA adapter alone are drawing 650 mA just under the 700 mA fuse rating.

    The newer R Pi with 1.0A fuse should be OK to run both.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • klricks
    klricks over 13 years ago

    I went and did some measurements.

    The R Pi with WiPi (WIFI) and HDMI to VGA adapter are drawing about 850 mA  That is with WIFI activity going on.

    RPi and VGA adapter alone are drawing 650 mA just under the 700 mA fuse rating.

    The newer R Pi with 1.0A fuse should be OK to run both.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • johnbeetem
    johnbeetem over 13 years ago in reply to klricks

    1A sounds good.  I wouldn't recommend going above 1A, because we don't know how wide power traces are elsewhere on the RasPi board, and whatever is the weakest wire will become the fuse.  You might consider replacing the 1A polyfuse with a 1A single-blow fuse if you find that the voltage drop across the polyfuse is excessive.

     

    I'm glad to hear your HDMI to VGA is working.  If you run into problems, there's good information at the RasPi Wiki here (RGB analog/VGA) and here (Verified Peripherals).  For example, some HDMI to VGA converters draw too much current from RasPi and burn out diode D1.  If the HDMI to VGA unit you're using works OK, it would help the community if you add it to the Verified Peripherals Wiki if it's not already there.