Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Hostname issue.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 708 subscribers
  • Views 3346 views
  • Users 0 members are here
  • wifi
  • cmdrobot
  • help
  • tplink
  • helpme
  • element14
  • raspi
  • wlan
  • network
  • raspberry_pi
  • help!!!!
  • wlan0
  • prototyping
  • raspberrypi
  • hostname
  • rpi
  • wireless
Related

Hostname issue.

wallarug
wallarug over 13 years ago

I have been trying to get this to work for days but have been unsuccessful.

 

I posted here:  http://www.raspberrypi.org/phpBB3/viewtopic.php?f=27&t=10071&p=230854#p230854 but got no responce (which I expected).

 

Most of my details are on there (from last night)

 

I started with a fresh image today and still no luck.

 

What I am trying to do is, using the python command: "socket.gethostbyaddr('10.0.128.2')"

... Check what Raspberry Pi I have connected to and then use this information to decide what to do next.

 

Currently, I have been able to 'hit' every computer on my network with this command except for the raspberry pi.  This is very frustrating.  All the websites that I have read seem to say that it should just work.  I know someone who has a raspberry pi and this seems to work for him.

 

I have set-up a dummy network (which is used above) to attempt to get everything to work.  So far I have had no luck pinging the hostname 'raspberrypi' or 'CMDoverwatch'. 

 

What is really confusing is that the router has the CORRECT hostname but the computers on the network can't use it.

 

I need some help to find out why and then fix it.

 

Below are some of the router setting details:

 

 

DHCP Settings

DHCP Server:Disable Enable
Start IP Address:10.0.128.100
End IP Address:10.0.128.199
Address Lease Time:120 minutes (1~2880 minutes, the default value is 120)
Default Gateway:10.0.128.1 (optional)
Default Domain: (optional)
Primary DNS:10.0.128.1 (optional)
Secondary DNS:8.8.8.8 (optional)

 

Client LIST:

 

IDClient NameMAC AddressAssigned IPLease Time
1raspberrypiB8-27-EB-A0-56-1E10.0.128.10001:58:14
2PC-private10-9A-DD-BC-8F-D210.0.128.10101:45:07

 

 

 

Wireless Settings

SSID:CMDnetwork-base-station
Region:AlbaniaAlgeriaArgentinaArmeniaAustraliaAustriaAzerbaijanBahrainBelarusBelgiumBelizeBolviaBrazilBrunei DarussalamBulgariaCanadaChileChinaColombiaCosta RicaCroatiaCyprusCzech RepublicDenmarkDominican RepublicEcuadorEgyptEl SalvadorEstoniaFinlandFranceGeorgiaGermanyGreeceGuatemalaHondurasHong KongHungaryIcelandIndiaIndonesiaIranIrelandIsraelItalyJapanJapan1Japan2Japan3Japan4Japan5Japan6JordanKazakhstanNorth KoreaKorea RepublicKorea Republic2KuwaitLatviaLebanonLiechtensteinLithuaniaLuxembourgMacauMacedoniaMalaysiaMaltaMexicoMonacoMoroccoNetherlandsNew ZealandNorwayOmanPakistanPanamaPeruPhilippinesPolandPortugalPuerto RicoQatarRomaniaRussiaSaudi ArabiaSingaporeSlovak RepublicSloveniaSouth AfricaSpainSwedenSwitzerlandSyriaTaiwanThailandTrinidad & TobagoTunisiaTurkeyUkraineUnited Arab EmiratesUnited KingdomUnited StatesUruguayUzbekistanVenezuelaViet NamYemenZimbabwe
Warning:Ensure you select a correct country to conform local law.
Incorrect settings may cause interference.

Channel: 12345678910111213
Mode:11Mbps (802.11b)54Mbps (802.11g)

Enable Wireless Router Radio
Enable SSID Broadcast
Enable Bridges

Enable Wireless Security
Security Type:WEP WPA/WPA2WPA-PSK/WPA2-PSK
Security Option: AutomaticWPA-PSKWPA2-PSK
Encryption:AutomaticTKIPAES
PSK Passphrase:doesitreallymatter???
(The Passphrase is between 8 and 63 characters long)
Group Key Update Period:86400(in second, minimum is 30, 0 means no update)

 

LAN

MAC Address:

00-23-CD-C7-12-32

IP Address:
Subnet Mask:      255.255.255.0      255.255.0.0

 

 

That should be all the settings that have been enabled or helpful to people trying to help me.  All the raspberry pi settings are on the link above.

 

Just for those hackers out there, this is not connect to the internet and does not have ANY information on it. image

 

Thanks for anyone who can solve this issue.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Well, I  have no answer but I need to learn about this stuff, so I have a question ....

     

    If your router is set to 192.168.1.1, with a subnet mask of 255.255.255.255.0 , why would you put your peripheral devices on a different subnet (10.0.128.100)?

    Would you expect to be able to ping them?

    This is a *genuine* question from a relative novice.

    --G

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 13 years ago in reply to e14 Contributor

    I think you might be confused.

     

    I wanted to have a portable network set-up using the 10.0.128.100 IP address.

     

    My Personal Home network uses 192.168.*.*  (removed numbers)

     

    I am talking about two network situations where the devices are in separate situations.

     

     

    About your question:

     

    Would you expect to be able to ping them?

    Yes.  Provided you have put the same subnet mask on both devices.  I have seen this done on Corperate networks where they use an IP address for wireless devices and LAN devices. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to wallarug

    Cian

    I think you'll find they add a route to allow the different IP address to work, or they use NAT (Network Address Translation) which is effectively what your broadband router does.

    This may be part of the switch, or within the devices protocols.

     

    Normally you will have a gateway address, where the device heads if its not an address on the local LAN.

    For grahame's example there are 254 address's available, so anything that is 192.168.1. x will be treated as Local, and anything else heads out the gateway and is resolved elsewhere.

     

    If I understand correctly you have a portable network that is attached onto your home network.

    Have you tried changing the Gateway address to the 192.168.*.* (pick something that doesn't clash).

    This would then mean that anything not intended to be local (ie 10.0.128. x) will go out the gateway which should be your local lan.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GreenYamo
    GreenYamo over 13 years ago in reply to wallarug

    Cian,

    You need to bridge the two networks together, both the 192 and 10 networks are reserved for internal networking. These will be the internal addresses on your own network, not the outward facing IP assigned by your ISP.

    Putting the same netmask will not cause them to be linked, as Mark indicates this is only in reference to the number of ip address available on that subnet. See below, I think it will give you some pointers.

    http://serverfault.com/questions/198419/how-to-bridge-networks-192-168-191-0-24-and-10-9-0-0-16

    Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • GreenYamo
    GreenYamo over 13 years ago in reply to wallarug

    Cian,

    You need to bridge the two networks together, both the 192 and 10 networks are reserved for internal networking. These will be the internal addresses on your own network, not the outward facing IP assigned by your ISP.

    Putting the same netmask will not cause them to be linked, as Mark indicates this is only in reference to the number of ip address available on that subnet. See below, I think it will give you some pointers.

    http://serverfault.com/questions/198419/how-to-bridge-networks-192-168-191-0-24-and-10-9-0-0-16

    Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to GreenYamo

    I wasn't confused Cian, so much as curious. Thanks for explaining about your two networks. The comments above seem to be well in line with my own humble thinking, and will hopefully help you reach your goal.

    --G

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    P.S.

     

    Since you know the IPs on your alternative network -- I imagine that you use Address Reservation or no DHCP -- it should be very simple to access them  that way. Interested to know the advantage(s) of calling them by name (lots to learn, here).

    --G

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    I was curious, and cautiously so, to know what would happen if one sends an IP request 'intended' for local receipt out onto the internet, so I did a whois on    10.0.128.100   and got this....

     

    NetRange:       10.0.0.0 - 10.255.255.255

    CIDR:           10.0.0.0/8

    OriginAS:      

    NetName:        PRIVATE-ADDRESS-ABLK-RFC1918-IANA-RESERVED

    NetHandle:      NET-10-0-0-0-1

    Parent:        

    NetType:        IANA Special Use

    RegDate:       

    Updated:        2011-04-12

    Ref:            http://whois.arin.net/rest/net/NET-10-0-0-0-1

     

    OrgName:        Internet Assigned Numbers Authority

    OrgId:          IANA

    Address:        12025 Waterfront Drive

    Address:        Suite 300

    City:           Los Angeles

    StateProv:      CA

    PostalCode:     90292

    Country:        US

    RegDate:       

    Updated:        2012-08-31

     

    I suppose it doesn't matter much, and they might blame the Albanians anyway, according to your info.

    --G

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 13 years ago in reply to GreenYamo

    Steve Read wrote:

     

    Cian,

    You need to bridge the two networks together, both the 192 and 10 networks are reserved for internal networking. These will be the internal addresses on your own network, not the outward facing IP assigned by your ISP.

    Putting the same netmask will not cause them to be linked, as Mark indicates this is only in reference to the number of ip address available on that subnet. See below, I think it will give you some pointers.

    http://serverfault.com/questions/198419/how-to-bridge-networks-192-168-191-0-24-and-10-9-0-0-16

    Steve

    Thanks for the help explaining there....  I think I might have been a bit out of my depth image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to wallarug

    Cian

    Has any of the answers resolved your problem?

    Is there something you're still stuck with.?

     

    If it has somewhere at the bottom you can tag its been answered, and give credit to any helpful answers....

     

    It also lets everyone else know the topic has been resolved.

     

     

    cheers

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 13 years ago in reply to mcb1

    Still has not been resolved yet.  the only OS on the raspberry Pi that my router detects hostname is pwnpi.

     

    I am going to look into pwnpi and the software installed and see if there is something that is fixing it for pwnpi and not raspbian.

     

    This might also be a case of different OSes not liking to talk with each other for different reasons and therefore, impossible to solve.  I think installing samba or some other software could work as well.  I will have a detailed look at all scenarios and report back shortly.

     

    First, I must test the latest RPi software image that came out today!