Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Help - R Pi Errors Boot Failing :-(
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 706 subscribers
  • Views 891 views
  • Users 0 members are here
  • raspberry_pi
Related

Help - R Pi Errors Boot Failing :-(

e14 Contributor
e14 Contributor over 13 years ago

Set up :

Rev B. Kingston SDHC 32GB Class 10 (SD10G2.32GB) ulitmate X 100X loaded with 2012-12-16-wheezy-raspbian.img

 

Note - I checked the SD card was valid on http://www.raspberry-pi.co.uk/2012/06/0 ... -sd-cards/ before buying it.?

 

Card setup via Windows 7, using Win32DiskImager.

 

Not connected to LAN

Keyboard/mouse connected via Logitec USB Wireless - problem occurrs irrespective of this being connected

HDMI connected LG TV

 

I get the following warnings/errors : (not complete)

 

VFS: Cannot open root device "mmcblk0p2" or unknow-block(179,2)

Please append a correct "root=" boot option; here are the available partitions:

b300 30908416 mmcblk0 driver: mmcblk

Kernel panic - not syncingL VFS: Unable to mount root fs on unknown-block(179,2)

... loads of other messages..... eventually

PANIC: VFS: Unable to mount root fs on unknown-block(179,2)

 

Entering kdb due to Keyboard Entry (this is arrived at even without a keyboard plugged in)

kdb> (BUT I CANT actually input anything)

 

This happens on 2 R Pi units.

 

I have also tried a different image - 2012-09-18.img no look.

 

Any help/guidance appreciated..... i have a daughter who can't get to her xmas present :-(

 

regards,

 

Pawiter

  • Sign in to reply
  • Cancel
  • Nate1616
    Nate1616 over 13 years ago

    I've seen this error when a file isnt in the location that is specified.  I've also heard of Win32DiskImage causing corruption in the card.   Here is a good tuturial on setting up the sd card http://elinux.org/RPi_Easy_SD_Card_Setup

    hope this helps!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago

    While I've never used it myself, I have heard of people having problems with Win32DiskImager.  One cause is using a built-in SD Card reader instead of an external USB-based SD Card reader, or you may have a bad version of Win32DiskImager.  Here's a typical thread from raspberrypi.org: Windows 7, win32diskimager not working!  I suggest entering "Win32DiskImager" in the search box at the top of this page and on the front page at raspberrypi.org.

     

    It's also possible that your particular SD Card is bad.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • element14jamie
    element14jamie over 13 years ago

    Hello Pawiter,

    I am moving this to the Raspberry Pi Area of the Community.

     

     

    Thank you and we hope you are enjoying the Community!

     

     

    Jamie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dhaggar
    dhaggar over 13 years ago

    Ditch the CL10 cards and get a few CL4. I've not had one CL10 card that works although I haven't tried very many.

    I've also had trouble with every Verbatim 4GB CL4 card that I tried. I have used quite a few SanDisk 8GB CL4 cards without any issues.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tabarus12
    tabarus12 over 13 years ago in reply to dhaggar

    That is true, Ive seen many folks complaint abbout CL10 cards not working, apparently its very dificult to setup a CL10 and many people prefer the CL4, even pages like sparkfun and adafruit sells CL4 to use with the RPi.

     

    Best bet use CL4 cards and ditch the CL10 till fruther notice.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sbi3clp
    sbi3clp over 13 years ago

    Have you tried downloading NOOBS instead? Previously I have had problems writing wheezy to some SD cards, but the problem goes when I have used NOOBS instead.