Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Help - R Pi Errors Boot Failing :-(
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 709 subscribers
  • Views 865 views
  • Users 0 members are here
  • raspberry_pi
Related

Help - R Pi Errors Boot Failing :-(

e14 Contributor
e14 Contributor over 13 years ago

Set up :

Rev B. Kingston SDHC 32GB Class 10 (SD10G2.32GB) ulitmate X 100X loaded with 2012-12-16-wheezy-raspbian.img

 

Note - I checked the SD card was valid on http://www.raspberry-pi.co.uk/2012/06/0 ... -sd-cards/ before buying it.?

 

Card setup via Windows 7, using Win32DiskImager.

 

Not connected to LAN

Keyboard/mouse connected via Logitec USB Wireless - problem occurrs irrespective of this being connected

HDMI connected LG TV

 

I get the following warnings/errors : (not complete)

 

VFS: Cannot open root device "mmcblk0p2" or unknow-block(179,2)

Please append a correct "root=" boot option; here are the available partitions:

b300 30908416 mmcblk0 driver: mmcblk

Kernel panic - not syncingL VFS: Unable to mount root fs on unknown-block(179,2)

... loads of other messages..... eventually

PANIC: VFS: Unable to mount root fs on unknown-block(179,2)

 

Entering kdb due to Keyboard Entry (this is arrived at even without a keyboard plugged in)

kdb> (BUT I CANT actually input anything)

 

This happens on 2 R Pi units.

 

I have also tried a different image - 2012-09-18.img no look.

 

Any help/guidance appreciated..... i have a daughter who can't get to her xmas present :-(

 

regards,

 

Pawiter

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 13 years ago

    While I've never used it myself, I have heard of people having problems with Win32DiskImager.  One cause is using a built-in SD Card reader instead of an external USB-based SD Card reader, or you may have a bad version of Win32DiskImager.  Here's a typical thread from raspberrypi.org: Windows 7, win32diskimager not working!  I suggest entering "Win32DiskImager" in the search box at the top of this page and on the front page at raspberrypi.org.

     

    It's also possible that your particular SD Card is bad.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 13 years ago

    While I've never used it myself, I have heard of people having problems with Win32DiskImager.  One cause is using a built-in SD Card reader instead of an external USB-based SD Card reader, or you may have a bad version of Win32DiskImager.  Here's a typical thread from raspberrypi.org: Windows 7, win32diskimager not working!  I suggest entering "Win32DiskImager" in the search box at the top of this page and on the front page at raspberrypi.org.

     

    It's also possible that your particular SD Card is bad.