Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Nano Error Writting
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 676 subscribers
  • Views 1184 views
  • Users 0 members are here
  • nano
  • helpme
  • element14
  • pi
  • vnc
  • raspberry_pi
  • raspberrypi
  • rpi
Related

Nano Error Writting

Former Member
Former Member over 12 years ago

I am trying to set up VNC Server on my PI as per instruction on pengiuntutor.com/linux/tightvnc.

when attempting to add to the start up using the Provided script and pasting in Nano when I came to save it i get a "error writing to /ect/init.d/tightvncserver: no such file or directory"

I have tried using root and 'pre-creating' the file in the GUI with no luck.

What am I doing wrong?

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 12 years ago

    You might try "/etc/init.d" instead of "/ect/init.d".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 12 years ago

    You might try "/etc/init.d" instead of "/ect/init.d".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • wallarug
    wallarug over 12 years ago in reply to johnbeetem

    You could try it a different way:

     

    1. boot up RPi

    2. On RPi open up a file called '/etc/rc.local':

     

    sudo nano /etc/rc.local

     

    3. add the line to the bottom of the file BUT ABOVE  ' exit0 '

     

     

    su -c "vncserver -geometry 1024x800 -depth 24" root

     

    This will start a tightVNC session with the dimentions of 1024 x 800.  You can change this what-ever you want providing it is a supported resolution/the shape you want.  Also note that this session is for the user 'root' . Change this to the user you want to use.

     

    This will start the tightVNC server everytime you boot up your RPi.  Personally, I wouldn't mess around wit .init scripts when there is a simpler way to do it (I have not used .init scripts for this but I have used one for a LCD display I am using...I had many problems and hence my dislike of that method.)

     

    Hope this helps you.

     

    /etc/rc.local:

     

    #!/bin/sh -e

    #

    # rc.local

    #

    # This script is executed at the end of each multiuser runlevel.

    # Make sure that the script will "exit 0" on success or any other

    # value on error.

    #

    # In order to enable or disable this script just change the execution

    # bits.

    #

    # By default this script does nothing.

     

     

    # Print the IP address

    _IP=$(hostname -I) || true

    if [ "$_IP" ]; then

      printf "My IP address is %s\n" "$_IP"

      printf "VNCserver has started on $_IP"       # I added this one to look cool image

    fi

    su -c "vncserver -geometry 1280x800 -depth 24" root

     

    exit 0

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago in reply to johnbeetem

    Ok First I thought that was just a typo in my post I would have check that. Then I has a look tried it and it worked image&image.

    Thanks for the correction your a star

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago in reply to wallarug

    Fergus Byrne wrote:

     

    You could try it a different way:

     

    1. boot up RPi

    2. On RPi open up a file called '/etc/rc.local':

     

    sudo nano /etc/rc.local

     

    3. add the line to the bottom of the file BUT ABOVE  ' exit0 '

     

     

    su -c "vncserver -geometry 1024x800 -depth 24" root

     

    This will start a tightVNC session with the dimentions of 1024 x 800.  You can change this what-ever you want providing it is a supported resolution/the shape you want.  Also note that this session is for the user 'root' . Change this to the user you want to use.

     

    This will start the tightVNC server everytime you boot up your RPi.  Personally, I wouldn't mess around wit .init scripts when there is a simpler way to do it (I have not used .init scripts for this but I have used one for a LCD display I am using...I had many problems and hence my dislike of that method.)

     

    Hope this helps you.

     

    /etc/rc.local:

     

    #!/bin/sh -e

    #

    # rc.local

    #

    # This script is executed at the end of each multiuser runlevel.

    # Make sure that the script will "exit 0" on success or any other

    # value on error.

    #

    # In order to enable or disable this script just change the execution

    # bits.

    #

    # By default this script does nothing.

     

     

    # Print the IP address

    _IP=$(hostname -I) || true

    if [ "$_IP" ]; then

      printf "My IP address is %s\n" "$_IP"

      printf "VNCserver has started on $_IP"       # I added this one to look cool image

    fi

    su -c "vncserver -geometry 1280x800 -depth 24" root

     

    exit 0

    Cheers Fergus

    Got the other way working but will give you suggestion a try when I get a chance looks like it might be neater and give me something else to play with.

    I guess I should ask How one would remove the Scripts from the start up, that one has now added?image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 12 years ago in reply to Former Member

    Delete it. image

     

    from prompt:

    rm /<directory>/<file>