Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi running slowly!! Very slowly!!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 704 subscribers
  • Views 1600 views
  • Users 0 members are here
  • raspberry
  • slow
  • pi
  • running
Related

Raspberry Pi running slowly!! Very slowly!!

e14 Contributor
e14 Contributor over 13 years ago

Hi got my Raspberry Pi but it's running very slow. Put it this way when I move the terminal window in X mode using the mouse the CPU usage jumps up to 70% - 80% thats not normal surely?

 

Im not new to Linux so I checked the logs DMESG etc. but there seem to be no problems. I am awaiting a multimeter to check powersupply using T1 T2 on the board. I have also looked into the possible cause being the SD card. Mine is a Kingston branded (but made in China) 4GB micro SD with a SDHC logo on it rated at class 4. When the multimeter arrives I will also check the polyfuse. I thought it may be a formatting or partitioning problem so I used berryboot which seems to be idiot proof, and still no joy. Can someone give me any ideas?? oh yeah tried to do a benchmark using sysbench ran a random I/O mode with 50MB of data and after an hour i had ot abort the process! This can't be normal. Is anyone else having similar problems / or has solved any problems??

 

Cheers Hungdonk3y

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    > Hi got my Raspberry Pi but it's running very slow. Put it this way when I move the terminal window in X mode using the mouse the CPU usage jumps up to 70% - 80% thats not normal surely?

     

    Yes, I think it is.  The RPi has a relatively fast GPU, but a relatively slow CPU,

    and X mode uses the CPU.  There is a volunteer, Simon, working on trying to

    accelerate X using the GPU, but he is not optimistic about the prospects.

    see my post #4 on this recent thread:

    http://www.element14.com/community/message/67203#67203/l/re-2013-the-year-of-arm-linux-on-the-desktop

     

    When the X slowness is mentioned, JamesH makes it sound like Simon's

    work is a promising solution, such as when he recently wrote:

     

    "See teh_orphs thread about GPU accleration for X - currently in testing."

    in this thread:

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=29046