Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum PiFace Problems
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 78 replies
  • Subscribers 717 subscribers
  • Views 12330 views
  • Users 0 members are here
  • raspberry_pi
  • piface
  • raspberry_pi_accessories
Related

PiFace Problems

keithtowns
keithtowns over 13 years ago

Am I missing something? I have two PiFace and 3 Raspberry Pi. I followed the instructions the get the PiFace working but have yet to succeed. I have tried the image provided as well as updating an existing Raspian image to no avail. I have also tried all my Pi and the two PiFace in all the combinations. I almost gave up but also tried a different power supply and SD card. None of the above got the emulator to switch on the LEDs and I could not do it through Python. Any ideas? I've spent hours on this, please tell me I've missed something. Thanks.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Keith, you are not alone. The 'documentation' with the piface is worse than useless. I particularly like the typo on page 2 of the 'instructions' (etc/ which should be /etc/) and that if the emulator fails (I can't get it to work – ends with 'segmentation fault') the 'instructions' that follow are, again, useless. I will get it working in the end, but no thanks to the fools at man.ac.uk. How difficult would it have been to provide basic instructions in the box? Good luck with it - I'll reply back when I've finished arm-wrestling with it and got it doing something (I have a job in mind).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    ... not sure if urls are allowed here - if they are, here's some documentation for piface ...

     

    https://docs.google.com/folder/d/0B-UAZ9CyJCLGQjJ3RDlqa2pqaDg/edit?pli=1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to e14 Contributor

    Thomas

    If you want a better image showing the default jumpers you can use my picture.

    http://www.element14.com/community/roadTestReviews/1452

    If you want the fullsized image, PM me with your email.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Hello Thomas,
    I have the PiFace 2.1 with the latest version of pifacecommon and pifacedigitalio on the last raspbian running. Control of IO is not a problem. But the interrupts do not work with python. The sample code, for example, shows no function. But the interrupts works fine withe the Java lib Pi4J. Do you have any idea what could go wrong?

    best greetings Andreas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Hi, sorry for the delayed reply, I've been on holiday!

     

    Are you using the example code from here: http://piface.github.io/pifacedigitalio/example.html#interrupts? Did you reboot after installing? Can you show me the code you are trying to use?

     

    Pi4J is a Java library for accessing the GPIO pins, not PiFace (to my knowledge at least).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Hey Thomas,
    thanks for your answer. I have reinstalled the distribution. I try the / usr/share/doch/python3-pifacedigitalio/examples/presslights.py program and also the example code on the webpage (ure link). Nothing works. But simple polling on a button works fine. So buttons and leds are working...

    To Pi4J, "With the Pi-Face Java API interface now available in the libraries Pi4J (Pi4J in version 0.0.5-SNAPSHOT and later)" Source: http://www.savagehomeautomation.com/projects/raspberry-pi-programming -pi-face-with-java-pi4j.html
    The API package comes with two examples for the piface PiFaceExample.java and PiFaceGpioExample.java. I compile and run the PiFaceExample
    (it use listener (interrupts)) and it ran as it should, so I think that the interrupts generally works?!

     

    I hope you have another ideas image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    That's great news about Java support for PiFace!

     

    Are you running the latest versions of the Python modules? Can you show me the output of the following commands:

     

    $ python3 -c "import pifacedigitalio.version as p; print(p.__version__)"

    $ python3 -c "import pifacecommon.version as p; print(p.__version__)"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Python3: 3.2.3 (Mar 1) GCC 4.6.3

    PiFacedigitalio: 2.0.3

    PiFaceCommon: 3.0.0

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    How about the outputs from the following commands:

     

    groups

    lsmod

    cat /etc/modprobe.d/raspi-blacklist.conf

    cat /lib/udev/rules.d/60-python3-pifacecommon.rules

     

    I can't seem to replicate the issue I'm afraid.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    PiFace Common is now on v3.1.1, which has a fix for an installation bug that was there since v3.1, maybe even v3.0. Can you try installing the lastest version and see if that fixes your issue?

     

    https://github.com/piface/pifacecommon/releases

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    3.1.1 still nothing happend image

     

    groups:

    pi adm dialout cdrom sudo audio video plugdev games users netdev input spi gpio

     

    lsmod:

    Module                  Size  Used by

    snd_bcm2835            16432  0

    snd_pcm                77728  1 snd_bcm2835

    snd_seq                53482  0

    snd_timer              20110  2 snd_pcm,snd_seq

    snd_seq_device          6462  1 snd_seq

    snd                    58744  5 snd_bcm2835,snd_timer,snd_pcm,snd_seq,snd_seq_device

    snd_page_alloc          5169  1 snd_pcm

    joydev                  9356  0

    spidev                  5248  4

    evdev                   9450  6

    leds_gpio               2243  0

    led_class               3570  1 leds_gpio

    spi_bcm2708             4841  0

    hid_cherry              1575  0

     

    cat /etc/modprobe.d/raspi-blacklist.conf

    #blacklist spi-bcm2708

    blacklist i2c-bcm2708

     

    cat /lib/udev/rules.d/60-python3-pifacecommon.rules

    KERNEL=="spidev*", GROUP="spi", MODE="0660"

    SUBSYSTEM=="gpio*", PROGRAM="/bin/sh -c 'chown -R root:gpio /sys/class/gpio && chmod -R 770 /sys/class/gpio; chown -R root:gpio /sys/devices/virtual/gpio && chmod -R 770 /sys/devices/virtual/gpio'"p

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Everything appears to be set up correctly. Does the following Python code print anything when you press switch 0 after the last line?

     

    import pifacedigitalio

    pifacedigitalio.init()

    pifacedigital = pifacedigitalio.PiFaceDigital()

    listener = pifacedigitalio.InputEventListener()

    listener.register(0, pifacedigitalio.IODIR_ON, print)

    listener.activate()

     

     

    As a last resort, have you tried reinstalling Raspbian and then installing pifacedigitalio on a fresh install?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Everything appears to be set up correctly. Does the following Python code print anything when you press switch 0 after the last line?

     

    import pifacedigitalio

    pifacedigitalio.init()

    pifacedigital = pifacedigitalio.PiFaceDigital()

    listener = pifacedigitalio.InputEventListener()

    listener.register(0, pifacedigitalio.IODIR_ON, print)

    listener.activate()

     

     

    As a last resort, have you tried reinstalling Raspbian and then installing pifacedigitalio on a fresh install?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Okay. I run ure sample code, no output. Reinstalling Rasbian was my first try of troubleshooting.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Did you press switch 0? Perhaps your switch is broken? Try connecting the ground pin and pin 0 with a wire (a paperclip will do). What happens then?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Hey, i think you mean sw1 / input0, but i also try all the other switches and as i said in a earlier post "But simple polling on a button works fine. So buttons and leds are working...".  So the hardware should be fine?!. Strange that I seem to be the only one with this behavior image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Hello Thomas,

    I have my SD card inserted and tested in a different RPi with another PiFace. The error is thus definitely somewhere in the software configuration!

    I'm going to make the Raspian completely new and write down step by step what I did. Perhaps you notice what's wrong or missing.

     

    Thanks for your help so far!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Sounds like a good idea. Hopefully we can get to the bottom of this!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Okay that's exactly what I did, no more and no less!

     

     

    • Downloading 2013-09-10-wheezy-raspbian from raspberrypi.org
    • Writing Image on SD Card with win32 disk imager (v0.9)
    • First boot
    • Enable boot to desktop
    • Reboot
    • Connect via WinSCP
    • Copy common 3.1.1 and digitalio 2.1.0
    • Install common (sudo dpkg –i python3-pifacecommon…)
    • Reboot
    • Install digitalio (sudo dpkg –i python3-pifacedigital…)
    • Reboot
    • Lunch IDLE3
    • Select  / usr/share/doc/python3-pifacedigitalio/examples/presslights.py
    • Run F5
    • Press the Buttons

     

    Nothing happens. Still the same sh** :-( I'm desperate ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    It might be somethig to do with IDLE (I've never used it). Try running the program from the command line (xterm or lxterminal).

     

    $ python3 /usr/share/doc/python3-pifacedigitalio/examples/presslights.py

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    image yeah! That's it. Hours that I have employed you and then such an error.. big thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • videogame95
    videogame95 over 12 years ago in reply to e14 Contributor

    Hi i have a piface all the pins light up on override 1-7

    The piface will not recognized import piface.pfio as pfio

    most programmes i have run come up with syntex error

    i conected a door closer to the pin ligths up it works but relay does not swiitch

    i will do fresh install piface already loaded but it has no wifi installed

     

    any help with this it sounds a bit the same as yours

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to videogame95

    Are you using the most up-to-date libraries? You can install them with:

     

    $ sudo apt-get update && sudo apt-get install python{,3}-pifacedigitalio

     

    Examples on how to use pifacedigitalio can be found here: http://piface.github.io/pifacedigitalio/example.html