Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum PiFace Problems
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 78 replies
  • Subscribers 717 subscribers
  • Views 12304 views
  • Users 0 members are here
  • raspberry_pi
  • piface
  • raspberry_pi_accessories
Related

PiFace Problems

keithtowns
keithtowns over 13 years ago

Am I missing something? I have two PiFace and 3 Raspberry Pi. I followed the instructions the get the PiFace working but have yet to succeed. I have tried the image provided as well as updating an existing Raspian image to no avail. I have also tried all my Pi and the two PiFace in all the combinations. I almost gave up but also tried a different power supply and SD card. None of the above got the emulator to switch on the LEDs and I could not do it through Python. Any ideas? I've spent hours on this, please tell me I've missed something. Thanks.

  • Sign in to reply
  • Cancel
  • mrbuzzcut
    mrbuzzcut over 13 years ago in reply to keithtowns

    Did you get any error messages in the terminal window when you ran the emulator?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • keithtowns
    keithtowns over 13 years ago in reply to mrbuzzcut

    Hi Jeff

     

    No errors, the emulator window opens and says piface detected but nothing works. In the terminal window the cursor waits and returns to root@raspberrypi:~# once the emulator has been closed.

     

    Cheers

     

    Keith

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mrbuzzcut
    mrbuzzcut over 13 years ago in reply to keithtowns

    PiFace detected...that's a start. Did you click the override button?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to keithtowns

    Keith, can you run the commands I listed in post #8 and tell me the output? If you can see the SPI device files (/dev/spidev0.0 and /dev/spidev0.1) and running the Python shell commands doesn't error then it's probably an error with your board.

     

    Also, try reading from the board:

     

    $ python

    >>> import piface.pfio as p

    >>> p.digital_read(0)

     

    This should return a 1 or 0 value depending on whether the switch was pressed. So you should run the digital_read() command twice, once while holding the first switch and once while not. The returned values should be different. If they are the same even when you have held down the switch then it's a hardware fault.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • keithtowns
    keithtowns over 13 years ago in reply to e14 Contributor

    Hello Thomas

     

    The commands returned the following:

     

    root@raspberrypi:~# ls -l /dev/spidev*

    crw-rw---T 1 root spiuser 153, 0 Jan  1  1970 /dev/spidev0.0

    crw-rw---T 1 root spiuser 153, 1 Jan  1  1970 /dev/spidev0.1

     

    However, the input was more revealing:

     

    root@raspberrypi:~# python

    Python 2.7.3 (default, Jan 13 2013, 11:20:46)

    [GCC 4.6.3] on linux2

    Type "help", "copyright", "credits" or "license" for more information.

    >>> import piface.pfio as p

    >>> p.digital_read(0)

    Traceback (most recent call last):

      File "<stdin>", line 1, in <module>

      File "/usr/local/lib/python2.7/dist-packages/piface/pfio.py", line 249, in digital_read

        current_pin_values = read_input()

      File "/usr/local/lib/python2.7/dist-packages/piface/pfio.py", line 300, in read_input

        port, data = read(INPUT_PORT)

      File "/usr/local/lib/python2.7/dist-packages/piface/pfio.py", line 329, in read

        operation, port, data = send([(READ_CMD, port, 0xff)])[0] # send is expecting and returns a list

      File "/usr/local/lib/python2.7/dist-packages/piface/pfio.py", line 342, in send

        raise InitError("The pfio module has not yet been initialised. Before send(), call init().")

    piface.pfio.InitError: The pfio module has not yet been initialised. Before send(), call init().

    >>>

     

     

    Thanks

     

    Keith

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to keithtowns

    Ah, my bad. You need to initialised the pfio first.

     

    $ python

    >>> import piface.pfio as p

    >>> p.init()

    >>> p.digital_read(0)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • keithtowns
    keithtowns over 13 years ago in reply to mrbuzzcut

    Hi Jeff

     

    Yes I did click on the override enable and then all on/off and individual pins but nothing......

     

    Thanks anyway

     

    Keith

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • keithtowns
    keithtowns over 13 years ago in reply to e14 Contributor

    Hi Thomas

     

    I tried the code below:

     

    root@raspberrypi:/home/pi# python

    Python 2.7.3 (default, Jan 13 2013, 11:20:46)

    [GCC 4.6.3] on linux2

    Type "help", "copyright", "credits" or "license" for more information.

    >>> import piface.pfio as p

    >>> p.init()

    >>> p.digital_read(0)

    1

    >>> p.digital_read(1)

    1

    >>> p.digital_read(0)

    1

    >>> p.digital_read(1)

    1

    >>>

     

    For the first two tries, no button was pressed. For the second two, I pressed all the buttons.

     

    Cheers

     

    Keith

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • keithtowns
    keithtowns over 13 years ago in reply to e14 Contributor

    Hi Thomas

     

    Just tried the same again with my other Piface board, exactly the same results.

     

    Cheers

     

    Keith

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to keithtowns

    Where are your jumpers on the board in the correct place? They should both be on 0. Here is a picture I just took of my PiFace for reference.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<>