Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum PiFace Problems
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 78 replies
  • Subscribers 717 subscribers
  • Views 12357 views
  • Users 0 members are here
  • raspberry_pi
  • piface
  • raspberry_pi_accessories
Related

PiFace Problems

keithtowns
keithtowns over 13 years ago

Am I missing something? I have two PiFace and 3 Raspberry Pi. I followed the instructions the get the PiFace working but have yet to succeed. I have tried the image provided as well as updating an existing Raspian image to no avail. I have also tried all my Pi and the two PiFace in all the combinations. I almost gave up but also tried a different power supply and SD card. None of the above got the emulator to switch on the LEDs and I could not do it through Python. Any ideas? I've spent hours on this, please tell me I've missed something. Thanks.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    PiFace Common is now on v3.1.1, which has a fix for an installation bug that was there since v3.1, maybe even v3.0. Can you try installing the lastest version and see if that fixes your issue?

     

    https://github.com/piface/pifacecommon/releases

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    3.1.1 still nothing happend image

     

    groups:

    pi adm dialout cdrom sudo audio video plugdev games users netdev input spi gpio

     

    lsmod:

    Module                  Size  Used by

    snd_bcm2835            16432  0

    snd_pcm                77728  1 snd_bcm2835

    snd_seq                53482  0

    snd_timer              20110  2 snd_pcm,snd_seq

    snd_seq_device          6462  1 snd_seq

    snd                    58744  5 snd_bcm2835,snd_timer,snd_pcm,snd_seq,snd_seq_device

    snd_page_alloc          5169  1 snd_pcm

    joydev                  9356  0

    spidev                  5248  4

    evdev                   9450  6

    leds_gpio               2243  0

    led_class               3570  1 leds_gpio

    spi_bcm2708             4841  0

    hid_cherry              1575  0

     

    cat /etc/modprobe.d/raspi-blacklist.conf

    #blacklist spi-bcm2708

    blacklist i2c-bcm2708

     

    cat /lib/udev/rules.d/60-python3-pifacecommon.rules

    KERNEL=="spidev*", GROUP="spi", MODE="0660"

    SUBSYSTEM=="gpio*", PROGRAM="/bin/sh -c 'chown -R root:gpio /sys/class/gpio && chmod -R 770 /sys/class/gpio; chown -R root:gpio /sys/devices/virtual/gpio && chmod -R 770 /sys/devices/virtual/gpio'"p

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Everything appears to be set up correctly. Does the following Python code print anything when you press switch 0 after the last line?

     

    import pifacedigitalio

    pifacedigitalio.init()

    pifacedigital = pifacedigitalio.PiFaceDigital()

    listener = pifacedigitalio.InputEventListener()

    listener.register(0, pifacedigitalio.IODIR_ON, print)

    listener.activate()

     

     

    As a last resort, have you tried reinstalling Raspbian and then installing pifacedigitalio on a fresh install?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Okay. I run ure sample code, no output. Reinstalling Rasbian was my first try of troubleshooting.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Did you press switch 0? Perhaps your switch is broken? Try connecting the ground pin and pin 0 with a wire (a paperclip will do). What happens then?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Hey, i think you mean sw1 / input0, but i also try all the other switches and as i said in a earlier post "But simple polling on a button works fine. So buttons and leds are working...".  So the hardware should be fine?!. Strange that I seem to be the only one with this behavior image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Hello Thomas,

    I have my SD card inserted and tested in a different RPi with another PiFace. The error is thus definitely somewhere in the software configuration!

    I'm going to make the Raspian completely new and write down step by step what I did. Perhaps you notice what's wrong or missing.

     

    Thanks for your help so far!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Sounds like a good idea. Hopefully we can get to the bottom of this!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Okay that's exactly what I did, no more and no less!

     

     

    • Downloading 2013-09-10-wheezy-raspbian from raspberrypi.org
    • Writing Image on SD Card with win32 disk imager (v0.9)
    • First boot
    • Enable boot to desktop
    • Reboot
    • Connect via WinSCP
    • Copy common 3.1.1 and digitalio 2.1.0
    • Install common (sudo dpkg –i python3-pifacecommon…)
    • Reboot
    • Install digitalio (sudo dpkg –i python3-pifacedigital…)
    • Reboot
    • Lunch IDLE3
    • Select  / usr/share/doc/python3-pifacedigitalio/examples/presslights.py
    • Run F5
    • Press the Buttons

     

    Nothing happens. Still the same sh** :-( I'm desperate ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    It might be somethig to do with IDLE (I've never used it). Try running the program from the command line (xterm or lxterminal).

     

    $ python3 /usr/share/doc/python3-pifacedigitalio/examples/presslights.py

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>