Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum New kid on the block the pcDuino ...
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 56 replies
  • Subscribers 707 subscribers
  • Views 10363 views
  • Users 0 members are here
  • raspberry_pi
Related

New kid on the block the pcDuino ...

jamodio
jamodio over 13 years ago

Yet another ARM Cortex board ... The pcDuino com ... getting one to see how compares with the Rpi ...

 

Atr least I didn't have to wake up in wee hours like a year ago to get one.

 

Cheers

Jorge

  • Sign in to reply
  • Cancel
Parents
  • jamodio
    jamodio over 13 years ago

    I've the Wandboard Quad on the bench, worked out of the box !

     

    Added the WiFi antenna, few minutes configuration via the ubuntu system settings, and joined my WiFi network without a glitch.

     

    Very, very impressed with the quality of video, even playing videos through vnc. Nicely done. Blog article coming soon ...

     

    image

     

    Cheers

    Jorge

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 13 years ago in reply to jamodio

    Thanks for very sharing - very cool!  You seem to have all the cool single board computer toys image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Do you get any sense of the embedded industry moving (or even wanting to move) towards modular standardisation of the EDM, SOM or even EOMA-68 kind?  Unfortunately, I don't.

    EDM seems to have some mindshare, but the wandboard seems to be the cheapest and most powerful example.  I know some folks here like EOMA, but I'm skeptical. EDM clearly isn't gaining acceptance, so what killer feature would EOMA have that EDM doesn't in already existing products ?

     

    Perhaps we should be aiming for R-Pi form factor instead image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 13 years ago in reply to morgaine

    Nope, I don't see any clear signs of any coordinated effort to generate an industry standard for modular SBCs, also I don't know how feasible that could be with such a diverse universe of SoC or application processors.

     

    What I see as modular is something that can be taken as a "module" and integrated into another board for a specific application, good solutions are those where most of the interesting signals/interface/power are brought to some sort of expansion connector.

     

    The Raspberry Pi for example is not good at all, I'd say that the Beagle Bone [Black] is one of the best given that strikes a good balance on type and quantity of signals in a pair of standard and cheap header connectors.

     

    The Wandboard is on the other side of the spectrum, almost all signals are on the connector to the motherboard but it is not as cheap or standard to be integrated.

     

    Olimex is very good on this front for simple applications.

     

    The Cubie board is an interesting option but documentation is very scarce.

     

    I still have the pcDuino on my list of things to test, but this is another Allwinner board so documentation is not good either, and not that many IO and as easy to integrate like the BBB.

     

    You also have to give some points for quality of design and production, and very very important what development tools and support community you have around.

     

    Adding everything up if I have today to pick a winner it will be the Beagle Bone Black.

     

    My. 02

    Jorge

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to jamodio

    You're both confirming the impression I'd gained of the state of play in modular boards.  That's a pity.

     

    Although we have no power to influence the direction of industry in any significant way, perhaps there is room for enthusiast-level design (or promotion) of OSHW modular systems independent of industry, if only one major barrier could be overcome.

     

    BGA is the big elephant in the room, a nearly impossible hurdle placed between SoC manufacturers and enthusiasts (yes I know that a few enthusiasts can handle BGA, but that doesn't change the statistics much).  There is however a way of cutting the elephant down to size, and that is to choose a cheap intermediate adapter form that is easier to handle, and then getting the BGA-on-adapters mass produced for not a lot more than the SoCs themselves.  Based on these pre-mounted BGAs, enthusiasts could then take module design in directions where the embedded industry has not found a reason to go.  Coupled with 3D printing, modular enthusiast OSHW computers would then be not too far-fetched an idea.

     

    The current direction in which every board is different and requires its own case design and mandates almost wholesale reinvestment when you change manufacturers is really bad.  The OSHW community could chose to do better than this, even if industry doesn't want to help.

     

     

    Addendum: I've just realized that this is the Pi group, singularly the wrong place to be having a discussion about OSHW modules. The chances of getting a BCM2835 on a bare BGA-adapter boardlet are not very good. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to jamodio

    jamodio wrote:

    The Wandboard is on the other side of the spectrum, almost all signals are on the connector to the motherboard but it is not as cheap or standard to be integrated.

    As I understand it, the wandboard follows the EDM 'standard'.  I'd been kind of hoping it might help drive some more adoption.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    The current direction in which every board is different and requires its own case design

    Consumers want shiny cases, not me image

     

    You're right about BGA, it makes the barrier quite high, both from the assembly side and as jamodio points out from the pcb design angle. Once you designing 6 or 8 layer boards in order to get your signals out from under the BGA you're probably as well thinking about volumes and getting them assembled by someone with the proper equipment.

    For a while there Olimex seemed to be trying to support people wanting to hand assemble stuff by using TQFP's where possible, but I see most of their Allwinner based stuff is BGA now.

    So while a standard module with all the bga stuff contained would be a wonderful idea, in practise the commercial entities building these things are in it for their own (or their shareholders) gain, so 'value add' and 'lock in' is far more important than keeping us OSHW proponents happy.

     

    Ultimately, it's not just BGA though. Any sufficiently high density connector will cause problems for enthusiasts, the higher the density the harder it is to handle and the number of people capable of doing it reduces as the cost and complexity of the equipment needed rises.  So a balance is needed, otherwise people just end up buying a commercial carrier for the module anyway, at which point you're back to the argument of 'why bother'

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    As I understand it, the wandboard follows the EDM 'standard'.  I'd been kind of hoping it might help drive some more adoption.

     

    An OSHW kickstarter campaign to put one (or all) of TI, Allwinner, Samsung and ST applications processors on the same EDM form factor as was used by Wandboard for Freescale's i.MX6 aren't beyond the bounds of possibility.  Kickstarters have been successful with far stupider goals.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    Ultimately, it's not just BGA though. Any sufficiently high density connector will cause problems for enthusiasts, the higher the density the harder it is to handle and the number of people capable of doing it reduces as the cost and complexity of the equipment needed rises.

    To some extent, high density is a commercial affectation, driven by the need to look modern and high tech and also because real estate costs money.  Most enthusiasts don't need high density though, and as you say, it's just a liability to them.  As long as signal paths are properly balanced and well within all the electrical specs, spread them out to low-density edges of adapters.  Modules and connectors being a bit bigger is an advantage for OSHW.

     

    And that in turn would obviate the need for the commercial carrier that you mentioned, because the carrier can then also be low-density OSHW.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    jamodio wrote:

    The Wandboard is on the other side of the spectrum, almost all signals are on the connector to the motherboard but it is not as cheap or standard to be integrated.

    As I understand it, the wandboard follows the EDM 'standard'.  I'd been kind of hoping it might help drive some more adoption.

     

    There is no such thing as an "EDM standard".

     

    The wandboard and the "EDM standard" are creations of the same company.

     

    It may look confusing and misleading but behind all of them is TechNexion LTD of Taiwan. The only company to use EDM is them so there is no "standard" as you can see from this detailed list of products that support it http://www.edm-standard.org/index.php/product-list or the exensive list of companies that adhere to the standard http://www.edm-standard.org/index.php/members

     

    Those guys may succeed tyring to fool some newbie but not an old dog image

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 13 years ago in reply to e14 Contributor

    One more bit of information to share, the Wandboard afaik has not a single certification, I didn't do a detailed analysis but I'd venture to bet that if they try, it won't pass FCC Class B, not even close.

     

    On the other hand, the BBB is both CE and FCC certified (class B). You can even download the certificate of compliance https://github.com/CircuitCo/-BeagleBone-Black/blob/master/10238105EUS1.pdf?raw=true

     

    -J

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 13 years ago in reply to morgaine

    I think we can have an interesting discussion somewhere else in the forum about BGA vs ???, there are pros and cons, and as I always say it depends on the application and the target "customer."

     

    If you are in this just for a hobby, a DYI project or some basic integration, don't mess with what you don't know how to do or have the tools to do it, you will waste more time and money, just buy a ready made BBB and have fun with it.

     

    My .02

    -J

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jamodio
    jamodio over 13 years ago in reply to morgaine

    I think we can have an interesting discussion somewhere else in the forum about BGA vs ???, there are pros and cons, and as I always say it depends on the application and the target "customer."

     

    If you are in this just for a hobby, a DYI project or some basic integration, don't mess with what you don't know how to do or have the tools to do it, you will waste more time and money, just buy a ready made BBB and have fun with it.

     

    My .02

    -J

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • morgaine
    morgaine over 13 years ago in reply to jamodio

    jamodio wrote:

     

    I think we can have an interesting discussion somewhere else in the forum about BGA vs ???, there are pros and cons, and as I always say it depends on the application and the target "customer."

     

    If you are in this just for a hobby, a DYI project or some basic integration, don't mess with what you don't know how to do or have the tools to do it, you will waste more time and money, just buy a ready made BBB and have fun with it.

     

    Although I agree that BBB is well in the lead for embedded OSHW capability up to Cortex-A8 level, I was looking beyond that.  It's not like there is a Beagle roadmap catering for all our needs into the distant future, and even if there was, we still wouldn't want to be dependent on a single manufacturer.

     

    The community of OSHW enthusiasts would be stronger if it took control of its own destiny than by being mere consumers of OSHW designs that commercial companies feel like providing.  It's just like what happened when 3D printing enthusiasts discovered that they could build their own printers and that this independence from commercial 3D printing gave them immense power and control over their own destinies.

     

    Exactly the same would happen if we took computer design and construction into our own hands.