Raspberry Pi Forum Ras Pi as a security Device
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 681 subscribers
  • Views 483 views
  • Users 0 members are here
  • raspberry_pi
Related

Ras Pi as a security Device

GreenYamo
GreenYamo over 13 years ago

I've been thinking about getting the British Gas Safer Home starter kit, as per here: http://www.britishgas.co.uk/products-and-services/safe-and-secure/starter-kit.html

 

A thought closely on the heels of that one (and in a effort to save some cash) was to put the Pi to use as a similar device. I beleive the system used Zigbee as the wireless system so although the on-line part wouldn't be that easy to replicate, the rest of it should be.

 

I'd be grateful to hear any thoughts and if indeed it would be cost effective.

 

Thank you.

 

Steve

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 13 years ago

    I tend to agree, sadly some home alarm is virtually essential these days. If you're going down the ready-built route, you may also want to consider honeywell systems, they are rather low cost and I believe are one of the standard types installed by alarm fitters. The configuration on them is a little convoluted but very feasible. Personally I would use a wired system, but sometimes that is not possible.

    For a home-built solution, the rasp-pi would be ideal if you wanted to add internet connectivity to your alarm system. It may be easier to use an existing alarm system (e.g. the honeywell types) and add the Rasp-Pi to it. Most of the existing systems have LED status lights, and lots of room inside the case (as long as you don't buy the 'compact' control panels), so it could be feasible to monitor some LEDs (just solder a wire to it) via

    the Rasp-Pi. This way, you'd have a reliable system that could continue to function even if the add-on misbehaves.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 13 years ago

    I tend to agree, sadly some home alarm is virtually essential these days. If you're going down the ready-built route, you may also want to consider honeywell systems, they are rather low cost and I believe are one of the standard types installed by alarm fitters. The configuration on them is a little convoluted but very feasible. Personally I would use a wired system, but sometimes that is not possible.

    For a home-built solution, the rasp-pi would be ideal if you wanted to add internet connectivity to your alarm system. It may be easier to use an existing alarm system (e.g. the honeywell types) and add the Rasp-Pi to it. Most of the existing systems have LED status lights, and lots of room inside the case (as long as you don't buy the 'compact' control panels), so it could be feasible to monitor some LEDs (just solder a wire to it) via

    the Rasp-Pi. This way, you'd have a reliable system that could continue to function even if the add-on misbehaves.