Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi Hardware mods
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 708 subscribers
  • Views 1226 views
  • Users 0 members are here
  • raspberry_pi
Related

Pi Hardware mods

e14 Contributor
e14 Contributor over 13 years ago

I've been a bit quiet on the R-Pi front for a while, so I thought some of you might enjoy a quick look at what I've been up to.

 

imageimage

There's some more at https://picasaweb.google.com/selsinork/RaspberryPiModifications

 

So any guesses what I've been building ?

  • Sign in to reply
  • Cancel
Parents
  • jamodio
    jamodio over 13 years ago

    Very nice, thanks for sharing !!!

     

    I like that you took care of the power supplies using the TPS54231, I love those litte switchers and now I'm getting in love with even a smaller one for other application which can handle up to 1.2A, the TPS62080 which has some variants with fixed outputs. But it is a small QFN not really very prototype friendly.

     

    Since I'm getting involved in some educational efforts I may put together a design for an add on board designed around activities for the kids. I like the one you did with the serial interface, I'd go probably go with the FTDI chip for a serial-USB converter given that most of the laptops/netbooks we'll have no longer have the old COM serial ports. I don't think I'll replace the 3.3V and 1.8V regulators but most probably put something better for the main 5V like I did with the TPS54231 for one of the boards I've.

     

    I'm really waiting for the Model A to become available in the US, the plan is to have them just with wifi, use VNC from the netbooks and perhaps a 802.15.4 option.

     

    It is not a great piece of engineering but I recently tested the PiMatrix http://www.youtube.com/watch?v=7hiOmja1a7A it is a good gizmo to teach kids how computers work, binary and hexadecimal numbers, etc. I'll most probably post online some of the ideas using Python and Scratch.

     

    Cheers

    Jorge

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jamodio
    jamodio over 13 years ago

    Very nice, thanks for sharing !!!

     

    I like that you took care of the power supplies using the TPS54231, I love those litte switchers and now I'm getting in love with even a smaller one for other application which can handle up to 1.2A, the TPS62080 which has some variants with fixed outputs. But it is a small QFN not really very prototype friendly.

     

    Since I'm getting involved in some educational efforts I may put together a design for an add on board designed around activities for the kids. I like the one you did with the serial interface, I'd go probably go with the FTDI chip for a serial-USB converter given that most of the laptops/netbooks we'll have no longer have the old COM serial ports. I don't think I'll replace the 3.3V and 1.8V regulators but most probably put something better for the main 5V like I did with the TPS54231 for one of the boards I've.

     

    I'm really waiting for the Model A to become available in the US, the plan is to have them just with wifi, use VNC from the netbooks and perhaps a 802.15.4 option.

     

    It is not a great piece of engineering but I recently tested the PiMatrix http://www.youtube.com/watch?v=7hiOmja1a7A it is a good gizmo to teach kids how computers work, binary and hexadecimal numbers, etc. I'll most probably post online some of the ideas using Python and Scratch.

     

    Cheers

    Jorge