Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi Ethernet Problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 30 replies
  • Subscribers 707 subscribers
  • Views 18465 views
  • Users 0 members are here
  • raspberry
  • raspberry_pi
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Raspberry Pi Ethernet Problem

e14 Contributor
e14 Contributor over 13 years ago

Whenever I turn my Raspberry Pi on, the three network lights just blink and it can't connect to the internet. I have checked all network items and they do work so it comes down to the Raspberry Pi.  Is there something physicaly wrong with the board itself?

 

It is Model B and I have Wheezy installed on the SD card if that helps or makes a difference at all.

  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    In that case it seems that the network device is OK. Try manually setting the network configuration.

    Use your favourite editor on /etc/network/interfaces file. Make sure it looks like this:

     

    auto eth0

    iface eth0 inet dhcp

     

    If that works, you should be good to go. If that doesn't work then set the IP address manually, you need to know the subnet, usually 192.168.0.0 or 192.168.1.0, and your router IP address,

     

    auto eth0

        iface eth0 inet static

            address 192.168.0.55

            netmask 255.255.255.0

            gateway 192.168.0.254

     

    If this works you should have network connection, man interfaces should give you more information on this file should you need it.

     

    This will test whether you can get a network configuration loaded. If you can then se if you can ping your router.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    In that case it seems that the network device is OK. Try manually setting the network configuration.

    Use your favourite editor on /etc/network/interfaces file. Make sure it looks like this:

     

    auto eth0

    iface eth0 inet dhcp

     

    If that works, you should be good to go. If that doesn't work then set the IP address manually, you need to know the subnet, usually 192.168.0.0 or 192.168.1.0, and your router IP address,

     

    auto eth0

        iface eth0 inet static

            address 192.168.0.55

            netmask 255.255.255.0

            gateway 192.168.0.254

     

    If this works you should have network connection, man interfaces should give you more information on this file should you need it.

     

    This will test whether you can get a network configuration loaded. If you can then se if you can ping your router.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    I tried both. By setting it to DHCP, upon reboot it just searched several times for an IP address but never got one. I tried to ping once it rebooted and nothng. I also tried setting a static IP as you said and nothing for a ping still. Perhaps something is physically wrong with the ethernet port?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    That is possibility, but more likely it is your ethernet cable. Test that on a workimg system just to discount it.

     

    Also try one of the other distributions or an updated copy of Raspbian from here http://www.raspberrypi.org/downloads

    (you didn't say what version you were running).

     

    Also check your router is actually sending DHCP out on the ethernet port (you didn't mention what router you had).

     

    If you have managed to configure a static IP address properly can you post the output of ifconfig please. Also can you ensure that your chosen IP address is on the same subnet as the router (sorry if this is basic stuff, but I don't like to make assumptions about your experience level as you haven't said).

     

    Another trick is to connect another device into the wired network and try that out. Once you have a working connection on that device try connecting to the Pi or vice versa. It would be useful if you could also post the output of ipconfig /a from any Windows device you have connected, or ifconfig from a Mac or Linux terminal session on the other device.

     

    Ethernet ports are usually quite reliable. Mostly it is bad cables, dodgy DHCP configurations or problems with the arbitration of a connection speed with the switch/hub. On that subject what is your switch/hub (manufacturer and model)?

     

    Please also list your IP address configuration for the internal network of your router, Pi and other wire connected computing device, just so we are clear that everything is OK.

     

    Christian

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to e14 Contributor

    Eric Finendale wrote:

     

    I tried both. By setting it to DHCP, upon reboot it just searched several times for an IP address but never got one. I tried to ping once it rebooted and nothng. I also tried setting a static IP as you said and nothing for a ping still. Perhaps something is physically wrong with the ethernet port?

    The LEDs blinking might mean that the Ethernet port is trying to auto-negotiate and/or auto-MDIX (exchanging the RX and TX pairs so it doesn't matter what kind of cable you have plugged in) and is failing due to a bad Ethernet cable or physically bad Ethernet jack on the RasPi.  Check it carefully with a strong light to make sure the pins look good, and check the discrete resistors and capacitors near the Ethernet jack for bad solder joints and missing components.  Make sure the Ethernet jack pins actually go through the board and are soldered properly.  (A long shot is that the manufacturer used the wrong kind of Ethernet magjack, but that's pretty unlikely.)

     

    If trying to ping RasPi causes it to reboot you may have a hardware problem.  Check the TP1-TP2 voltage, since iffy power supplies can cause all sorts of RasPi problems: see the RasPi Troubleshooting Wiki here and here.

     

    Another possibility is a bad OS image.  You might try rewriting the OS image onto your SD card.

     

    If none of these work, it might be a bad solder joint or cracked PC board trace somewhere and you should RMA.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • drifter1693
    drifter1693 over 8 years ago in reply to e14 Contributor

    Can I use mobile hotspot as a router