Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum how to download arduino on raspberry pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 708 subscribers
  • Views 3219 views
  • Users 0 members are here
  • raspberry_pi
Related

how to download arduino on raspberry pi

chiversj
chiversj over 13 years ago

I followed the instructions from the book, titled Installing Arduino in Raspian. BIG FAIL. The word electronics did not show up. I have the latest download of Wheezy. Would appreciate some help on this. Thanks Jimmy

  • Sign in to reply
  • Cancel
Parents
  • gdstew
    gdstew over 13 years ago

    Here's what I did to get the Arduino IDE on the Raspberry Pi:

     

    sudo apt-get update

    sudo apt get install arduino

     

    The update command will make sure that you get the latest versions of all the files. If you do not do this it may not find

    some of the files and it will not install. I've had this happen to me twice now.

     

    The install command will automatically download and install all the files needed  (including arduino-core) for the Arduino IDE.

     

    After you have have done this you should see the Electronics folder in your Applications menu. The Arduino IDE should be in

    that folder.

     

    Good luck.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • chiversj
    chiversj over 13 years ago in reply to gdstew

    Mr Stewart Idid exactly that more than once and it did NOT work. Do not know why but the electronics folder does not come up. Thank you. Jimmy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to chiversj

    OK, let's try this, I know it looks like a lot but you will only need to do 1 or 2 (not both), and

      3 only if 1 or 2 fails:

     

    1) If you know how to use the vi editor:

     

      a. Make a backup copy first:

     

        sudo cp /etc/apt/sources.list /etc/apt/sources.list.bak

     

      b. Edit the file:

     

        sudo vi /etc/apt/sources.list

     

      c. Add this line:

     

        deb http://mirrordirector.raspbian.org/raspbian wheezy main contrib non-free rpi

     

      d. Try the apt-get update and install again.

     

    2) If you do not know how to use vi use a graphical interface editor by:

     

      a. Make a backup copy as shown in 1a

     

      b. Assuming you are in the pi home directory (/home/pi) so you know where the file is,

          copy the sources.list file:

     

        sudo cp /etc/apt/sources.list .

     

      c. Change the ownership so you can modify it:

     

        sudo chown pi:pi sources.list

     

      d. Use any text editor you like to add the same line as in 1c

     

      e. Put the modified file back where it belongs:

     

        sudo chown root:root sources.list

     

        sudo mv sources.list /etc/apt

     

       Note:  using chown again is probably not needed if sudo is used to move it back, but

                 just in case I added the command anyway.

     

      f. Try the atp-get update and install again.

     

    3) If 1 or 2 fails

     

    Do another apt-get install and send the error output and standard output from that command to

    the file arduino.txt using this command:

     

    sudo apt-get install arduino 2>&1 arduino.txt

     

    None of the normal text output from the command will be sent to the screen so just wait until the

    command line prompt is displayed before going to the next command.

     

    Change the ownership of arduino.txt to make sure you can read and write it:

     

    sudo chown pi:pi arduino.txt

     

    Attach the arduino.txt file to an email and send it to the email address in my profile.

     

    If there is an error message in the file I should be able to find it and help fix it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mconners
    mconners over 13 years ago in reply to chiversj

    Just for fun I started with a fresh install.

     

    I did

     

    sudo apt-get update

     

    sudo apt-get upgrade

     

    sudo reboot

     

    sudo apt-get install arduino

     

    everything worked fine.

     

    Now it did install java, the avr tools, etc...

     

    the only think I can think of is that the installation did not complete somehow. Do what Gary said and capture your output. Are you sure you have plenty of diskspace? I did this on a 16gb card, a 2 or a 4 may be too small.

     

    It definitely installed it in /usr/share/arduino and it created the Electronics folder in the menu and put Arduin IDE

    in there.

     

    We can solve this for you, I'm sure it is something silly.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mconners
    mconners over 13 years ago in reply to chiversj

    Just for fun I started with a fresh install.

     

    I did

     

    sudo apt-get update

     

    sudo apt-get upgrade

     

    sudo reboot

     

    sudo apt-get install arduino

     

    everything worked fine.

     

    Now it did install java, the avr tools, etc...

     

    the only think I can think of is that the installation did not complete somehow. Do what Gary said and capture your output. Are you sure you have plenty of diskspace? I did this on a 16gb card, a 2 or a 4 may be too small.

     

    It definitely installed it in /usr/share/arduino and it created the Electronics folder in the menu and put Arduin IDE

    in there.

     

    We can solve this for you, I'm sure it is something silly.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • gdstew
    gdstew over 13 years ago in reply to mconners

    Hi Mike and Jimmy,

     

    I have installed the Arduino IDE five or six times on the Pi (I have two Pi's, one 256MB and one 512MB, and have upgraded Raspbian and

    the SD card disks a couple of times on each) and the only thing I've had problems with recently is forgetting to update before the install.

    However Jimmy, Mike's disk size question is a good one. The Arduino IDE install requires a quite a bit of disk space mainly because of

    Java and the way apt-get caches packages it is installing and I'm pretty sure that it was a problem on one of my earliest install attempts

    with a 2GB SD card. This was one of the main reasons for my first SD card upgrades. I definitely recommend a 4GB SD card minimum if

    you plan to add any software at all to  the Pi.

     

    If you have a 4 GB or larger SD card or just prefer to skip my first two suggestions and go directly to the ouput capture go ahead. Like Mike

    said I'm sure we can help you get this working.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mconners
    mconners over 13 years ago in reply to gdstew

    I didn't remember having any issues when I had installed it before either. As a matter of fact tonight I did it on 2 seperate pi's and had no issues with the instructions I gave. One I did over VNC and one through ssh on the console. I've gotta believe something went wrong in the install, either ran out of disk space, or something couldnt get resolved. But the packages seemed pretty tight tonight.

     

    We'll get him going.

     

    Mike